ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_CTRL_REG5_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_CTRL_REG5_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_cfg_drdy: 1
 
   uint8_t   int_cfg_a_vecm: 1
 
   uint8_t   int_cfg_ff_mt: 1
 
   uint8_t   int_cfg_pulse: 1
 
   uint8_t   int_cfg_lndprt: 1
 
   uint8_t   int_cfg_trans: 1
 
   uint8_t   int_cfg_fifo: 1
 
   uint8_t   int_cfg_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1920 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ int_cfg_a_vecm

uint8_t int_cfg_a_vecm

Definition at line 1924 of file fxls8471q.h.

◆ int_cfg_aslp

uint8_t int_cfg_aslp

Definition at line 1936 of file fxls8471q.h.

◆ int_cfg_drdy

uint8_t int_cfg_drdy

Definition at line 1922 of file fxls8471q.h.

◆ int_cfg_ff_mt

uint8_t int_cfg_ff_mt

Definition at line 1926 of file fxls8471q.h.

◆ int_cfg_fifo

uint8_t int_cfg_fifo

Definition at line 1934 of file fxls8471q.h.

◆ int_cfg_lndprt

uint8_t int_cfg_lndprt

Definition at line 1930 of file fxls8471q.h.

◆ int_cfg_pulse

uint8_t int_cfg_pulse

Definition at line 1928 of file fxls8471q.h.

◆ int_cfg_trans

uint8_t int_cfg_trans

Definition at line 1932 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1939 of file fxls8471q.h.


The documentation for this union was generated from the following file: