ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_A_FFMT_THS_Y_MSB_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_A_FFMT_THS_Y_MSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   a_ffmt_ths_y: 7
 
   uint8_t   a_ffmt_trans_ths_en: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 2391 of file fxls8471q.h.

Field Documentation

◆ a_ffmt_ths_y

uint8_t a_ffmt_ths_y

Definition at line 2393 of file fxls8471q.h.

◆ a_ffmt_trans_ths_en

uint8_t a_ffmt_trans_ths_en

Definition at line 2394 of file fxls8471q.h.

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 2396 of file fxls8471q.h.


The documentation for this union was generated from the following file: