ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS896x_SENS_CONFIG3_t Union Reference

#include <fxls896x.h>

Collaboration diagram for FXLS896x_SENS_CONFIG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   sleep_odr: 4
 
   uint8_t   wake_odr: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 533 of file fxls896x.h.

Field Documentation

◆ b

struct { ... } b

◆ sleep_odr

uint8_t sleep_odr

Definition at line 537 of file fxls896x.h.

◆ w

uint8_t w

Definition at line 542 of file fxls896x.h.

◆ wake_odr

uint8_t wake_odr

Definition at line 539 of file fxls896x.h.


The documentation for this union was generated from the following file: