ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS896x_INT_EN_t Union Reference

#include <fxls896x.h>

Collaboration diagram for FXLS896x_INT_EN_t:
Collaboration graph

Data Fields

struct {
   uint8_t   wake_out_en: 1
 
   uint8_t   boot_dis: 1
 
   uint8_t   aslp_en: 1
 
   uint8_t   orient_en: 1
 
   uint8_t   sdcd_wt_en: 1
 
   uint8_t   sdcd_ot_en: 1
 
   uint8_t   buf_en: 1
 
   uint8_t   drdy_en: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 803 of file fxls896x.h.

Field Documentation

◆ aslp_en

uint8_t aslp_en

Definition at line 811 of file fxls896x.h.

◆ b

struct { ... } b

◆ boot_dis

uint8_t boot_dis

Definition at line 809 of file fxls896x.h.

◆ buf_en

uint8_t buf_en

Definition at line 819 of file fxls896x.h.

◆ drdy_en

uint8_t drdy_en

Definition at line 820 of file fxls896x.h.

◆ orient_en

uint8_t orient_en

Definition at line 813 of file fxls896x.h.

◆ sdcd_ot_en

uint8_t sdcd_ot_en

Definition at line 817 of file fxls896x.h.

◆ sdcd_wt_en

uint8_t sdcd_wt_en

Definition at line 815 of file fxls896x.h.

◆ w

uint8_t w

Definition at line 823 of file fxls896x.h.

◆ wake_out_en

uint8_t wake_out_en

Definition at line 807 of file fxls896x.h.


The documentation for this union was generated from the following file: