ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS896x_INT_PIN_SEL_t Union Reference

#include <fxls896x.h>

Collaboration diagram for FXLS896x_INT_PIN_SEL_t:
Collaboration graph

Data Fields

struct {
   uint8_t   wk_out_int2: 1
 
   uint8_t   boot_int2: 1
 
   uint8_t   aslp_int2: 1
 
   uint8_t   orient_int2: 1
 
   uint8_t   sdcd_wt_int2: 1
 
   uint8_t   sdcd_ot_int2: 1
 
   uint8_t   buf_int2: 1
 
   uint8_t   drdy_int2: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 886 of file fxls896x.h.

Field Documentation

◆ aslp_int2

uint8_t aslp_int2

Definition at line 894 of file fxls896x.h.

◆ b

struct { ... } b

◆ boot_int2

uint8_t boot_int2

Definition at line 892 of file fxls896x.h.

◆ buf_int2

uint8_t buf_int2

Definition at line 902 of file fxls896x.h.

◆ drdy_int2

uint8_t drdy_int2

Definition at line 904 of file fxls896x.h.

◆ orient_int2

uint8_t orient_int2

Definition at line 896 of file fxls896x.h.

◆ sdcd_ot_int2

uint8_t sdcd_ot_int2

Definition at line 900 of file fxls896x.h.

◆ sdcd_wt_int2

uint8_t sdcd_wt_int2

Definition at line 898 of file fxls896x.h.

◆ w

uint8_t w

Definition at line 907 of file fxls896x.h.

◆ wk_out_int2

uint8_t wk_out_int2

Definition at line 890 of file fxls896x.h.


The documentation for this union was generated from the following file: