ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS896x_SDCD_INT_SRC1_t Union Reference

#include <fxls896x.h>

Collaboration diagram for FXLS896x_SDCD_INT_SRC1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   z_ot_pol: 1
 
   uint8_t   z_ot_ef: 1
 
   uint8_t   y_ot_pol: 1
 
   uint8_t   y_ot_ef: 1
 
   uint8_t   x_ot_pol: 1
 
   uint8_t   x_ot_ef: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   ot_ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1352 of file fxls896x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1368 of file fxls896x.h.

◆ b

struct { ... } b

◆ ot_ea

uint8_t ot_ea

Definition at line 1369 of file fxls896x.h.

◆ w

uint8_t w

Definition at line 1372 of file fxls896x.h.

◆ x_ot_ef

uint8_t x_ot_ef

Definition at line 1366 of file fxls896x.h.

◆ x_ot_pol

uint8_t x_ot_pol

Definition at line 1364 of file fxls896x.h.

◆ y_ot_ef

uint8_t y_ot_ef

Definition at line 1362 of file fxls896x.h.

◆ y_ot_pol

uint8_t y_ot_pol

Definition at line 1360 of file fxls896x.h.

◆ z_ot_ef

uint8_t z_ot_ef

Definition at line 1358 of file fxls896x.h.

◆ z_ot_pol

uint8_t z_ot_pol

Definition at line 1356 of file fxls896x.h.


The documentation for this union was generated from the following file: