ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPQ3115_T_MIN_LSB_t Union Reference

#include <fxpq3115.h>

Collaboration diagram for FXPQ3115_T_MIN_LSB_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 4
 
   uint8_t   mintd: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 714 of file fxpq3115.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 716 of file fxpq3115.h.

◆ b

struct { ... } b

◆ mintd

uint8_t mintd

Definition at line 717 of file fxpq3115.h.

◆ w

uint8_t w

Definition at line 720 of file fxpq3115.h.


The documentation for this union was generated from the following file: