ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPQ3115_CTRL_REG1_t Union Reference

#include <fxpq3115.h>

Collaboration diagram for FXPQ3115_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   sbyb: 1
 
   uint8_t   ost: 1
 
   uint8_t   rst: 1
 
   uint8_t   os: 3
 
   uint8_t   raw: 1
 
   uint8_t   alt: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 822 of file fxpq3115.h.

Field Documentation

◆ alt

uint8_t alt

Definition at line 836 of file fxpq3115.h.

◆ b

struct { ... } b

◆ os

uint8_t os

Definition at line 831 of file fxpq3115.h.

◆ ost

uint8_t ost

Definition at line 826 of file fxpq3115.h.

◆ raw

uint8_t raw

Definition at line 833 of file fxpq3115.h.

◆ rst

uint8_t rst

Definition at line 829 of file fxpq3115.h.

◆ sbyb

uint8_t sbyb

Definition at line 824 of file fxpq3115.h.

◆ w

uint8_t w

Definition at line 839 of file fxpq3115.h.


The documentation for this union was generated from the following file: