ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPQ3115_CTRL_REG4_t Union Reference

#include <fxpq3115.h>

Collaboration diagram for FXPQ3115_CTRL_REG4_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_en_tchg: 1
 
   uint8_t   int_en_pchg: 1
 
   uint8_t   int_en_tth: 1
 
   uint8_t   int_en_pth: 1
 
   uint8_t   int_en_tw: 1
 
   uint8_t   int_en_pw: 1
 
   uint8_t   int_en_fifo: 1
 
   uint8_t   int_en_drdy: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1004 of file fxpq3115.h.

Field Documentation

◆ b

struct { ... } b

◆ int_en_drdy

uint8_t int_en_drdy

Definition at line 1020 of file fxpq3115.h.

◆ int_en_fifo

uint8_t int_en_fifo

Definition at line 1018 of file fxpq3115.h.

◆ int_en_pchg

uint8_t int_en_pchg

Definition at line 1008 of file fxpq3115.h.

◆ int_en_pth

uint8_t int_en_pth

Definition at line 1012 of file fxpq3115.h.

◆ int_en_pw

uint8_t int_en_pw

Definition at line 1016 of file fxpq3115.h.

◆ int_en_tchg

uint8_t int_en_tchg

Definition at line 1006 of file fxpq3115.h.

◆ int_en_tth

uint8_t int_en_tth

Definition at line 1010 of file fxpq3115.h.

◆ int_en_tw

uint8_t int_en_tw

Definition at line 1014 of file fxpq3115.h.

◆ w

uint8_t w

Definition at line 1023 of file fxpq3115.h.


The documentation for this union was generated from the following file: