ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_INT_SOURCE_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_INT_SOURCE_t:
Collaboration graph

Data Fields

struct {
   uint8_t   src_drdy: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   src_ff_mt: 1
 
   uint8_t   src_pulse: 1
 
   uint8_t   src_lndprt: 1
 
   uint8_t   src_trans: 1
 
   uint8_t   src_fifo: 1
 
   uint8_t   src_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 402 of file mma845x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 406 of file mma845x.h.

◆ b

struct { ... } b

◆ src_aslp

uint8_t src_aslp

Definition at line 417 of file mma845x.h.

◆ src_drdy

uint8_t src_drdy

Definition at line 404 of file mma845x.h.

◆ src_ff_mt

uint8_t src_ff_mt

Definition at line 407 of file mma845x.h.

◆ src_fifo

uint8_t src_fifo

Definition at line 415 of file mma845x.h.

◆ src_lndprt

uint8_t src_lndprt

Definition at line 411 of file mma845x.h.

◆ src_pulse

uint8_t src_pulse

Definition at line 409 of file mma845x.h.

◆ src_trans

uint8_t src_trans

Definition at line 413 of file mma845x.h.

◆ w

uint8_t w

Definition at line 420 of file mma845x.h.


The documentation for this union was generated from the following file: