ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_FF_MT_CFG_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_FF_MT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   reserved: 3
 
   uint8_t   xefe: 1
 
   uint8_t   yefe: 1
 
   uint8_t   zefe: 1
 
   uint8_t   oae: 1
 
   uint8_t   ele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 787 of file mma845x.h.

Field Documentation

◆ b

struct { ... } b

◆ ele

uint8_t ele

Definition at line 799 of file mma845x.h.

◆ oae

uint8_t oae

Definition at line 797 of file mma845x.h.

◆ reserved

uint8_t reserved

Definition at line 789 of file mma845x.h.

◆ w

uint8_t w

Definition at line 802 of file mma845x.h.

◆ xefe

uint8_t xefe

Definition at line 791 of file mma845x.h.

◆ yefe

uint8_t yefe

Definition at line 793 of file mma845x.h.

◆ zefe

uint8_t zefe

Definition at line 795 of file mma845x.h.


The documentation for this union was generated from the following file: