ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_PULSE_CFG_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_PULSE_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xspefe: 1
 
   uint8_t   xdpefe: 1
 
   uint8_t   yspefe: 1
 
   uint8_t   ydpefe: 1
 
   uint8_t   zspefe: 1
 
   uint8_t   zdpefe: 1
 
   uint8_t   ele: 1
 
   uint8_t   dpa: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1200 of file mma845x.h.

Field Documentation

◆ b

struct { ... } b

◆ dpa

uint8_t dpa

Definition at line 1216 of file mma845x.h.

◆ ele

uint8_t ele

Definition at line 1214 of file mma845x.h.

◆ w

uint8_t w

Definition at line 1219 of file mma845x.h.

◆ xdpefe

uint8_t xdpefe

Definition at line 1204 of file mma845x.h.

◆ xspefe

uint8_t xspefe

Definition at line 1202 of file mma845x.h.

◆ ydpefe

uint8_t ydpefe

Definition at line 1208 of file mma845x.h.

◆ yspefe

uint8_t yspefe

Definition at line 1206 of file mma845x.h.

◆ zdpefe

uint8_t zdpefe

Definition at line 1212 of file mma845x.h.

◆ zspefe

uint8_t zspefe

Definition at line 1210 of file mma845x.h.


The documentation for this union was generated from the following file: