ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_PULSE_SRC_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_PULSE_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   polx: 1
 
   uint8_t   poly: 1
 
   uint8_t   polz: 1
 
   uint8_t   dpe: 1
 
   uint8_t   axx: 1
 
   uint8_t   axy: 1
 
   uint8_t   axz: 1
 
   uint8_t   ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1282 of file mma845x.h.

Field Documentation

◆ axx

uint8_t axx

Definition at line 1292 of file mma845x.h.

◆ axy

uint8_t axy

Definition at line 1294 of file mma845x.h.

◆ axz

uint8_t axz

Definition at line 1296 of file mma845x.h.

◆ b

struct { ... } b

◆ dpe

uint8_t dpe

Definition at line 1290 of file mma845x.h.

◆ ea

uint8_t ea

Definition at line 1298 of file mma845x.h.

◆ polx

uint8_t polx

Definition at line 1284 of file mma845x.h.

◆ poly

uint8_t poly

Definition at line 1286 of file mma845x.h.

◆ polz

uint8_t polz

Definition at line 1288 of file mma845x.h.

◆ w

uint8_t w

Definition at line 1301 of file mma845x.h.


The documentation for this union was generated from the following file: