ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_PULSE_THSY_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_PULSE_THSY_t:
Collaboration graph

Data Fields

struct {
   uint8_t   thsy: 7
 
   uint8_t   reserved: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1393 of file mma845x.h.

Field Documentation

◆ b

struct { ... } b

◆ reserved

uint8_t reserved

Definition at line 1397 of file mma845x.h.

◆ thsy

uint8_t thsy

Definition at line 1395 of file mma845x.h.

◆ w

uint8_t w

Definition at line 1400 of file mma845x.h.


The documentation for this union was generated from the following file: