ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_CTRL_REG1_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   mode: 1
 
   uint8_t   f_read: 1
 
   uint8_t   lnoise: 1
 
   uint8_t   dr: 3
 
   uint8_t   aslp_rate: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1559 of file mma845x.h.

Field Documentation

◆ aslp_rate

uint8_t aslp_rate

Definition at line 1569 of file mma845x.h.

◆ b

struct { ... } b

◆ dr

uint8_t dr

Definition at line 1567 of file mma845x.h.

◆ f_read

uint8_t f_read

Definition at line 1563 of file mma845x.h.

◆ lnoise

uint8_t lnoise

Definition at line 1565 of file mma845x.h.

◆ mode

uint8_t mode

Definition at line 1561 of file mma845x.h.

◆ w

uint8_t w

Definition at line 1573 of file mma845x.h.


The documentation for this union was generated from the following file: