ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA845x_CTRL_REG5_t Union Reference

#include <mma845x.h>

Collaboration diagram for MMA845x_CTRL_REG5_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_cfg_drdy: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   int_cfg_ff_mt: 1
 
   uint8_t   int_cfg_pulse: 1
 
   uint8_t   int_cfg_lndprt: 1
 
   uint8_t   int_cfg_trans: 1
 
   uint8_t   int_cfg_fifo: 1
 
   uint8_t   int_cfg_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1844 of file mma845x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1848 of file mma845x.h.

◆ b

struct { ... } b

◆ int_cfg_aslp

uint8_t int_cfg_aslp

Definition at line 1859 of file mma845x.h.

◆ int_cfg_drdy

uint8_t int_cfg_drdy

Definition at line 1846 of file mma845x.h.

◆ int_cfg_ff_mt

uint8_t int_cfg_ff_mt

Definition at line 1849 of file mma845x.h.

◆ int_cfg_fifo

uint8_t int_cfg_fifo

Definition at line 1857 of file mma845x.h.

◆ int_cfg_lndprt

uint8_t int_cfg_lndprt

Definition at line 1853 of file mma845x.h.

◆ int_cfg_pulse

uint8_t int_cfg_pulse

Definition at line 1851 of file mma845x.h.

◆ int_cfg_trans

uint8_t int_cfg_trans

Definition at line 1855 of file mma845x.h.

◆ w

uint8_t w

Definition at line 1862 of file mma845x.h.


The documentation for this union was generated from the following file: