ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA8491Q_STATUS_t Union Reference

#include <mma8491q.h>

Collaboration diagram for MMA8491Q_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xdr: 1
 
   uint8_t   ydr: 1
 
   uint8_t   zdr: 1
 
   uint8_t   zyxdr: 1
 
   uint8_t   reserved: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 37 of file mma8491q.h.

Field Documentation

◆ b

struct { ... } b

◆ reserved

uint8_t reserved

Definition at line 49 of file mma8491q.h.

◆ w

uint8_t w

Definition at line 52 of file mma8491q.h.

Referenced by MMA8491Q_I2C_Initialize().

◆ xdr

uint8_t xdr

Definition at line 41 of file mma8491q.h.

◆ ydr

uint8_t ydr

Definition at line 43 of file mma8491q.h.

◆ zdr

uint8_t zdr

Definition at line 45 of file mma8491q.h.

◆ zyxdr

uint8_t zyxdr

Definition at line 47 of file mma8491q.h.


The documentation for this union was generated from the following file: