31     if ((pSensorHandle == NULL) || (pBus == NULL))
    71     if ((pSensorHandle == NULL) || (pReadList == NULL) || (pBuffer == NULL))
    85     if (ARM_DRIVER_OK != status)
 
This defines the function pointers and sensor specific information. 
 
int32_t Sensor_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, const registerreadlist_t *pReadList, uint8_t *pOutBuffer)
Read register data from a sensor. 
 
int32_t Register_I2C_Read(ARM_DRIVER_I2C *pCommDrv, registerDeviceInfo_t *devInfo, uint16_t slaveAddress, uint8_t offset, uint8_t length, uint8_t *pOutBuffer)
The interface function to read a sensor register. 
 
ARM_DRIVER_I2C * pCommDrv
 
typedef int32_t(DATA_FORMAT_Append_t))(void *pData
The interface function to append the data on the formated stream. 
 
void MMA8491Q_I2C_SetIdleTask(mma8491q_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
 
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
 
registerDeviceInfo_t deviceInfo
 
int32_t MMA8491Q_I2C_ReadData(mma8491q_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
 
The mma8491q_drv.h file describes the MMA8491Q driver interface and structures. 
 
int32_t MMA8491Q_I2C_Initialize(mma8491q_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress)
The interface function to initialize the sensor. 
 
#define MMA8491Q_STATUS_RESERVED_MASK
 
This structure defines the Read command List. 
 
#define MMA8491Q_STATUS_RESERVED_ZERO
 
registeridlefunction_t idleFunction