![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The GyroSensor structure stores raw and processed measurements for a 3-axis gyroscope. More...
#include <sensor_fusion.h>

Data Fields | |
| uint8_t | iWhoAmI |
| sensor whoami More... | |
| bool | isEnabled |
| true if the device is sampling More... | |
| uint8_t | iFIFOCount |
| number of measurements read from FIFO More... | |
| uint16_t | iFIFOExceeded |
| Number of samples received in excess of software FIFO size. More... | |
| int16_t | iYsFIFO [GYRO_FIFO_SIZE][3] |
| FIFO measurements (counts) More... | |
| float | fYs [3] |
| averaged measurement (deg/s) More... | |
| float | fDegPerSecPerCount |
| deg/s per count More... | |
| int16_t | iCountsPerDegPerSec |
| counts per deg/s More... | |
| int16_t | iYs [3] |
| average measurement (counts) More... | |
The GyroSensor structure stores raw and processed measurements for a 3-axis gyroscope.
The GyroSensor structure stores raw and processed measurements, as well as metadata for a single 3-axis gyroscope. This structure is normally "fed" by the sensor driver and "consumed" by the fusion routines.
Definition at line 236 of file sensor_fusion.h.
| float fDegPerSecPerCount |
deg/s per count
Definition at line 245 of file sensor_fusion.h.
Referenced by fRun_6DOF_GY_KALMAN().
| float fYs[3] |
averaged measurement (deg/s)
Definition at line 244 of file sensor_fusion.h.
Referenced by fInit_6DOF_GY_KALMAN(), fInit_9DOF_GBY_KALMAN(), and fRun_3DOF_Y_BASIC().
| int16_t iCountsPerDegPerSec |
counts per deg/s
Definition at line 246 of file sensor_fusion.h.
| uint8_t iFIFOCount |
number of measurements read from FIFO
Definition at line 240 of file sensor_fusion.h.
Referenced by ApplyGyroHAL(), and fRun_6DOF_GY_KALMAN().
| uint16_t iFIFOExceeded |
Number of samples received in excess of software FIFO size.
Definition at line 241 of file sensor_fusion.h.
| bool isEnabled |
true if the device is sampling
Definition at line 239 of file sensor_fusion.h.
| uint8_t iWhoAmI |
sensor whoami
Definition at line 238 of file sensor_fusion.h.
| int16_t iYs[3] |
average measurement (counts)
Definition at line 247 of file sensor_fusion.h.
Referenced by fRun_6DOF_GY_KALMAN().
| int16_t iYsFIFO[GYRO_FIFO_SIZE][3] |
FIFO measurements (counts)
Definition at line 242 of file sensor_fusion.h.
Referenced by ApplyGyroHAL(), and fRun_6DOF_GY_KALMAN().