12 #include "fsl_common.h" 19 #define BOARD_NAME "MIMXRT1024-EVK" 22 #define BOARD_DEBUG_UART_TYPE kSerialPort_Uart 23 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) LPUART1 24 #define BOARD_DEBUG_UART_INSTANCE 1U 26 #define BOARD_DEBUG_UART_CLK_FREQ BOARD_DebugConsoleSrcFreq() 28 #define BOARD_UART_IRQ LPUART1_IRQn 29 #define BOARD_UART_IRQ_HANDLER LPUART1_IRQHandler 31 #ifndef BOARD_DEBUG_UART_BAUDRATE 32 #define BOARD_DEBUG_UART_BAUDRATE (115200U) 36 #define BOARD_ACCEL_I2C_BASEADDR LPI2C4 37 #define BOARD_ACCEL_I2C_CLOCK_SOURCE_SELECT (0U) 38 #define BOARD_ACCEL_I2C_CLOCK_SOURCE_DIVIDER (5U) 39 #define BOARD_ACCEL_I2C_CLOCK_FREQ (CLOCK_GetFreq(kCLOCK_Usb1PllClk) / 8 / (BOARD_ACCEL_I2C_CLOCK_SOURCE_DIVIDER + 1U)) 41 #define BOARD_CODEC_I2C_BASEADDR LPI2C1 42 #define BOARD_CODEC_I2C_INSTANCE 1U 43 #define BOARD_CODEC_I2C_CLOCK_SOURCE_SELECT (0U) 44 #define BOARD_CODEC_I2C_CLOCK_SOURCE_DIVIDER (5U) 45 #define BOARD_CODEC_I2C_CLOCK_FREQ (10000000U) 48 #define LOGIC_LED_ON (0U) 49 #define LOGIC_LED_OFF (1U) 50 #ifndef BOARD_USER_LED_GPIO 51 #define BOARD_USER_LED_GPIO GPIO1 53 #ifndef BOARD_USER_LED_GPIO_PIN 54 #define BOARD_USER_LED_GPIO_PIN (5U) 57 #define USER_LED_INIT(output) \ 58 GPIO_PinWrite(BOARD_USER_LED_GPIO, BOARD_USER_LED_GPIO_PIN, output); \ 59 BOARD_USER_LED_GPIO->GDIR |= (1U << BOARD_USER_LED_GPIO_PIN) 60 #define USER_LED_ON() \ 61 GPIO_PortClear(BOARD_USER_LED_GPIO, 1U << BOARD_USER_LED_GPIO_PIN) 62 #define USER_LED_OFF() GPIO_PortSet(BOARD_USER_LED_GPIO, 1U << BOARD_USER_LED_GPIO_PIN) 63 #define USER_LED_TOGGLE() \ 64 GPIO_PinWrite(BOARD_USER_LED_GPIO, BOARD_USER_LED_GPIO_PIN, \ 65 0x1 ^ GPIO_PinRead(BOARD_USER_LED_GPIO, BOARD_USER_LED_GPIO_PIN)) 68 #ifndef BOARD_USER_BUTTON_GPIO 69 #define BOARD_USER_BUTTON_GPIO GPIO5 71 #ifndef BOARD_USER_BUTTON_GPIO_PIN 72 #define BOARD_USER_BUTTON_GPIO_PIN (0U) 74 #define BOARD_USER_BUTTON_IRQ GPIO5_Combined_0_15_IRQn 75 #define BOARD_USER_BUTTON_IRQ_HANDLER GPIO5_Combined_0_15_IRQHandler 76 #define BOARD_USER_BUTTON_NAME "SW4" 79 #define BOARD_FLASH_SIZE (0x800000U) 82 #define BOARD_ENET0_PHY_ADDRESS (0x02U) 85 #define BOARD_USB_PHY_D_CAL (0x0CU) 86 #define BOARD_USB_PHY_TXCAL45DP (0x06U) 87 #define BOARD_USB_PHY_TXCAL45DM (0x06U) 89 #define BOARD_ARDUINO_INT_IRQ (GPIO1_Combined_16_31_IRQn) 90 #define BOARD_ARDUINO_I2C_IRQ (LPI2C4_IRQn) 91 #define BOARD_ARDUINO_I2C_INDEX (4) 92 #define BOARD_USDHC1_BASEADDR USDHC1 93 #define BOARD_USDHC2_BASEADDR USDHC2 94 #define BOARD_USDHC_CD_GPIO_BASE GPIO3 95 #define BOARD_USDHC_CD_GPIO_PIN 19 96 #define BOARD_USDHC_CD_PORT_IRQ GPIO3_Combined_16_31_IRQn 97 #define BOARD_USDHC_CD_PORT_IRQ_HANDLER GPIO3_Combined_16_31_IRQHandler 99 #define BOARD_USDHC_CD_STATUS() (GPIO_PinRead(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN)) 101 #define BOARD_USDHC_CD_INTERRUPT_STATUS() (GPIO_PortGetInterruptFlags(BOARD_USDHC_CD_GPIO_BASE)) 102 #define BOARD_USDHC_CD_CLEAR_INTERRUPT(flag) (GPIO_PortClearInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, flag)) 104 #define BOARD_USDHC_CD_GPIO_INIT() \ 106 gpio_pin_config_t sw_config = { \ 107 kGPIO_DigitalInput, \ 109 kGPIO_IntRisingOrFallingEdge, \ 111 GPIO_PinInit(BOARD_USDHC_CD_GPIO_BASE, BOARD_USDHC_CD_GPIO_PIN, &sw_config); \ 112 GPIO_PortEnableInterrupts(BOARD_USDHC_CD_GPIO_BASE, 1U << BOARD_USDHC_CD_GPIO_PIN); \ 113 GPIO_PortClearInterruptFlags(BOARD_USDHC_CD_GPIO_BASE, ~0); \ 116 #define BOARD_HAS_SDCARD (1U) 117 #define BOARD_SD_POWER_RESET_GPIO (GPIO3) 118 #define BOARD_SD_POWER_RESET_GPIO_PIN (24U) 120 #define BOARD_USDHC_CARD_INSERT_CD_LEVEL (0U) 122 #define BOARD_USDHC_MMCCARD_POWER_CONTROL(state) 124 #define BOARD_USDHC_MMCCARD_POWER_CONTROL_INIT() \ 126 gpio_pin_config_t sw_config = { \ 127 kGPIO_DigitalOutput, \ 131 GPIO_PinInit(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, &sw_config); \ 132 GPIO_PinWrite(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, true); \ 135 #define BOARD_USDHC_SDCARD_POWER_CONTROL_INIT() \ 137 gpio_pin_config_t sw_config = { \ 138 kGPIO_DigitalOutput, \ 142 GPIO_PinInit(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, &sw_config); \ 145 #define BOARD_USDHC_SDCARD_POWER_CONTROL(state) \ 146 (GPIO_PinWrite(BOARD_SD_POWER_RESET_GPIO, BOARD_SD_POWER_RESET_GPIO_PIN, state)) 148 #define BOARD_USDHC1_CLK_FREQ (CLOCK_GetSysPfdFreq(kCLOCK_Pfd0) / (CLOCK_GetDiv(kCLOCK_Usdhc1Div) + 1U)) 149 #define BOARD_USDHC2_CLK_FREQ (CLOCK_GetSysPfdFreq(kCLOCK_Pfd0) / (CLOCK_GetDiv(kCLOCK_Usdhc2Div) + 1U)) 151 #define BOARD_SD_HOST_BASEADDR BOARD_USDHC1_BASEADDR 152 #define BOARD_SD_HOST_CLK_FREQ BOARD_USDHC1_CLK_FREQ 153 #define BOARD_SD_HOST_IRQ USDHC1_IRQn 155 #define BOARD_MMC_HOST_BASEADDR BOARD_USDHC2_BASEADDR 156 #define BOARD_MMC_HOST_CLK_FREQ BOARD_USDHC2_CLK_FREQ 157 #define BOARD_MMC_HOST_IRQ USDHC2_IRQn 158 #define BOARD_MMC_VCCQ_SUPPLY kMMC_VoltageWindow170to195 159 #define BOARD_MMC_VCC_SUPPLY kMMC_VoltageWindows270to360 164 #define BOARD_MMC_SUPPORT_8BIT_BUS (1U) 166 #define BOARD_SD_HOST_SUPPORT_SDR104_FREQ (100000000U) 167 #define BOARD_SD_HOST_SUPPORT_HS200_FREQ (180000000U) 169 #define BOARD_INITGT202SHIELD_PWRON_GPIO GPIO1 170 #define BOARD_INITGT202SHIELD_PWRON_PORT 1U 171 #define BOARD_INITGT202SHIELD_PWRON_GPIO_PIN 23U 172 #define BOARD_INITGT202SHIELD_PWRON_PIN_NAME GPIO1_23 173 #define BOARD_INITGT202SHIELD_PWRON_LABEL "PWRON" 174 #define BOARD_INITGT202SHIELD_PWRON_NAME "PWRON" 175 #define BOARD_INITGT202SHIELD_PWRON_DIRECTION kGPIO_DigitalOutput 177 #define BOARD_INITGT202SHIELD_IRQ_GPIO GPIO1 178 #define BOARD_INITGT202SHIELD_IRQ_PORT 1U 179 #define BOARD_INITGT202SHIELD_IRQ_GPIO_PIN 22U 180 #define BOARD_INITGT202SHIELD_IRQ_PIN_NAME GPIO1_22 181 #define BOARD_INITGT202SHIELD_IRQ_LABEL "IRQ" 182 #define BOARD_INITGT202SHIELD_IRQ_NAME "IRQ" 183 #define BOARD_INITGT202SHIELD_IRQ_DIRECTION kGPIO_DigitalInput 185 #if defined(__cplusplus) 196 #if defined(SDK_I2C_BASED_COMPONENT_USED) && SDK_I2C_BASED_COMPONENT_USED 198 void BOARD_LPI2C_Init(LPI2C_Type *base, uint32_t clkSrc_Hz);
199 status_t BOARD_LPI2C_Send(LPI2C_Type *base,
200 uint8_t deviceAddress,
202 uint8_t subaddressSize,
205 status_t BOARD_LPI2C_Receive(LPI2C_Type *base,
206 uint8_t deviceAddress,
208 uint8_t subaddressSize,
211 void BOARD_Accel_I2C_Init(
void);
212 status_t BOARD_Accel_I2C_Send(uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint32_t txBuff);
213 status_t BOARD_Accel_I2C_Receive(
214 uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
215 void BOARD_Codec_I2C_Init(
void);
216 status_t BOARD_Codec_I2C_Send(
217 uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize,
const uint8_t *txBuff, uint8_t txBuffSize);
218 status_t BOARD_Codec_I2C_Receive(
219 uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
223 #if defined(__cplusplus)
void BOARD_InitDebugConsole(void)
void BOARD_MMC_Pin_Config(uint32_t speed, uint32_t strength)
uint32_t BOARD_DebugConsoleSrcFreq(void)
void BOARD_SD_Pin_Config(uint32_t speed, uint32_t strength)
void BOARD_ConfigMPU(void)