![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
| #define RTE_I2C0_DMA_RX_CH 1 |
Definition at line 51 of file RTE_Device.h.
| #define RTE_I2C0_DMA_RX_DMA_BASE DMA0 |
Definition at line 54 of file RTE_Device.h.
| #define RTE_I2C0_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 53 of file RTE_Device.h.
| #define RTE_I2C0_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMux0LPI2C0Rx |
Definition at line 52 of file RTE_Device.h.
| #define RTE_I2C0_DMA_TX_CH 0 |
Definition at line 47 of file RTE_Device.h.
| #define RTE_I2C0_DMA_TX_DMA_BASE DMA0 |
Definition at line 50 of file RTE_Device.h.
| #define RTE_I2C0_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 49 of file RTE_Device.h.
| #define RTE_I2C0_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMux0LPI2C0Tx |
Definition at line 48 of file RTE_Device.h.
| #define RTE_I2C3 1 |
Definition at line 14 of file RTE_Device.h.
| #define RTE_I2C3_DMA_EN 0 |
Definition at line 15 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_CH 1 |
Definition at line 60 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_DMA_BASE DMA1 |
Definition at line 63 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_DMAMUX_BASE DMAMUX1 |
Definition at line 62 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMux1LPI2C3Rx |
Definition at line 61 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_CH 0 |
Definition at line 56 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_DMA_BASE DMA1 |
Definition at line 59 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_DMAMUX_BASE DMAMUX1 |
Definition at line 58 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMux1LPI2C3Tx |
Definition at line 57 of file RTE_Device.h.
| #define RTE_SPI0 1 |
Definition at line 16 of file RTE_Device.h.
| #define RTE_SPI0_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 68 of file RTE_Device.h.
| #define RTE_SPI0_DMA_EN 0 |
Definition at line 17 of file RTE_Device.h.
| #define RTE_SPI0_DMA_RX_CH 1 |
Definition at line 75 of file RTE_Device.h.
| #define RTE_SPI0_DMA_RX_DMA_BASE DMA0 |
Definition at line 78 of file RTE_Device.h.
| #define RTE_SPI0_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 77 of file RTE_Device.h.
| #define RTE_SPI0_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMux0LPSPI0Rx |
Definition at line 76 of file RTE_Device.h.
| #define RTE_SPI0_DMA_TX_CH 0 |
Definition at line 71 of file RTE_Device.h.
| #define RTE_SPI0_DMA_TX_DMA_BASE DMA0 |
Definition at line 74 of file RTE_Device.h.
| #define RTE_SPI0_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 73 of file RTE_Device.h.
| #define RTE_SPI0_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMux0LPSPI0Tx |
Definition at line 72 of file RTE_Device.h.
| #define RTE_SPI0_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs2) |
Definition at line 69 of file RTE_Device.h.
| #define RTE_SPI0_PCS_TO_SCK_DELAY 1000 |
Definition at line 66 of file RTE_Device.h.
| #define RTE_SPI0_SCK_TO_PSC_DELAY 1000 |
Definition at line 67 of file RTE_Device.h.
| #define RTE_SPI0_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs2) |
Definition at line 70 of file RTE_Device.h.
| #define RTE_USART0 1 |
Definition at line 18 of file RTE_Device.h.
| #define RTE_USART0_DMA_EN 0 |
Definition at line 19 of file RTE_Device.h.
| #define RTE_USART0_DMA_RX_CH 1 |
Definition at line 32 of file RTE_Device.h.
| #define RTE_USART0_DMA_RX_DMA_BASE DMA0 |
Definition at line 35 of file RTE_Device.h.
| #define RTE_USART0_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 34 of file RTE_Device.h.
| #define RTE_USART0_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMux0LPUART0Rx |
Definition at line 33 of file RTE_Device.h.
| #define RTE_USART0_DMA_TX_CH 0 |
Definition at line 28 of file RTE_Device.h.
| #define RTE_USART0_DMA_TX_DMA_BASE DMA0 |
Definition at line 31 of file RTE_Device.h.
| #define RTE_USART0_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 30 of file RTE_Device.h.
| #define RTE_USART0_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMux0LPUART0Tx |
Definition at line 29 of file RTE_Device.h.
| #define RTE_USART1 1 |
Definition at line 20 of file RTE_Device.h.
| #define RTE_USART1_DMA_EN 0 |
Definition at line 21 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_CH 1 |
Definition at line 41 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_DMA_BASE DMA0 |
Definition at line 44 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 43 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMux0LPUART1Rx |
Definition at line 42 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_CH 0 |
Definition at line 37 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_DMA_BASE DMA0 |
Definition at line 40 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 39 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMux0LPUART1Tx |
Definition at line 38 of file RTE_Device.h.
| #define USART0_RX_BUFFER_ENABLE 1 |
Definition at line 25 of file RTE_Device.h.
| #define USART1_RX_BUFFER_ENABLE 1 |
Definition at line 26 of file RTE_Device.h.
| #define USART_RX_BUFFER_LEN 64 |
Definition at line 24 of file RTE_Device.h.