![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
| #define RTE_I2C1 1 |
Definition at line 13 of file RTE_Device.h.
| #define RTE_I2C1_DMA_EN 0 |
Definition at line 14 of file RTE_Device.h.
| #define RTE_I2C1_DMA_RX_CH 1 |
Definition at line 69 of file RTE_Device.h.
| #define RTE_I2C1_DMA_RX_DMA_BASE DMA0 |
Definition at line 72 of file RTE_Device.h.
| #define RTE_I2C1_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 71 of file RTE_Device.h.
| #define RTE_I2C1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C1 |
Definition at line 70 of file RTE_Device.h.
| #define RTE_I2C1_DMA_TX_CH 0 |
Definition at line 65 of file RTE_Device.h.
| #define RTE_I2C1_DMA_TX_DMA_BASE DMA0 |
Definition at line 68 of file RTE_Device.h.
| #define RTE_I2C1_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 67 of file RTE_Device.h.
| #define RTE_I2C1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C1 |
Definition at line 66 of file RTE_Device.h.
| #define RTE_I2C2 0 |
Definition at line 15 of file RTE_Device.h.
| #define RTE_I2C2_DMA_EN 0 |
Definition at line 16 of file RTE_Device.h.
| #define RTE_I2C2_DMA_RX_CH 3 |
Definition at line 78 of file RTE_Device.h.
| #define RTE_I2C2_DMA_RX_DMA_BASE DMA0 |
Definition at line 81 of file RTE_Device.h.
| #define RTE_I2C2_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 80 of file RTE_Device.h.
| #define RTE_I2C2_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C2 |
Definition at line 79 of file RTE_Device.h.
| #define RTE_I2C2_DMA_TX_CH 2 |
Definition at line 74 of file RTE_Device.h.
| #define RTE_I2C2_DMA_TX_DMA_BASE DMA0 |
Definition at line 77 of file RTE_Device.h.
| #define RTE_I2C2_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 76 of file RTE_Device.h.
| #define RTE_I2C2_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C2 |
Definition at line 75 of file RTE_Device.h.
| #define RTE_I2C3 0 |
Definition at line 17 of file RTE_Device.h.
| #define RTE_I2C3_DMA_EN 0 |
Definition at line 18 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_CH 5 |
Definition at line 87 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_DMA_BASE DMA0 |
Definition at line 90 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 89 of file RTE_Device.h.
| #define RTE_I2C3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C3 |
Definition at line 88 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_CH 4 |
Definition at line 83 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_DMA_BASE DMA0 |
Definition at line 86 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 85 of file RTE_Device.h.
| #define RTE_I2C3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C3 |
Definition at line 84 of file RTE_Device.h.
| #define RTE_I2C4 0 |
Definition at line 19 of file RTE_Device.h.
| #define RTE_I2C4_DMA_EN 0 |
Definition at line 20 of file RTE_Device.h.
| #define RTE_I2C4_DMA_RX_CH 7 |
Definition at line 96 of file RTE_Device.h.
| #define RTE_I2C4_DMA_RX_DMA_BASE DMA0 |
Definition at line 99 of file RTE_Device.h.
| #define RTE_I2C4_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 98 of file RTE_Device.h.
| #define RTE_I2C4_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C4 |
Definition at line 97 of file RTE_Device.h.
| #define RTE_I2C4_DMA_TX_CH 6 |
Definition at line 92 of file RTE_Device.h.
| #define RTE_I2C4_DMA_TX_DMA_BASE DMA0 |
Definition at line 95 of file RTE_Device.h.
| #define RTE_I2C4_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 94 of file RTE_Device.h.
| #define RTE_I2C4_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C4 |
Definition at line 93 of file RTE_Device.h.
| #define RTE_I2C5 0 |
Definition at line 21 of file RTE_Device.h.
| #define RTE_I2C5_DMA_EN 0 |
Definition at line 22 of file RTE_Device.h.
| #define RTE_I2C5_DMA_RX_CH 9 |
Definition at line 105 of file RTE_Device.h.
| #define RTE_I2C5_DMA_RX_DMA_BASE DMA0 |
Definition at line 108 of file RTE_Device.h.
| #define RTE_I2C5_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 107 of file RTE_Device.h.
| #define RTE_I2C5_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C5 |
Definition at line 106 of file RTE_Device.h.
| #define RTE_I2C5_DMA_TX_CH 8 |
Definition at line 101 of file RTE_Device.h.
| #define RTE_I2C5_DMA_TX_DMA_BASE DMA0 |
Definition at line 104 of file RTE_Device.h.
| #define RTE_I2C5_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 103 of file RTE_Device.h.
| #define RTE_I2C5_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C5 |
Definition at line 102 of file RTE_Device.h.
| #define RTE_I2C6 0 |
Definition at line 23 of file RTE_Device.h.
| #define RTE_I2C6_DMA_EN 0 |
Definition at line 24 of file RTE_Device.h.
| #define RTE_I2C6_DMA_RX_CH 11 |
Definition at line 114 of file RTE_Device.h.
| #define RTE_I2C6_DMA_RX_DMA_BASE DMA0 |
Definition at line 117 of file RTE_Device.h.
| #define RTE_I2C6_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 116 of file RTE_Device.h.
| #define RTE_I2C6_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C6 |
Definition at line 115 of file RTE_Device.h.
| #define RTE_I2C6_DMA_TX_CH 10 |
Definition at line 110 of file RTE_Device.h.
| #define RTE_I2C6_DMA_TX_DMA_BASE DMA0 |
Definition at line 113 of file RTE_Device.h.
| #define RTE_I2C6_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 112 of file RTE_Device.h.
| #define RTE_I2C6_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C6 |
Definition at line 111 of file RTE_Device.h.
| #define RTE_SPI1 1 |
Definition at line 26 of file RTE_Device.h.
| #define RTE_SPI1_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 122 of file RTE_Device.h.
| #define RTE_SPI1_DMA_EN 0 |
Definition at line 27 of file RTE_Device.h.
| #define RTE_SPI1_DMA_RX_CH 1 |
Definition at line 129 of file RTE_Device.h.
| #define RTE_SPI1_DMA_RX_DMA_BASE DMA0 |
Definition at line 132 of file RTE_Device.h.
| #define RTE_SPI1_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 131 of file RTE_Device.h.
| #define RTE_SPI1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI1Rx |
Definition at line 130 of file RTE_Device.h.
| #define RTE_SPI1_DMA_TX_CH 0 |
Definition at line 125 of file RTE_Device.h.
| #define RTE_SPI1_DMA_TX_DMA_BASE DMA0 |
Definition at line 128 of file RTE_Device.h.
| #define RTE_SPI1_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 127 of file RTE_Device.h.
| #define RTE_SPI1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI1Tx |
Definition at line 126 of file RTE_Device.h.
| #define RTE_SPI1_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 123 of file RTE_Device.h.
| #define RTE_SPI1_PCS_TO_SCK_DELAY 1000 |
Definition at line 120 of file RTE_Device.h.
| #define RTE_SPI1_SCK_TO_PSC_DELAY 1000 |
Definition at line 121 of file RTE_Device.h.
| #define RTE_SPI1_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 124 of file RTE_Device.h.
| #define RTE_SPI2 0 |
Definition at line 28 of file RTE_Device.h.
| #define RTE_SPI2_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 136 of file RTE_Device.h.
| #define RTE_SPI2_DMA_EN 0 |
Definition at line 29 of file RTE_Device.h.
| #define RTE_SPI2_DMA_RX_CH 3 |
Definition at line 143 of file RTE_Device.h.
| #define RTE_SPI2_DMA_RX_DMA_BASE DMA0 |
Definition at line 146 of file RTE_Device.h.
| #define RTE_SPI2_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 145 of file RTE_Device.h.
| #define RTE_SPI2_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI2Tx |
Definition at line 144 of file RTE_Device.h.
| #define RTE_SPI2_DMA_TX_CH 2 |
Definition at line 139 of file RTE_Device.h.
| #define RTE_SPI2_DMA_TX_DMA_BASE DMA0 |
Definition at line 142 of file RTE_Device.h.
| #define RTE_SPI2_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 141 of file RTE_Device.h.
| #define RTE_SPI2_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI2Tx |
Definition at line 140 of file RTE_Device.h.
| #define RTE_SPI2_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 137 of file RTE_Device.h.
| #define RTE_SPI2_PCS_TO_SCK_DELAY 1000 |
Definition at line 134 of file RTE_Device.h.
| #define RTE_SPI2_SCK_TO_PSC_DELAY 1000 |
Definition at line 135 of file RTE_Device.h.
| #define RTE_SPI2_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 138 of file RTE_Device.h.
| #define RTE_SPI3 0 |
Definition at line 30 of file RTE_Device.h.
| #define RTE_SPI3_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 150 of file RTE_Device.h.
| #define RTE_SPI3_DMA_EN 0 |
Definition at line 31 of file RTE_Device.h.
| #define RTE_SPI3_DMA_RX_CH 5 |
Definition at line 157 of file RTE_Device.h.
| #define RTE_SPI3_DMA_RX_DMA_BASE DMA0 |
Definition at line 160 of file RTE_Device.h.
| #define RTE_SPI3_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 159 of file RTE_Device.h.
| #define RTE_SPI3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI3Rx |
Definition at line 158 of file RTE_Device.h.
| #define RTE_SPI3_DMA_TX_CH 4 |
Definition at line 153 of file RTE_Device.h.
| #define RTE_SPI3_DMA_TX_DMA_BASE DMA0 |
Definition at line 156 of file RTE_Device.h.
| #define RTE_SPI3_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 155 of file RTE_Device.h.
| #define RTE_SPI3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI3Tx |
Definition at line 154 of file RTE_Device.h.
| #define RTE_SPI3_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 151 of file RTE_Device.h.
| #define RTE_SPI3_PCS_TO_SCK_DELAY 1000 |
Definition at line 148 of file RTE_Device.h.
| #define RTE_SPI3_SCK_TO_PSC_DELAY 1000 |
Definition at line 149 of file RTE_Device.h.
| #define RTE_SPI3_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 152 of file RTE_Device.h.
| #define RTE_SPI4 0 |
Definition at line 32 of file RTE_Device.h.
| #define RTE_SPI4_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 164 of file RTE_Device.h.
| #define RTE_SPI4_DMA_EN 0 |
Definition at line 33 of file RTE_Device.h.
| #define RTE_SPI4_DMA_RX_CH 7 |
Definition at line 171 of file RTE_Device.h.
| #define RTE_SPI4_DMA_RX_DMA_BASE DMA0 |
Definition at line 174 of file RTE_Device.h.
| #define RTE_SPI4_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 173 of file RTE_Device.h.
| #define RTE_SPI4_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI4Rx |
Definition at line 172 of file RTE_Device.h.
| #define RTE_SPI4_DMA_TX_CH 6 |
Definition at line 167 of file RTE_Device.h.
| #define RTE_SPI4_DMA_TX_DMA_BASE DMA0 |
Definition at line 170 of file RTE_Device.h.
| #define RTE_SPI4_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 169 of file RTE_Device.h.
| #define RTE_SPI4_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI4Tx |
Definition at line 168 of file RTE_Device.h.
| #define RTE_SPI4_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 165 of file RTE_Device.h.
| #define RTE_SPI4_PCS_TO_SCK_DELAY 1000 |
Definition at line 162 of file RTE_Device.h.
| #define RTE_SPI4_SCK_TO_PSC_DELAY 1000 |
Definition at line 163 of file RTE_Device.h.
| #define RTE_SPI4_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 166 of file RTE_Device.h.
| #define RTE_SPI5 0 |
Definition at line 34 of file RTE_Device.h.
| #define RTE_SPI5_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 178 of file RTE_Device.h.
| #define RTE_SPI5_DMA_EN 0 |
Definition at line 35 of file RTE_Device.h.
| #define RTE_SPI5_DMA_RX_CH 9 |
Definition at line 185 of file RTE_Device.h.
| #define RTE_SPI5_DMA_RX_DMA_BASE DMA0 |
Definition at line 188 of file RTE_Device.h.
| #define RTE_SPI5_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 187 of file RTE_Device.h.
| #define RTE_SPI5_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI5Rx |
Definition at line 186 of file RTE_Device.h.
| #define RTE_SPI5_DMA_TX_CH 8 |
Definition at line 181 of file RTE_Device.h.
| #define RTE_SPI5_DMA_TX_DMA_BASE DMA0 |
Definition at line 184 of file RTE_Device.h.
| #define RTE_SPI5_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 183 of file RTE_Device.h.
| #define RTE_SPI5_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI5Tx |
Definition at line 182 of file RTE_Device.h.
| #define RTE_SPI5_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 179 of file RTE_Device.h.
| #define RTE_SPI5_PCS_TO_SCK_DELAY 1000 |
Definition at line 176 of file RTE_Device.h.
| #define RTE_SPI5_SCK_TO_PSC_DELAY 1000 |
Definition at line 177 of file RTE_Device.h.
| #define RTE_SPI5_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 180 of file RTE_Device.h.
| #define RTE_SPI6 0 |
Definition at line 36 of file RTE_Device.h.
| #define RTE_SPI6_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 192 of file RTE_Device.h.
| #define RTE_SPI6_DMA_EN 0 |
Definition at line 37 of file RTE_Device.h.
| #define RTE_SPI6_DMA_RX_CH 11 |
Definition at line 199 of file RTE_Device.h.
| #define RTE_SPI6_DMA_RX_DMA_BASE DMA0 |
Definition at line 202 of file RTE_Device.h.
| #define RTE_SPI6_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 201 of file RTE_Device.h.
| #define RTE_SPI6_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI6Rx |
Definition at line 200 of file RTE_Device.h.
| #define RTE_SPI6_DMA_TX_CH 10 |
Definition at line 195 of file RTE_Device.h.
| #define RTE_SPI6_DMA_TX_DMA_BASE DMA0 |
Definition at line 198 of file RTE_Device.h.
| #define RTE_SPI6_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 197 of file RTE_Device.h.
| #define RTE_SPI6_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI6Tx |
Definition at line 196 of file RTE_Device.h.
| #define RTE_SPI6_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 193 of file RTE_Device.h.
| #define RTE_SPI6_PCS_TO_SCK_DELAY 1000 |
Definition at line 190 of file RTE_Device.h.
| #define RTE_SPI6_SCK_TO_PSC_DELAY 1000 |
Definition at line 191 of file RTE_Device.h.
| #define RTE_SPI6_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 194 of file RTE_Device.h.
| #define RTE_USART1 1 |
Definition at line 39 of file RTE_Device.h.
| #define RTE_USART10 0 |
Definition at line 57 of file RTE_Device.h.
| #define RTE_USART10_DMA_EN 0 |
Definition at line 58 of file RTE_Device.h.
| #define RTE_USART10_DMA_RX_CH 19 |
Definition at line 290 of file RTE_Device.h.
| #define RTE_USART10_DMA_RX_DMA_BASE DMA0 |
Definition at line 293 of file RTE_Device.h.
| #define RTE_USART10_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 292 of file RTE_Device.h.
| #define RTE_USART10_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART10Rx |
Definition at line 291 of file RTE_Device.h.
| #define RTE_USART10_DMA_TX_CH 18 |
Definition at line 286 of file RTE_Device.h.
| #define RTE_USART10_DMA_TX_DMA_BASE DMA0 |
Definition at line 289 of file RTE_Device.h.
| #define RTE_USART10_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 288 of file RTE_Device.h.
| #define RTE_USART10_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART10Tx |
Definition at line 287 of file RTE_Device.h.
| #define RTE_USART11 0 |
Definition at line 59 of file RTE_Device.h.
| #define RTE_USART11_DMA_EN 0 |
Definition at line 60 of file RTE_Device.h.
| #define RTE_USART11_DMA_RX_CH 21 |
Definition at line 299 of file RTE_Device.h.
| #define RTE_USART11_DMA_RX_DMA_BASE DMA0 |
Definition at line 302 of file RTE_Device.h.
| #define RTE_USART11_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 301 of file RTE_Device.h.
| #define RTE_USART11_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART11Rx |
Definition at line 300 of file RTE_Device.h.
| #define RTE_USART11_DMA_TX_CH 20 |
Definition at line 295 of file RTE_Device.h.
| #define RTE_USART11_DMA_TX_DMA_BASE DMA0 |
Definition at line 298 of file RTE_Device.h.
| #define RTE_USART11_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 297 of file RTE_Device.h.
| #define RTE_USART11_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART11Tx |
Definition at line 296 of file RTE_Device.h.
| #define RTE_USART12 0 |
Definition at line 61 of file RTE_Device.h.
| #define RTE_USART12_DMA_EN 0 |
Definition at line 62 of file RTE_Device.h.
| #define RTE_USART12_DMA_RX_CH 23 |
Definition at line 308 of file RTE_Device.h.
| #define RTE_USART12_DMA_RX_DMA_BASE DMA0 |
Definition at line 311 of file RTE_Device.h.
| #define RTE_USART12_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 310 of file RTE_Device.h.
| #define RTE_USART12_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART12Rx |
Definition at line 309 of file RTE_Device.h.
| #define RTE_USART12_DMA_TX_CH 22 |
Definition at line 304 of file RTE_Device.h.
| #define RTE_USART12_DMA_TX_DMA_BASE DMA0 |
Definition at line 307 of file RTE_Device.h.
| #define RTE_USART12_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 306 of file RTE_Device.h.
| #define RTE_USART12_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART12Tx |
Definition at line 305 of file RTE_Device.h.
| #define RTE_USART1_DMA_EN 1 |
Definition at line 40 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_CH 1 |
Definition at line 209 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_DMA_BASE DMA0 |
Definition at line 212 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 211 of file RTE_Device.h.
| #define RTE_USART1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART1Rx |
Definition at line 210 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_CH 0 |
Definition at line 205 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_DMA_BASE DMA0 |
Definition at line 208 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 207 of file RTE_Device.h.
| #define RTE_USART1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART1Tx |
Definition at line 206 of file RTE_Device.h.
| #define RTE_USART2 0 |
Definition at line 41 of file RTE_Device.h.
| #define RTE_USART2_DMA_EN 0 |
Definition at line 42 of file RTE_Device.h.
| #define RTE_USART2_DMA_RX_CH 3 |
Definition at line 218 of file RTE_Device.h.
| #define RTE_USART2_DMA_RX_DMA_BASE DMA0 |
Definition at line 221 of file RTE_Device.h.
| #define RTE_USART2_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 220 of file RTE_Device.h.
| #define RTE_USART2_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART2Rx |
Definition at line 219 of file RTE_Device.h.
| #define RTE_USART2_DMA_TX_CH 2 |
Definition at line 214 of file RTE_Device.h.
| #define RTE_USART2_DMA_TX_DMA_BASE DMA0 |
Definition at line 217 of file RTE_Device.h.
| #define RTE_USART2_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 216 of file RTE_Device.h.
| #define RTE_USART2_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART2Tx |
Definition at line 215 of file RTE_Device.h.
| #define RTE_USART3 0 |
Definition at line 43 of file RTE_Device.h.
| #define RTE_USART3_DMA_EN 0 |
Definition at line 44 of file RTE_Device.h.
| #define RTE_USART3_DMA_RX_CH 5 |
Definition at line 227 of file RTE_Device.h.
| #define RTE_USART3_DMA_RX_DMA_BASE DMA0 |
Definition at line 230 of file RTE_Device.h.
| #define RTE_USART3_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 229 of file RTE_Device.h.
| #define RTE_USART3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART3Rx |
Definition at line 228 of file RTE_Device.h.
| #define RTE_USART3_DMA_TX_CH 4 |
Definition at line 223 of file RTE_Device.h.
| #define RTE_USART3_DMA_TX_DMA_BASE DMA0 |
Definition at line 226 of file RTE_Device.h.
| #define RTE_USART3_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 225 of file RTE_Device.h.
| #define RTE_USART3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART3Tx |
Definition at line 224 of file RTE_Device.h.
| #define RTE_USART4 0 |
Definition at line 45 of file RTE_Device.h.
| #define RTE_USART4_DMA_EN 0 |
Definition at line 46 of file RTE_Device.h.
| #define RTE_USART4_DMA_RX_CH 7 |
Definition at line 236 of file RTE_Device.h.
| #define RTE_USART4_DMA_RX_DMA_BASE DMA0 |
Definition at line 239 of file RTE_Device.h.
| #define RTE_USART4_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 238 of file RTE_Device.h.
| #define RTE_USART4_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART4Rx |
Definition at line 237 of file RTE_Device.h.
| #define RTE_USART4_DMA_TX_CH 6 |
Definition at line 232 of file RTE_Device.h.
| #define RTE_USART4_DMA_TX_DMA_BASE DMA0 |
Definition at line 235 of file RTE_Device.h.
| #define RTE_USART4_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 234 of file RTE_Device.h.
| #define RTE_USART4_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART4Tx |
Definition at line 233 of file RTE_Device.h.
| #define RTE_USART5 0 |
Definition at line 47 of file RTE_Device.h.
| #define RTE_USART5_DMA_EN 0 |
Definition at line 48 of file RTE_Device.h.
| #define RTE_USART5_DMA_RX_CH 9 |
Definition at line 245 of file RTE_Device.h.
| #define RTE_USART5_DMA_RX_DMA_BASE DMA0 |
Definition at line 248 of file RTE_Device.h.
| #define RTE_USART5_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 247 of file RTE_Device.h.
| #define RTE_USART5_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART5Rx |
Definition at line 246 of file RTE_Device.h.
| #define RTE_USART5_DMA_TX_CH 8 |
Definition at line 241 of file RTE_Device.h.
| #define RTE_USART5_DMA_TX_DMA_BASE DMA0 |
Definition at line 244 of file RTE_Device.h.
| #define RTE_USART5_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 243 of file RTE_Device.h.
| #define RTE_USART5_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART5Tx |
Definition at line 242 of file RTE_Device.h.
| #define RTE_USART6 0 |
Definition at line 49 of file RTE_Device.h.
| #define RTE_USART6_DMA_EN 0 |
Definition at line 50 of file RTE_Device.h.
| #define RTE_USART6_DMA_RX_CH 11 |
Definition at line 254 of file RTE_Device.h.
| #define RTE_USART6_DMA_RX_DMA_BASE DMA0 |
Definition at line 257 of file RTE_Device.h.
| #define RTE_USART6_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 256 of file RTE_Device.h.
| #define RTE_USART6_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART6Rx |
Definition at line 255 of file RTE_Device.h.
| #define RTE_USART6_DMA_TX_CH 10 |
Definition at line 250 of file RTE_Device.h.
| #define RTE_USART6_DMA_TX_DMA_BASE DMA0 |
Definition at line 253 of file RTE_Device.h.
| #define RTE_USART6_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 252 of file RTE_Device.h.
| #define RTE_USART6_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART6Tx |
Definition at line 251 of file RTE_Device.h.
| #define RTE_USART7 0 |
Definition at line 51 of file RTE_Device.h.
| #define RTE_USART7_DMA_EN 0 |
Definition at line 52 of file RTE_Device.h.
| #define RTE_USART7_DMA_RX_CH 13 |
Definition at line 263 of file RTE_Device.h.
| #define RTE_USART7_DMA_RX_DMA_BASE DMA0 |
Definition at line 266 of file RTE_Device.h.
| #define RTE_USART7_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 265 of file RTE_Device.h.
| #define RTE_USART7_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART7Rx |
Definition at line 264 of file RTE_Device.h.
| #define RTE_USART7_DMA_TX_CH 12 |
Definition at line 259 of file RTE_Device.h.
| #define RTE_USART7_DMA_TX_DMA_BASE DMA0 |
Definition at line 262 of file RTE_Device.h.
| #define RTE_USART7_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 261 of file RTE_Device.h.
| #define RTE_USART7_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART7Tx |
Definition at line 260 of file RTE_Device.h.
| #define RTE_USART8 0 |
Definition at line 53 of file RTE_Device.h.
| #define RTE_USART8_DMA_EN 0 |
Definition at line 54 of file RTE_Device.h.
| #define RTE_USART8_DMA_RX_CH 15 |
Definition at line 272 of file RTE_Device.h.
| #define RTE_USART8_DMA_RX_DMA_BASE DMA0 |
Definition at line 275 of file RTE_Device.h.
| #define RTE_USART8_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 274 of file RTE_Device.h.
| #define RTE_USART8_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART8Rx |
Definition at line 273 of file RTE_Device.h.
| #define RTE_USART8_DMA_TX_CH 14 |
Definition at line 268 of file RTE_Device.h.
| #define RTE_USART8_DMA_TX_DMA_BASE DMA0 |
Definition at line 271 of file RTE_Device.h.
| #define RTE_USART8_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 270 of file RTE_Device.h.
| #define RTE_USART8_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART8Tx |
Definition at line 269 of file RTE_Device.h.
| #define RTE_USART9 0 |
Definition at line 55 of file RTE_Device.h.
| #define RTE_USART9_DMA_EN 0 |
Definition at line 56 of file RTE_Device.h.
| #define RTE_USART9_DMA_RX_CH 17 |
Definition at line 281 of file RTE_Device.h.
| #define RTE_USART9_DMA_RX_DMA_BASE DMA0 |
Definition at line 284 of file RTE_Device.h.
| #define RTE_USART9_DMA_RX_DMAMUX_BASE DMAMUX0 |
Definition at line 283 of file RTE_Device.h.
| #define RTE_USART9_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART9Rx |
Definition at line 282 of file RTE_Device.h.
| #define RTE_USART9_DMA_TX_CH 16 |
Definition at line 277 of file RTE_Device.h.
| #define RTE_USART9_DMA_TX_DMA_BASE DMA0 |
Definition at line 280 of file RTE_Device.h.
| #define RTE_USART9_DMA_TX_DMAMUX_BASE DMAMUX0 |
Definition at line 279 of file RTE_Device.h.
| #define RTE_USART9_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART9Tx |
Definition at line 278 of file RTE_Device.h.