18 #define GPIO_DRV_VERSION ARM_DRIVER_VERSION_MAJOR_MINOR(2, 3)     20 #define GPIO_NUMBER_OF_PIN 0x20    30     .
pinConfig = {kGPIO_DigitalInput, 0}, .interruptMode = kGPIO_IntLowLevel};
    58     if (NULL == apPinConfig)
    60         pGpioConfig = &gpioConfigDefault;
    71         EnableIRQ(pinHandle->
irq);
    75         GPIO_PortEnableInterrupts(pinHandle->
base, pinHandle->
mask);
   135     GPIO_WritePinOutput(pinHandle->
base, pinHandle->
pinNumber, aValue);
   147     return GPIO_ReadPinInput(pinHandle->
base, pinHandle->
pinNumber);
   158     uint32_t isfr = GPIO_GetPinsInterruptFlags(apBase);
   171             handle(isrObj[gpioPortNumber][i].pUserData);
   172             GPIO_ClearPinsInterruptFlags(apBase, (1 << i));
 uint32_t imxsdk_gpio_read_pin(pinID_t aPinId)
 
The GPIO Pin Configuration i.MX SDK. 
 
void imxsdk_gpio_set_pin(pinID_t aPinId)
 
gpio_pin_config_t pinConfig
 
void(* gpio_isr_handler_t)(void *apUserData)
 
Access structure of the GPIO Driver. 
 
void * pinID_t
GPIO Driver direction. 
 
void imxsdk_gpio_toggle_pin(pinID_t aPinId)
 
#define GPIO_NUMBER_OF_PIN
 
void imxsdk_gpio_clr_pin(pinID_t aPinId)
 
void imxsdk_gpio_pin_init(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
 
gpio_isr_handler_t isrHandle
 
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
 
enum gpio_direction_en gpio_direction_t
 
ARM_DRIVER_VERSION GENERIC_DRIVER_VERSION
 
GENERIC_DRIVER_VERSION imxsdk_gpio_get_version(void)
 
void imxsdk_gpio_handle_interrupt(GPIO_Type *apBase, port_number_t gpioPortNumber)
 
enum port_number port_number_t
GPIO PORT NAMES. 
 
The GPIO pin handle for i.MX SDK. 
 
void imxsdk_gpio_write_pin(pinID_t aPinId, uint8_t aValue)