![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
Access structure of the GPIO Driver. More...
#include <Driver_GPIO.h>

Data Fields | |
| GENERIC_DRIVER_VERSION(* | GetVersion )(void) |
| void(* | pin_init )(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData) |
| void(* | set_pin )(pinID_t aPinId) |
| void(* | clr_pin )(pinID_t aPinId) |
| void(* | toggle_pin )(pinID_t aPinId) |
| void(* | write_pin )(pinID_t aPinId, uint8_t aValue) |
| uint32_t(* | read_pin )(pinID_t aPinId) |
Access structure of the GPIO Driver.
Definition at line 38 of file Driver_GPIO.h.
| void(* clr_pin) (pinID_t aPinId) |
Pointer to clear the pin.
Definition at line 47 of file Driver_GPIO.h.
Referenced by ADS_InitSPI_DIFF_P(), ADS_InitSPI_FXLS8471(), ADS_InitSPI_FXLS8962(), FXAS21002_SPI_Initialize(), fxlc95000_enSensor(), FXLC95000_SPI_Initialize(), FXLS8471Q_SPI_Initialize(), FXLS8962_SPI_Initialize(), FXLS896x_SPI_Initialize(), FXLS8974_SPI_Initialize(), FXOS8700_SPI_Initialize(), main(), MMA9553_SPI_Initialize(), process_host_command(), and register_spi_control().
| GENERIC_DRIVER_VERSION(* GetVersion) (void) |
Pointer to get driver version.
Definition at line 40 of file Driver_GPIO.h.
| void(* pin_init) (pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData) |
Pointer to Initialize gpio Interface.
Definition at line 41 of file Driver_GPIO.h.
Referenced by ADS_DetectShield(), ADS_InitSPI_DIFF_P(), ADS_InitSPI_FXLS8471(), ADS_InitSPI_FXLS8962(), FXAS21002_SPI_Initialize(), FXLC95000_SPI_Initialize(), FXLS8471Q_Init(), FXLS8471Q_SPI_Initialize(), FXLS8962_SPI_Initialize(), FXLS896x_SPI_Initialize(), FXLS8974_SPI_Initialize(), FXOS8700_SPI_Initialize(), main(), and MMA9553_SPI_Initialize().
| uint32_t(* read_pin) (pinID_t aPinId) |
| void(* set_pin) (pinID_t aPinId) |
Pointer to set the pin.
Definition at line 46 of file Driver_GPIO.h.
Referenced by ADS_DetectShield(), ADS_InitSPI_DIFF_P(), ADS_InitSPI_FXLS8471(), ADS_InitSPI_FXLS8962(), FXAS21002_SPI_Initialize(), fxlc95000_enSensor(), FXLC95000_SPI_Initialize(), FXLS8471Q_SPI_Initialize(), FXLS8962_SPI_Initialize(), FXLS896x_SPI_Initialize(), FXLS8974_SPI_Initialize(), FXOS8700_SPI_Initialize(), main(), MMA9553_SPI_Initialize(), process_host_command(), and register_spi_control().
| void(* toggle_pin) (pinID_t aPinId) |
Pointer to toggle the pin.
Definition at line 48 of file Driver_GPIO.h.
Referenced by main(), and process_host_command().
| void(* write_pin) (pinID_t aPinId, uint8_t aValue) |
< read the pin value.
Definition at line 49 of file Driver_GPIO.h.