![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Modules | |
| Remote_auth_methods | |
| Remote_open_flags | |
| Remote_samp_methods | |
| Remote_source_ID | |
| Remote_source_string | |
| The formats allowed by the pcap_open() are the following: | |
Data Structures | |
| struct | pcap_rmtauth |
| This structure keeps the information needed to autheticate the user on a remote machine. More... | |
| struct | pcap_samp |
| This structure defines the information related to sampling. More... | |
Macros | |
| #define | PCAP_BUF_SIZE 1024 |
| Defines the maximum buffer size in which address, port, interface names are kept. More... | |
| #define | RPCAP_HOSTLIST_SIZE 1024 |
| Maximum lenght of an host name (needed for the RPCAP active mode) | |
| struct pcap_rmtauth |
The remote machine can either grant or refuse the access according to the information provided. In case the NULL authentication is required, both 'username' and 'password' can be NULL pointers.
This structure is meaningless if the source is not a remote interface; in that case, the functions which requires such a structure can accept a NULL pointer as well.
Data Fields | |
| int | type |
| Type of the authentication required. More... | |
| char * | username |
| Zero-terminated string containing the username that has to be used on the remote machine for authentication. More... | |
| char * | password |
| Zero-terminated string containing the password that has to be used on the remote machine for authentication. More... | |
| int pcap_rmtauth::type |
In order to provide maximum flexibility, we can support different types of authentication based on the value of this 'type' variable. The currently supported authentication methods are defined into the Remote Authentication Methods Section.
| char* pcap_rmtauth::username |
This field is meaningless in case of the RPCAP_RMTAUTH_NULL authentication and it can be NULL.
| char* pcap_rmtauth::password |
This field is meaningless in case of the RPCAP_RMTAUTH_NULL authentication and it can be NULL.
| struct pcap_samp |
In case the sampling is requested, the capturing device should read only a subset of the packets coming from the source. The returned packets depend on the sampling parameters.
Data Fields | |
| int | method |
| Method used for sampling. More... | |
| int | value |
| This value depends on the sampling method defined. More... | |
| int pcap_samp::method |
Currently, the supported methods are listed in the Sampling Methods Section.
| int pcap_samp::value |
For its meaning, please check at the Sampling Methods Section.
| #define PCAP_BUF_SIZE 1024 |
In case the adapter name or such is larger than this value, it is truncated. This is not used by the user; however it must be aware that an hostname / interface name longer than this value will be truncated.