![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | PCAP_SRC_FILE 2 |
| Internal representation of the type of source in use (file, remote/local interface). More... | |
| #define | PCAP_SRC_IFLOCAL 3 |
| Internal representation of the type of source in use (file, remote/local interface). More... | |
| #define | PCAP_SRC_IFREMOTE 4 |
| Internal representation of the type of source in use (file, remote/local interface). More... | |
| #define PCAP_SRC_FILE 2 |
This indicates a file, i.e. the user want to open a capture from a local file.
| #define PCAP_SRC_IFLOCAL 3 |
This indicates a local interface, i.e. the user want to open a capture from a local interface. This does not involve the RPCAP protocol.
| #define PCAP_SRC_IFREMOTE 4 |
This indicates a remote interface, i.e. the user want to open a capture from an interface on a remote host. This does involve the RPCAP protocol.