![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
#define | PCAP_SAMP_NOSAMP 0 |
No sampling has to be done on the current capture. More... | |
#define | PCAP_SAMP_1_EVERY_N 1 |
It defines that only 1 out of N packets must be returned to the user. More... | |
#define | PCAP_SAMP_FIRST_AFTER_N_MS 2 |
It defines that we have to return 1 packet every N milliseconds. More... | |
#define PCAP_SAMP_NOSAMP 0 |
In this case, no sampling algorithms are applied to the current capture.
#define PCAP_SAMP_1_EVERY_N 1 |
In this case, the 'value' field of the 'pcap_samp' structure indicates the number of packets (minus 1) that must be discarded before one packet got accepted. In other words, if 'value = 10', the first packet is returned to the caller, while the following 9 are discarded.
#define PCAP_SAMP_FIRST_AFTER_N_MS 2 |
In this case, the 'value' field of the 'pcap_samp' structure indicates the 'waiting time' in milliseconds before one packet got accepted. In other words, if 'value = 10', the first packet is returned to the caller; the next returned one will be the first packet that arrives when 10ms have elapsed.