![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | RPCAP_RMTAUTH_NULL 0 |
| It defines the NULL authentication. More... | |
| #define | RPCAP_RMTAUTH_PWD 1 |
| It defines the username/password authentication. More... | |
| #define RPCAP_RMTAUTH_NULL 0 |
This value has to be used within the 'type' member of the pcap_rmtauth structure. The 'NULL' authentication has to be equal to 'zero', so that old applications can just put every field of struct pcap_rmtauth to zero, and it does work.
| #define RPCAP_RMTAUTH_PWD 1 |
With this type of authentication, the RPCAP protocol will use the username/ password provided to authenticate the user on the remote machine. If the authentication is successful (and the user has the right to open network devices) the RPCAP connection will continue; otherwise it will be dropped.
This value has to be used within the 'type' member of the pcap_rmtauth structure.