MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Ftftx CACHE Driver

Data Structures

struct  ftfx_prefetch_speculation_status_t
 FTFx prefetch speculation status. More...
 
struct  ftfx_cache_config_t
 FTFx cache driver state information. More...
 

Enumerations

enum  _ftfx_cache_ram_func_constants { kFTFx_CACHE_RamFuncMaxSizeInWords = 16U }
 Constants for execute-in-RAM flash function. More...
 

Functions

status_t FTFx_CACHE_Init (ftfx_cache_config_t *config)
 Initializes the global FTFx cache structure members. More...
 
status_t FTFx_CACHE_ClearCachePrefetchSpeculation (ftfx_cache_config_t *config, bool isPreProcess)
 Process the cache/prefetch/speculation to the flash. More...
 
status_t FTFx_CACHE_PflashSetPrefetchSpeculation (ftfx_prefetch_speculation_status_t *speculationStatus)
 Sets the PFlash prefetch speculation to the intended speculation status. More...
 
status_t FTFx_CACHE_PflashGetPrefetchSpeculation (ftfx_prefetch_speculation_status_t *speculationStatus)
 Gets the PFlash prefetch speculation status. More...
 

FTFx cache version

#define FSL_FTFX_CACHE_DRIVER_VERSION   (MAKE_VERSION(3, 0, 0))
 Flexnvm driver version for SDK. More...
 

Detailed Description


Data Structure Documentation

struct ftfx_prefetch_speculation_status_t

Data Fields

bool instructionOff
 Instruction speculation. More...
 
bool dataOff
 Data speculation. More...
 

Field Documentation

bool ftfx_prefetch_speculation_status_t::instructionOff
bool ftfx_prefetch_speculation_status_t::dataOff
struct ftfx_cache_config_t

An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.

Data Fields

uint8_t flashMemoryIndex
 0 - primary flash; 1 - secondary flash
 
function_bit_operation_ptr_t bitOperFuncAddr
 An buffer point to the flash execute-in-RAM function. More...
 

Field Documentation

function_bit_operation_ptr_t ftfx_cache_config_t::bitOperFuncAddr

Macro Definition Documentation

#define FSL_FTFX_CACHE_DRIVER_VERSION   (MAKE_VERSION(3, 0, 0))

Version 1.0.0.

Enumeration Type Documentation

Enumerator
kFTFx_CACHE_RamFuncMaxSizeInWords 

The maximum size of execute-in-RAM function.

Function Documentation

status_t FTFx_CACHE_Init ( ftfx_cache_config_t *  config)

This function checks and initializes the Flash module for the other FTFx cache APIs.

Parameters
configPointer to the storage for the driver runtime state.
Return values
kStatus_FTFx_SuccessAPI was executed successfully.
kStatus_FTFx_InvalidArgumentAn invalid argument is provided.
kStatus_FTFx_ExecuteInRamFunctionNotReadyExecute-in-RAM function is not available.
status_t FTFx_CACHE_ClearCachePrefetchSpeculation ( ftfx_cache_config_t *  config,
bool  isPreProcess 
)
Parameters
configA pointer to the storage for the driver runtime state.
processThe possible option used to control flash cache/prefetch/speculation
Return values
kStatus_FTFx_SuccessAPI was executed successfully.
kStatus_FTFx_InvalidArgumentInvalid argument is provided.
kStatus_FTFx_ExecuteInRamFunctionNotReadyExecute-in-RAM function is not available.
status_t FTFx_CACHE_PflashSetPrefetchSpeculation ( ftfx_prefetch_speculation_status_t *  speculationStatus)
Parameters
speculationStatusThe expected protect status to set to the PFlash protection register. Each bit is
Return values
kStatus_FTFx_SuccessAPI was executed successfully.
kStatus_FTFx_InvalidSpeculationOptionAn invalid speculation option argument is provided.
status_t FTFx_CACHE_PflashGetPrefetchSpeculation ( ftfx_prefetch_speculation_status_t *  speculationStatus)
Parameters
speculationStatusSpeculation status returned by the PFlash IP.
Return values
kStatus_FTFx_SuccessAPI was executed successfully.