![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
| ADC16 channel conversion configuration | |
| ADC16 converter configuration | |
| ADC16 Hardware comparison configuration | |
| The callback message struct of button | |
| The button config structure | |
| The button gpio config structure | |
| Configures the comparator | |
| Configures the internal DAC | |
| Configures the filter | |
| CRC protocol configuration | |
| DAC buffer configuration | |
| DAC module configuration | |
| Dmamanager handle typedef | |
| EDMA channel priority configuration | |
| EDMA global configuration structure | |
| EDMA transfer handle structure | |
| EDMA minor offset configuration | |
| EDMA TCD | |
| EDMA transfer configuration | |
| Flash driver state information | |
| Define FlexIO Camera user configuration structure | |
| Camera eDMA handle | |
| Define FlexIO Camera transfer structure | |
| Define structure of configuring the FlexIO Camera device | |
| Define FlexIO user configuration structure | |
| Define FlexIO I2C master user configuration structure | |
| Define FlexIO I2C master handle structure | |
| Define FlexIO I2C master transfer structure | |
| Define FlexIO I2C master access structure typedef | |
| FlexIO I2S configure structure | |
| FlexIO I2S DMA transfer handle, users should not touch the content of the handle | |
| FlexIO I2S DMA transfer handle, users should not touch the content of the handle | |
| FlexIO I2S audio format, FlexIO I2S only support the same format in Tx and Rx | |
| Define FlexIO I2S handle structure | |
| Define FlexIO I2S transfer structure | |
| Define FlexIO I2S access structure typedef | |
| Define FlexIO MCULCD configuration structure | |
| FlexIO MCULCD DMA transfer handle, users should not touch the content of the handle | |
| FlexIO MCULCD eDMA transfer handle, users should not touch the content of the handle | |
| Define FlexIO MCULCD handle structure | |
| FlexIO MCULCD SMARTDMA configuration | |
| FlexIO MCULCD SMARTDMA transfer handle, users should not touch the content of the handle | |
| Define FlexIO MCULCD transfer structure | |
| Define FlexIO MCULCD access structure typedef | |
| Define FlexIO shifter configuration structure | |
| Define FlexIO SPI master configuration structure | |
| FlexIO SPI DMA transfer handle, users should not touch the content of the handle | |
| FlexIO SPI eDMA transfer handle, users should not touch the content of the handle | |
| Define FlexIO SPI handle structure | |
| Define FlexIO SPI slave configuration structure | |
| Define FlexIO SPI transfer structure | |
| Define FlexIO SPI access structure typedef | |
| Define FlexIO timer configuration structure | |
| Define FlexIO UART user configuration structure | |
| UART DMA handle | |
| UART eDMA handle | |
| Define FLEXIO UART handle structure | |
| Define FlexIO UART transfer structure | |
| Define FlexIO UART access structure typedef | |
| Flexnvm driver state information | |
| FTFx cache driver state information | |
| Flash driver state information | |
| Flash IFR memory descriptor | |
| Flash memory descriptor | |
| Active FTFx information for the current operation | |
| FTFx prefetch speculation status | |
| Ftfx special memory access information | |
| The GPIO pin configuration structure | |
| The pin config struct of GPIO adapter | |
| HAL timer configuration structure for HAL timer setting | |
| UART configuration structure | |
| UART transfer structure | |
| The config struct of LED | |
| The flash config struct of LED | |
| The pin config struct of monochrome LED | |
| The pin config struct of LED | |
| The pin config struct of rgb LED | |
| The list element | |
| The list structure | |
| An external input pin filter control structure | |
| IP parameter definition | |
| IP version ID definition | |
| LPI2C master data match configuration structure | |
| Structure with settings to initialize the LPI2C master module | |
| Driver handle for master DMA APIs | |
| Driver handle for master non-blocking APIs | |
| Non-blocking transfer descriptor structure | |
| Structure with settings to initialize the LPI2C slave module | |
| LPI2C slave handle structure | |
| LPI2C slave transfer structure | |
| Structure to configure the channel timer | |
| LPIT configuration structure | |
| LPSPI master configuration structure | |
| LPSPI master eDMA transfer handle structure used for transactional API | |
| LPSPI master transfer handle structure used for transactional API | |
| LPSPI slave configuration structure | |
| LPSPI slave eDMA transfer handle structure used for transactional API | |
| LPSPI slave transfer handle structure used for transactional API | |
| LPSPI master/slave transfer structure | |
| LPTMR config structure | |
| LPUART configuration structure | |
| LPUART DMA handle | |
| LPUART eDMA handle | |
| LPUART handle structure | |
| LPUART RTOS configuration structure | |
| LPUART transfer structure | |
| Callback configuration structure | |
| Notifier handle structure | |
| Notification block passed to the registered callback function | |
| Thread Definition structure contains startup information of a thread | |
| Thread Link Definition structure | |
| Definition structure contains timer parameters | |
| Panic data structure | |
| PFlash protection status | |
| Bandgap Buffer configuration | |
| High-voltage Detect Configuration Structure | |
| Low-voltage Detect Configuration Structure | |
| Low-voltage Warning Configuration Structure | |
| IP parameter definition | |
| IP version ID definition | |
| PORT pin configuration structure | |
| Reset pin filter configuration | |
| IP version ID definition | |
| RTC config structure | |
| Structure is used to hold the date and time | |
| Runtime RTOS Smart card driver context | |
| Sai bit clock configurations | |
| SAI user configuration structure | |
| SAI DMA transfer handle, users should not touch the content of the handle | |
| SAI DMA transfer handle, users should not touch the content of the handle | |
| Sai frame sync configurations | |
| SAI handle structure | |
| SAI DMA transfer handle, users should not touch the content of the handle | |
| Sai serial data configurations | |
| Sai transceiver configurations | |
| Sai transfer format | |
| SAI transfer structure | |
| SCG fast IRC clock configuration | |
| SCG fast IRC clock trim configuration | |
| SCG slow IRC clock configuration | |
| SCG system OSC configuration | |
| SCG system PLL configuration | |
| SCG system clock configuration | |
| Callback message structure | |
| Serial manager config structure | |
| Serial port swo config struct | |
| Serial port uart config struct | |
| Serial port usb config struct | |
| Serial port usb config struct | |
| User command data configuration structure | |
| Unique ID | |
| Defines card-specific parameters for Smart card driver | |
| Runtime state of the Smart card driver | |
| Defines user specified configuration of Smart card interface | |
| Smart card defines the state of the EMV timers in the Smart card driver | |
| Defines user transfer structure used to initialize transfer | |
| IP parameter definition | |
| SMC Low-Leakage Stop power mode configuration | |
| SMC Very Low-Leakage Stop power mode configuration | |
| IP version ID definition | |
| Timer config | |
| Options to configure a TPM channel's PWM signal | |
| TPM config structure | |
| TPM dual edge capture parameters | |
| TPM quadrature decode phase parameters | |
| Data structure for the TRNG initialization | |
| Data structure for definition of statistical check limits | |
| TSI calibration data storage | |
| TSI configuration structure | |
| The description structure for the VREF module | |
| Describes WDOG32 configuration structure | |
| Defines WDOG32 work mode |