MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
LED

Data Structures

struct  led_pin_config_t
 The pin config struct of LED. More...
 
struct  led_rgb_config_t
 The pin config struct of rgb LED. More...
 
struct  led_monochrome_config_t
 The pin config struct of monochrome LED. More...
 
struct  led_config_t
 The config struct of LED. More...
 
struct  led_flash_config_t
 The flash config struct of LED. More...
 

Macros

#define LED_DIMMING_ENABLEMENT   (0U)
 Definition to determine whether enable dimming. More...
 
#define LED_COLOR_WHEEL_ENABLEMENT   (0U)
 Definition to determine whether enable color wheel. More...
 
#define LED_HANDLE_SIZE   ((16U * 3U) + 36U)
 Definition of LED handle size. More...
 
#define LED_HANDLE_DEFINE(name)   uint32_t name[((LED_HANDLE_SIZE - 1U) >> 2U) + 1U];
 Defines the led handle buffer. More...
 
#define LED_TIMER_INTERVAL   (100U)
 Definition of LED timer interval,unit is ms. More...
 
#define LED_DIMMING_UPDATE_INTERVAL   (100U)
 Definition of LED dimming update interval,unit is ms. More...
 
#define LED_FLASH_CYCLE_FOREVER   (0xFFFFFFFFU)
 Definition of LED flash cycle forever. More...
 
#define LED_BLIP_INTERVAL   (250U)
 Definition of LED blip interval,unit is ms. More...
 
#define LED_MAKE_COLOR(r, g, b)   ((led_color_t)((((led_color_t)b) << 16) | (((led_color_t)g) << 8) | ((led_color_t)r)))
 Definition to set LED color. More...
 

Typedefs

typedef void * led_handle_t
 The handle of LED.
 
typedef uint32_t led_color_t
 The color struct of LED.
 

Enumerations

enum  led_status_t {
  kStatus_LED_Success = kStatus_Success,
  kStatus_LED_Error = MAKE_STATUS(kStatusGroup_LED, 1),
  kStatus_LED_InvalidParameter = MAKE_STATUS(kStatusGroup_LED, 2)
}
 The status type of LED. More...
 
enum  led_flash_type_t { kLED_FlashOneColor = 0x00U }
 The flash type of LED. More...
 
enum  _led_color {
  kLED_Black = LED_MAKE_COLOR(0, 0, 0),
  kLED_Red = LED_MAKE_COLOR(255, 0, 0),
  kLED_Green = LED_MAKE_COLOR(0, 255, 0),
  kLED_Yellow = LED_MAKE_COLOR(255, 255, 0),
  kLED_Blue = LED_MAKE_COLOR(0, 0, 255),
  kLED_Pink = LED_MAKE_COLOR(255, 0, 255),
  kLED_Aquamarine = LED_MAKE_COLOR(0, 255, 255),
  kLED_White = LED_MAKE_COLOR(255, 255, 255)
}
 The color type of LED. More...
 
enum  led_type_t {
  kLED_TypeRgb = 0x01U,
  kLED_TypeMonochrome = 0x02U
}
 The type of LED. More...
 

Functions

led_status_t LED_Init (led_handle_t ledHandle, led_config_t *ledConfig)
 Initializes a LED with the LED handle and the user configuration structure. More...
 
led_status_t LED_Deinit (led_handle_t ledHandle)
 Deinitializes a LED instance. More...
 
led_status_t LED_SetColor (led_handle_t ledHandle, led_color_t ledRgbColor)
 Sets the LED color. More...
 
led_status_t LED_TurnOnOff (led_handle_t ledHandle, uint8_t turnOnOff)
 Turns on or off the LED. More...
 
led_status_t LED_Blip (led_handle_t ledHandle)
 Blips the LED. More...
 
led_status_t LED_Flash (led_handle_t ledHandle, led_flash_config_t *ledFlash)
 Flashes the LED. More...
 
led_status_t LED_Dimming (led_handle_t ledHandle, uint16_t dimmingPeriod, uint8_t increasement)
 Adjusts the brightness of the LED. More...
 
led_status_t LED_EnterLowpower (led_handle_t ledHandle)
 Prepares to enter low power consumption. More...
 
led_status_t LED_ExitLowpower (led_handle_t ledHandle)
 Restores from low power consumption. More...
 

Detailed Description


Data Structure Documentation

struct led_pin_config_t

Data Fields

uint8_t dimmingEnable
 dimming enable, 0 - disable, 1 - enable
 
uint8_t port
 GPIO Port.
 
uint8_t pin
 GPIO Pin.
 
uint8_t pinStateDefault
 GPIO Pin voltage when LED is off (0 - low level, 1 - high level) More...
 
uint32_t sourceClock
 The clock source of the PWM module.
 
uint8_t instance
 PWM instance of the pin.
 
uint8_t channel
 PWM channel of the pin.
 

Field Documentation

uint8_t led_pin_config_t::pinStateDefault

The Pin voltage when LED is off (0 - low level, 1 - high level)

struct led_rgb_config_t

Data Fields

led_pin_config_t redPin
 Red pin setting.
 
led_pin_config_t greenPin
 Green pin setting.
 
led_pin_config_t bluePin
 Blue pin setting.
 
struct led_monochrome_config_t

Data Fields

led_pin_config_t monochromePin
 Monochrome pin setting.
 
struct led_config_t
struct led_flash_config_t

Data Fields

uint32_t times
 Flash times, LED_FLASH_CYCLE_FOREVER for forever.
 
uint16_t period
 Flash period, unit is ms.
 
led_flash_type_t flashType
 Flash type, one color or color wheel. More...
 
uint8_t duty
 Duty of the LED on for one period (duration = duty * period / 100). More...
 

Field Documentation

led_flash_type_t led_flash_config_t::flashType

Refer to led_flash_type_t

uint8_t led_flash_config_t::duty

Macro Definition Documentation

#define LED_DIMMING_ENABLEMENT   (0U)

Enable or disable the dimming feature

#define LED_COLOR_WHEEL_ENABLEMENT   (0U)

Enable or disable the color wheel feature

#define LED_HANDLE_SIZE   ((16U * 3U) + 36U)
#define LED_HANDLE_DEFINE (   name)    uint32_t name[((LED_HANDLE_SIZE - 1U) >> 2U) + 1U];

This macro is used to define a 4 byte aligned led handle buffer for led queue. Then uses the name to get the led handle buffer pointer.

The macro should be global and could be optional. You could also define led handle buffer by yourself.

This is an example,

* LED_HANDLE_DEFINE(ledHandle);
*
Parameters
nameThe name string of the led handle buffer.
#define LED_TIMER_INTERVAL   (100U)
#define LED_DIMMING_UPDATE_INTERVAL   (100U)
#define LED_FLASH_CYCLE_FOREVER   (0xFFFFFFFFU)
#define LED_BLIP_INTERVAL   (250U)
#define LED_MAKE_COLOR (   r,
  g,
  b 
)    ((led_color_t)((((led_color_t)b) << 16) | (((led_color_t)g) << 8) | ((led_color_t)r)))

Enumeration Type Documentation

Enumerator
kStatus_LED_Success 

Success.

kStatus_LED_Error 

Failed.

kStatus_LED_InvalidParameter 

Invalid parameter.

Enumerator
kLED_FlashOneColor 

Fast with one color.

enum _led_color
Enumerator
kLED_Black 

Black.

kLED_Red 

Red.

kLED_Green 

Green.

kLED_Yellow 

Yellow.

kLED_Blue 

Blue.

kLED_Pink 

Pink.

kLED_Aquamarine 

Aquamarine.

kLED_White 

White.

enum led_type_t
Enumerator
kLED_TypeRgb 

RGB LED.

kLED_TypeMonochrome 

Monochrome LED.

Function Documentation

led_status_t LED_Init ( led_handle_t  ledHandle,
led_config_t *  ledConfig 
)

This function configures the LED with user-defined settings. The user can configure the configuration structure. The parameter ledHandle is a pointer to point to a memory space of size LED_HANDLE_SIZE allocated by the caller. The LED supports two types LED, RGB and monochrome. Please refer to led_type_t. These two types can be set by using led_config_t. The LED also supports LED dimming mode.

Example below shows how to use this API to configure the LED. For monochrome LED,

* uint32_t s_ledMonochromeHandleBuffer[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1) / sizeof(uitn32_t))];
* led_handle_t s_ledMonochromeHandle = (led_handle_t)&s_ledMonochromeHandleBuffer[0];
* led_config_t ledMonochromeConfig;
* ledMonochromeConfig.type = kLED_TypeMonochrome;
* ledMonochromeConfig.ledMonochrome.monochromePin.dimmingEnable = 0;
* ledMonochromeConfig.ledMonochrome.monochromePin.gpio.port = 0;
* ledMonochromeConfig.ledMonochrome.monochromePin.gpio.pin = 1;
* ledMonochromeConfig.ledMonochrome.monochromePin.gpio.pinStateDefault = 0;
* LED_Init(s_ledMonochromeHandle, &ledMonochromeConfig);
*

For rgb LED,

* uint32_t s_ledRgbHandleBuffer[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1) / sizeof(uitn32_t))];
* led_handle_t s_ledRgbHandle = (led_handle_t)&s_ledRgbHandleBuffer[0];
* led_config_t ledRgbConfig;
* ledRgbConfig.type = kLED_TypeRgb;
* ledRgbConfig.ledRgb.redPin.dimmingEnable = 0;
* ledRgbConfig.ledRgb.redPin.gpio.port = 0;
* ledRgbConfig.ledRgb.redPin.gpio.pin = 1;
* ledRgbConfig.ledRgb.redPin.gpio.pinStateDefault = 0;
* ledRgbConfig.ledRgb.greenPin.dimmingEnable = 0;
* ledRgbConfig.ledRgb.greenPin.gpio.port = 0;
* ledRgbConfig.ledRgb.greenPin.gpio.pin = 2;
* ledRgbConfig.ledRgb.greenPin.gpio.pinStateDefault = 0;
* ledRgbConfig.ledRgb.bluePin.dimmingEnable = 0;
* ledRgbConfig.ledRgb.bluePin.gpio.port = 0;
* ledRgbConfig.ledRgb.bluePin.gpio.pin = 3;
* ledRgbConfig.ledRgb.bluePin.gpio.pinStateDefault = 0;
* LED_Init(s_ledRgbHandle, &ledRgbConfig);
*

For dimming monochrome LED,

* uint32_t s_ledMonochromeHandleBuffer[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1) / sizeof(uitn32_t))];
* led_handle_t s_ledMonochromeHandle = (led_handle_t)&s_ledMonochromeHandleBuffer[0];
* led_config_t ledMonochromeConfig;
* ledMonochromeConfig.type = kLED_TypeMonochrome;
* ledMonochromeConfig.ledMonochrome.monochromePin.dimmingEnable = 1;
* ledMonochromeConfig.ledMonochrome.monochromePin.dimming.sourceClock = 48000000;
* ledMonochromeConfig.ledMonochrome.monochromePin.dimming.instance = 0;
* ledMonochromeConfig.ledMonochrome.monochromePin.dimming.channel = 1;
* ledMonochromeConfig.ledMonochrome.monochromePin.dimming.pinStateDefault = 0;
* LED_Init(s_ledMonochromeHandle, &ledMonochromeConfig);
*
Parameters
ledHandlePointer to point to a memory space of size LED_HANDLE_SIZE allocated by the caller. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: LED_HANDLE_DEFINE(ledHandle); or uint32_t ledHandle[((LED_HANDLE_SIZE + sizeof(uint32_t) - 1) / sizeof(uitn32_t))];
ledConfigPointer to user-defined configuration structure.
Return values
kStatus_LED_ErrorAn error occurred.
kStatus_LED_SuccessLED initialization succeed.
led_status_t LED_Deinit ( led_handle_t  ledHandle)

This function deinitializes the LED instance.

Parameters
ledHandleLED handle pointer.
Return values
kStatus_LED_SuccessLED de-initialization succeed.
led_status_t LED_SetColor ( led_handle_t  ledHandle,
led_color_t  ledRgbColor 
)

This function sets the LED color. The function only supports the RGB LED. The default color is kLED_White. Please refer to LED_MAKE_COLOR(r,g,b).

Parameters
ledHandleLED handle pointer.
ledRgbColorLED color.
Return values
kStatus_LED_ErrorAn error occurred.
kStatus_LED_SuccessColor setting succeed.
led_status_t LED_TurnOnOff ( led_handle_t  ledHandle,
uint8_t  turnOnOff 
)

This function turns on or off the led.

Parameters
ledHandleLED handle pointer.
turnOnOffSetting value, 1 - turns on, 0 - turns off.
Return values
kStatus_LED_ErrorAn error occurred.
kStatus_LED_SuccessSuccessfully turn on or off the LED.
led_status_t LED_Blip ( led_handle_t  ledHandle)

This function blips the led.

Parameters
ledHandleLED handle pointer.
Return values
kStatus_LED_ErrorAn error occurred.
kStatus_LED_SuccessSuccessfully blip the LED.
led_status_t LED_Flash ( led_handle_t  ledHandle,
led_flash_config_t *  ledFlash 
)

This function flashes the led. The flash configuration is passed by using led_flash_config_t.

Parameters
ledHandleLED handle pointer.
ledFlashLED flash configuration.
Return values
kStatus_LED_ErrorAn error occurred.
kStatus_LED_SuccessSuccessfully flash the LED.
led_status_t LED_Dimming ( led_handle_t  ledHandle,
uint16_t  dimmingPeriod,
uint8_t  increasement 
)

This function adjust the brightness of the LED.

Parameters
ledHandleLED handle pointer.
dimmingPeriodThe duration of the dimming (unit is ms).
increasementBrighten or dim (1 - brighten, 0 - dim).
Return values
kStatus_LED_ErrorAn error occurred.
kStatus_LED_SuccessSuccessfully adjust the brightness of the LED.
led_status_t LED_EnterLowpower ( led_handle_t  ledHandle)

This function is used to prepare to enter low power consumption.

Parameters
ledHandleLED handle pointer.
Return values
kStatus_LED_SuccessSuccessful operation.
led_status_t LED_ExitLowpower ( led_handle_t  ledHandle)

This function is used to restore from low power consumption.

Parameters
ledHandleLED handle pointer.
Return values
kStatus_LED_SuccessSuccessful operation.