MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Macros

#define FSL_OSA_BM_TIMER_NONE   0U
 Bare Metal does not use timer. More...
 
#define FSL_OSA_BM_TIMER_SYSTICK   1U
 Bare Metal uses SYSTICK as timer. More...
 
#define FSL_OSA_BM_TIMER_CONFIG   FSL_OSA_BM_TIMER_NONE
 Configure what timer is used in Bare Metal. More...
 
#define OSA_WAIT_FOREVER   0xFFFFFFFFU
 Constant to pass as timeout value in order to wait indefinitely. More...
 
#define TASK_MAX_NUM   7
 How many tasks can the bare metal support. More...
 
#define FSL_OSA_TIME_RANGE   0xFFFFFFFFU
 OSA's time range in millisecond, OSA time wraps if exceeds this value. More...
 
#define OSA_DEFAULT_INT_HANDLER   ((osa_int_handler_t)(&DefaultISR))
 The default interrupt handler installed in vector table. More...
 

Typedefs

typedef void * task_param_t
 Type for task parameter.
 
typedef uint32_t event_flags_t
 Type for an event flags group, bit 32 is reserved.
 

Functions

void DefaultISR (void)
 The default interrupt handler installed in vector table. More...
 

Thread management

#define PRIORITY_OSA_TO_RTOS(osa_prio)   (osa_prio)
 Defines a task. More...
 
#define PRIORITY_RTOS_TO_OSA(rtos_prio)   (rtos_prio)
 

Detailed Description

Macro Definition Documentation

#define FSL_OSA_BM_TIMER_NONE   0U
#define FSL_OSA_BM_TIMER_SYSTICK   1U
#define FSL_OSA_BM_TIMER_CONFIG   FSL_OSA_BM_TIMER_NONE
#define OSA_WAIT_FOREVER   0xFFFFFFFFU
#define TASK_MAX_NUM   7
#define FSL_OSA_TIME_RANGE   0xFFFFFFFFU
#define OSA_DEFAULT_INT_HANDLER   ((osa_int_handler_t)(&DefaultISR))
#define PRIORITY_OSA_TO_RTOS (   osa_prio)    (osa_prio)

This macro defines resources for a task statically. Then, the OSA_TaskCreate creates the task based-on these resources.

Parameters
taskThe task function.
stackSizeThe stack size this task needs in bytes.

Function Documentation

void DefaultISR ( void  )