MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
MIPI DSI SMARTDMA driver

Overview

Data Structures

struct  dsi_smartdma_write_mem_transfer_t
 The pixel format sent on MIPI DSI data lanes. More...
 
struct  dsi_smartdma_handle_t
 MIPI DSI transfer handle structure. More...
 

Typedefs

typedef void(* dsi_smartdma_callback_t )(MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, status_t status, void *userData)
 MIPI DSI callback for finished transfer. More...
 

Enumerations

enum  dsi_smartdma_input_pixel_format_t {
  kDSI_SMARTDMA_InputPixelFormatRGB565,
  kDSI_SMARTDMA_InputPixelFormatRGB888
}
 The pixel format feed SMARTDMA. More...
 
enum  dsi_smartdma_output_pixel_format_t {
  kDSI_SMARTDMA_OutputPixelFormatRGB565,
  kDSI_SMARTDMA_OutputPixelFormatRGB888
}
 The pixel format sent on MIPI DSI data lanes. More...
 

Driver version

#define FSL_MIPI_DSI_SMARTDMA_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 

Transactional

status_t DSI_TransferCreateHandleSMARTDMA (MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, dsi_smartdma_callback_t callback, void *userData)
 Create the MIPI DSI SMARTDMA handle. More...
 
status_t DSI_TransferWriteMemorySMARTDMA (MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, dsi_smartdma_write_mem_transfer_t *xfer)
 Write display controller video memory using SMARTDMA. More...
 
void DSI_TransferAbortSMARTDMA (MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle)
 Abort current APB data transfer. More...
 

Data Structure Documentation

struct dsi_smartdma_write_mem_transfer_t

Data Fields

dsi_smartdma_input_pixel_format_t inputFormat
 Input format. More...
 
dsi_smartdma_output_pixel_format_t outputFormat
 Output format. More...
 
const uint8_t * data
 Data to send. More...
 
size_t dataSize
 The byte count to be write. More...
 

Field Documentation

dsi_smartdma_input_pixel_format_t dsi_smartdma_write_mem_transfer_t::inputFormat
dsi_smartdma_output_pixel_format_t dsi_smartdma_write_mem_transfer_t::outputFormat
const uint8_t* dsi_smartdma_write_mem_transfer_t::data
size_t dsi_smartdma_write_mem_transfer_t::dataSize
struct _dsi_smartdma_handle

Data Fields

MIPI_DSI_HOST_Type * dsi
 MIPI DSI peripheral. More...
 
volatile bool isBusy
 MIPI DSI is busy with data transfer. More...
 
dsi_smartdma_callback_t callback
 DSI callback.
 
void * userData
 Callback parameter.
 
smartdma_dsi_param_t param
 Parameter for smartdma function. More...
 
uint32_t smartdmaStack [16]
 Stack for smartdma function. More...
 

Field Documentation

MIPI_DSI_HOST_Type* dsi_smartdma_handle_t::dsi
volatile bool dsi_smartdma_handle_t::isBusy
smartdma_dsi_param_t dsi_smartdma_handle_t::param
uint32_t dsi_smartdma_handle_t::smartdmaStack[16]

Typedef Documentation

typedef void(* dsi_smartdma_callback_t)(MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, status_t status, void *userData)

When transfer finished, one of these status values will be passed to the user:

  • kStatus_Success Data transfer finished with no error.

Enumeration Type Documentation

Enumerator
kDSI_SMARTDMA_InputPixelFormatRGB565 

RGB565.

kDSI_SMARTDMA_InputPixelFormatRGB888 

RGB888.

Enumerator
kDSI_SMARTDMA_OutputPixelFormatRGB565 

RGB565.

kDSI_SMARTDMA_OutputPixelFormatRGB888 

RGB888.

Function Documentation

status_t DSI_TransferCreateHandleSMARTDMA ( MIPI_DSI_HOST_Type *  base,
dsi_smartdma_handle_t *  handle,
dsi_smartdma_callback_t  callback,
void *  userData 
)
Parameters
baseMIPI DSI host peripheral base address.
handleHandle pointer.
callbackCallback function.
userDataUser data.
status_t DSI_TransferWriteMemorySMARTDMA ( MIPI_DSI_HOST_Type *  base,
dsi_smartdma_handle_t *  handle,
dsi_smartdma_write_mem_transfer_t xfer 
)

Perform data transfer using SMARTDMA, when transfer finished, upper layer could be informed through callback function.

Parameters
baseMIPI DSI host peripheral base address.
handlepointer to dsi_smartdma_handle_t structure which stores the transfer state.
xferPointer to the transfer structure.
Return values
kStatus_SuccessData transfer started successfully.
kStatus_DSI_BusyFailed to start transfer because DSI is busy with pervious transfer.
kStatus_DSI_NotSupportedTransfer format not supported.
void DSI_TransferAbortSMARTDMA ( MIPI_DSI_HOST_Type *  base,
dsi_smartdma_handle_t *  handle 
)
Parameters
baseMIPI DSI host peripheral base address.
handlepointer to dsi_smartdma_handle_t structure which stores the transfer state.