MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  asrc_p2p_sdma_config_t
 destination peripheral configuration More...
 
struct  asrc_sdma_in_handle_t
 ASRC sdma in handle. More...
 
struct  asrc_sdma_out_handle_t
 ASRC sdma out handle. More...
 
struct  asrc_sdma_handle_t
 ASRC DMA transfer handle, users should not touch the content of the handle. More...
 

Macros

#define ASRC_XFER_IN_QUEUE_SIZE   4U
 ASRC xfer queue size.
 

Typedefs

typedef void(* asrc_sdma_callback_t )(ASRC_Type *base, asrc_sdma_handle_t *handle, status_t status, void *userData)
 ASRC SDMA transfer callback function for finish and error.
 
typedef void(* asrc_start_peripheral_t )(bool start)
 ASRC trigger peripheral function pointer.
 

Driver version

#define FSL_ASRC_SDMA_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 Version 2.0.0.
 

ASRC SDMA Transactional

void ASRC_TransferInCreateHandleSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_sdma_callback_t callback, sdma_handle_t *dmaHandle, uint32_t eventSource, asrc_context_t context, const asrc_p2p_sdma_config_t *periphConfig, void *userData)
 Initializes the ASRC input SDMA handle. More...
 
void ASRC_TransferOutCreateHandleSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_sdma_callback_t callback, sdma_handle_t *dmaHandle, uint32_t eventSource, asrc_context_t context, const asrc_p2p_sdma_config_t *periphConfig, void *userData)
 Initializes the ASRC output SDMA handle. More...
 
status_t ASRC_TransferSetContextConfigSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_context_config_t *asrcConfig)
 Configures the ASRC context. More...
 
status_t ASRC_TransferSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle, asrc_transfer_t *xfer)
 Performs a non-blocking ASRC transfer using DMA. More...
 
void ASRC_TransferAbortInSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle)
 Aborts a ASRC in transfer using SDMA. More...
 
void ASRC_TransferAbortOutSDMA (ASRC_Type *base, asrc_sdma_handle_t *handle)
 brief Aborts a ASRC out transfer using SDMA. More...
 

Data Structure Documentation

struct asrc_p2p_sdma_config_t

Data Fields

uint32_t eventSource
 peripheral event source
 
uint8_t watermark
 peripheral watermark
 
uint8_t channel
 peripheral channel number
 
uint8_t fifoWidth
 peripheral fifo width
 
bool enableContinuous
 
true is the amount of samples to be transferred is unknown and script will keep on

transferring as long as both events are detected and script must be stopped by application, false is The amount of samples to be transferred is equal to the count field of mode word

 
asrc_start_peripheral_t startPeripheral
 trigger peripheral start
 
struct asrc_sdma_in_handle_t

Data Fields

sdma_handle_t * sdmaHandle
 DMA handler for ASRC.
 
uint32_t eventSource
 ASRC event source number.
 
asrc_sdma_callback_t callback
 Callback for users while transfer finish or error occurs.
 
void * userData
 User callback parameter.
 
sdma_buffer_descriptor_t bdPool [ASRC_XFER_IN_QUEUE_SIZE]
 BD pool for SDMA transfer. More...
 
uint8_t asrcInWatermark
 The transfer data count in a DMA request.
 
uint8_t bytesPerSample
 Bytes in a sample.
 
uint32_t * asrcQueue [ASRC_XFER_IN_QUEUE_SIZE]
 Transfer queue storing queued transfer. More...
 
size_t sdmaTransferSize [ASRC_XFER_IN_QUEUE_SIZE]
 Data bytes need to transfer.
 
volatile uint8_t queueUser
 Index for user to queue transfer. More...
 
volatile uint8_t queueDriver
 Index for driver to get the transfer data and size.
 
const asrc_p2p_sdma_config_t * peripheralConfig
 peripheral configuration
 
uint32_t state
 Internal state for ASRC SDMA transfer.
 

Field Documentation

sdma_buffer_descriptor_t asrc_sdma_in_handle_t::bdPool[ASRC_XFER_IN_QUEUE_SIZE]
uint32_t* asrc_sdma_in_handle_t::asrcQueue[ASRC_XFER_IN_QUEUE_SIZE]
volatile uint8_t asrc_sdma_in_handle_t::queueUser
struct asrc_sdma_out_handle_t

Data Fields

sdma_handle_t * sdmaHandle
 DMA handler for ASRC.
 
void * userData
 User callback parameter.
 
uint32_t state
 Internal state for ASRC SDMA transfer.
 
uint8_t bytesPerSample
 Bytes in a sample.
 
uint32_t eventSource
 ASRC event source number.
 
asrc_sdma_callback_t callback
 Callback for users while transfer finish or error occurs.
 
uint8_t asrcOutWatermark
 The transfer data count in a DMA request.
 
sdma_buffer_descriptor_t bdPool [ASRC_XFER_OUT_QUEUE_SIZE]
 BD pool for SDMA transfer. More...
 
uint32_t * asrcQueue [ASRC_XFER_OUT_QUEUE_SIZE]
 Transfer queue storing queued transfer. More...
 
size_t sdmaTransferSize [ASRC_XFER_OUT_QUEUE_SIZE]
 Data bytes need to transfer.
 
volatile uint8_t queueUser
 Index for user to queue transfer. More...
 
volatile uint8_t queueDriver
 Index for driver to get the transfer data and size.
 
const asrc_p2p_sdma_config_t * peripheralConfig
 peripheral configuration
 
uint32_t nonAlignSize
 non align size
 
void * nonAlignAddr
 non align address
 

Field Documentation

sdma_buffer_descriptor_t asrc_sdma_out_handle_t::bdPool[ASRC_XFER_OUT_QUEUE_SIZE]
uint32_t* asrc_sdma_out_handle_t::asrcQueue[ASRC_XFER_OUT_QUEUE_SIZE]
volatile uint8_t asrc_sdma_out_handle_t::queueUser
struct _asrc_sdma_handle

ASRC sdma handle prototype.

Data Fields

asrc_sdma_in_handle_t inDMAHandle
 input dma handle
 
asrc_sdma_out_handle_t outDMAHandle
 output dma handle
 
asrc_context_t context
 ASRC context number.
 
uint8_t dataChannels
 ASRC process data channel number.
 

Function Documentation

void ASRC_TransferInCreateHandleSDMA ( ASRC_Type *  base,
asrc_sdma_handle_t *  handle,
asrc_sdma_callback_t  callback,
sdma_handle_t *  dmaHandle,
uint32_t  eventSource,
asrc_context_t  context,
const asrc_p2p_sdma_config_t *  periphConfig,
void *  userData 
)

This function initializes the ASRC input DMA handle, which can be used for other ASRC transactional APIs. Usually, for a specified ASRC context, call this API once to get the initialized handle.

Parameters
baseASRC base pointer.
handleASRC SDMA handle pointer.
baseASRC peripheral base address.
callbackPointer to user callback function.
dmaHandleSDMA handle pointer, this handle shall be static allocated by users.
eventSourceASRC input sdma event source.
contextASRC context number.
periphConfigperipheral configurations, used for case.
userDataUser parameter passed to the callback function.
void ASRC_TransferOutCreateHandleSDMA ( ASRC_Type *  base,
asrc_sdma_handle_t *  handle,
asrc_sdma_callback_t  callback,
sdma_handle_t *  dmaHandle,
uint32_t  eventSource,
asrc_context_t  context,
const asrc_p2p_sdma_config_t *  periphConfig,
void *  userData 
)

This function initializes the ASRC out DMA handle, which can be used for other ASRC transactional APIs. Usually, for a specified ASRC context, call this API once to get the initialized handle.

Parameters
baseASRC base pointer.
handleASRC SDMA handle pointer.
callback,ASRCoutcallback.
baseASRC peripheral base address.
dmaHandleSDMA handle pointer, this handle shall be static allocated by users.
eventSourceASRC output event source.
contextASRC context number.
periphConfigperipheral configurations, used for case.
userDataUser parameter passed to the callback function.
status_t ASRC_TransferSetContextConfigSDMA ( ASRC_Type *  base,
asrc_sdma_handle_t *  handle,
asrc_context_config_t *  asrcConfig 
)
Parameters
baseASRC base pointer.
handleASRC SDMA handle pointer.
asrcConfigasrc context configurations.
status_t ASRC_TransferSDMA ( ASRC_Type *  base,
asrc_sdma_handle_t *  handle,
asrc_transfer_t *  xfer 
)
Parameters
baseASRC base pointer.
handleASRC SDMA handle pointer.
xferASRC xfer configurations pointer.
Return values
kStatus_SuccessStart a ASRC SDMA send successfully.
kStatus_InvalidArgumentThe input argument is invalid.
kStatus_TxBusyASRC is busy sending data.
void ASRC_TransferAbortInSDMA ( ASRC_Type *  base,
asrc_sdma_handle_t *  handle 
)
Parameters
baseASRC base pointer.
handleASRC SDMA handle pointer.
void ASRC_TransferAbortOutSDMA ( ASRC_Type *  base,
asrc_sdma_handle_t *  handle 
)

param base ASRC base pointer. param handle ASRC SDMA handle pointer.