MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Power

Data Structures

struct  power_pad_vrange_t
 pad voltage range configuration. More...
 

Macros

#define SYSCTL0_TUPLE_REG(reg)   (*((volatile uint32_t *)(((uint32_t)(SYSCTL0)) + ((reg)&0xFFFU))))
 PMIC mode pin configuration API parameter.
 

Enumerations

enum  _pmc_interrupt {
  kPMC_INT_LVDCORE = PMC_CTRL_LVDCOREIE_MASK,
  kPMC_INT_HVDCORE = PMC_CTRL_HVDCOREIE_MASK,
  kPMC_INT_HVD1V8 = PMC_CTRL_HVD1V8IE_MASK,
  kPMC_INT_AUTOWK = PMC_CTRL_AUTOWKEN_MASK,
  kPMC_INT_INTRPAD
}
 PMC event flags. More...
 
enum  _pmc_event_flags {
  kPMC_FLAGS_PORCORE = PMC_FLAGS_PORCOREF_MASK,
  kPMC_FLAGS_POR1V8,
  kPMC_FLAGS_PORAO18,
  kPMC_FLAGS_LVDCORE,
  kPMC_FLAGS_HVDCORE,
  kPMC_FLAGS_HVD1V8,
  kPMC_FLAGS_RTC,
  kPMC_FLAGS_AUTOWK,
  kPMC_FLAGS_INTNPADF = PMC_FLAGS_INTNPADF_MASK,
  kPMC_FLAGS_RESETNPAD = PMC_FLAGS_RESETNPADF_MASK,
  kPMC_FLAGS_DEEPPD = PMC_FLAGS_DEEPPDF_MASK
}
 PMC event flags. More...
 
enum  power_mode_cfg_t
 Power mode configuration API parameter.
 
enum  body_bias_mode_t
 Body Bias mode definition.
 
enum  power_pad_vrange_val_t {
  kPadVol_171_360 = 0U,
  kPadVol_171_198 = 1U,
  kPadVol_300_360 = 2U
}
 pad voltage range value. More...
 
enum  power_lvd_falling_trip_vol_val_t {
  kLvdFallingTripVol_720 = 0U,
  kLvdFallingTripVol_735 = 1U,
  kLvdFallingTripVol_750 = 2U,
  kLvdFallingTripVol_765 = 3U,
  kLvdFallingTripVol_780 = 4U,
  kLvdFallingTripVol_795 = 5U,
  kLvdFallingTripVol_810 = 6U,
  kLvdFallingTripVol_825 = 7U,
  kLvdFallingTripVol_840 = 8U,
  kLvdFallingTripVol_855 = 9U,
  kLvdFallingTripVol_870 = 10U,
  kLvdFallingTripVol_885 = 11U,
  kLvdFallingTripVol_900 = 12U,
  kLvdFallingTripVol_915 = 13U,
  kLvdFallingTripVol_930 = 14U,
  kLvdFallingTripVol_945 = 15U
}
 LVD falling trip voltage value. More...
 
enum  power_part_temp_range {
  kPartTemp_0C_P70C = 0U,
  kPartTemp_N20C_P70C = 1U
}
 Part temperature range. More...
 

Functions

static void POWER_EnablePD (pd_bit_t en)
 API to enable PDRUNCFG bit in the Sysctl0. More...
 
static void POWER_DisablePD (pd_bit_t en)
 API to disable PDRUNCFG bit in the Sysctl0. More...
 
static void POWER_EnableDeepSleep (void)
 API to enable deep sleep bit in the ARM Core.
 
static void POWER_DisableDeepSleep (void)
 API to disable deep sleep bit in the ARM Core.
 
void POWER_UpdateOscSettlingTime (uint32_t osc_delay)
 API to update XTAL oscillator settling time . More...
 
void POWER_UpdatePmicRecoveryTime (uint32_t pmic_delay)
 API to update on-board PMIC vddcore recovery time. More...
 
void POWER_ApplyPD (void)
 API to apply updated PMC PDRUNCFG bits in the Sysctl0.
 
void POWER_ClearEventFlags (uint32_t statusMask)
 Clears the PMC event flags state. More...
 
uint32_t POWER_GetEventFlags (void)
 Get the PMC event flags state. More...
 
void POWER_EnableInterrupts (uint32_t interruptMask)
 Enable the PMC interrupt requests. More...
 
void POWER_DisableInterrupts (uint32_t interruptMask)
 Disable the PMC interrupt requests. More...
 
void POWER_SetAnalogBuffer (bool enable)
 Set the PMC analog buffer for references or ATX2. More...
 
static uint32_t POWER_GetPmicMode (pmic_mode_reg_t reg)
 Get PMIC_MODE pins configure value. More...
 
static body_bias_mode_t POWER_GetBodyBiasMode (pmic_mode_reg_t reg)
 Get RBB/FBB bit value. More...
 
void POWER_SetPadVolRange (const power_pad_vrange_t *config)
 Configure pad voltage level. More...
 
void POWER_EnterRbb (void)
 PMC Enter Rbb mode function call.
 
void POWER_EnterFbb (void)
 PMC Enter Fbb mode function call.
 
void POWER_EnterNbb (void)
 PMC exit Rbb & Fbb mode function call.
 
void POWER_SetLdoVoltageForFreq (power_part_temp_range temp_range, uint32_t main_clk_freq, uint32_t dsp_main_clk_freq)
 PMC Set Ldo volatage for particular frequency. NOTE: If LVD falling trip voltage is higher than the required core voltage for particular frequency, LVD voltage will be decreased to safe level to avoid unexpected LVD reset or interrupt event. More...
 
void POWER_SetLvdFallingTripVoltage (power_lvd_falling_trip_vol_val_t volt)
 Set vddcore low voltage detection falling trip voltage. More...
 
power_lvd_falling_trip_vol_val_t POWER_GetLvdFallingTripVoltage (void)
 Get current vddcore low voltage detection falling trip voltage. More...
 
void POWER_SetPmicMode (uint32_t mode, pmic_mode_reg_t reg)
 Set PMIC_MODE pins configure value. More...
 
void POWER_EnterSleep (void)
 Configures and enters in SLEEP low power mode.
 
void POWER_EnterDeepSleep (const uint32_t exclude_from_pd[4])
 PMC Deep Sleep function call. More...
 
void POWER_EnterDeepPowerDown (const uint32_t exclude_from_pd[4])
 PMC Deep Power Down function call. More...
 
void POWER_EnterFullDeepPowerDown (const uint32_t exclude_from_pd[4])
 PMC Full Deep Power Down function call. More...
 
void POWER_EnterPowerMode (power_mode_cfg_t mode, const uint32_t exclude_from_pd[4])
 Power Library API to enter different power mode. More...
 
void EnableDeepSleepIRQ (IRQn_Type interrupt)
 Enable specific interrupt for wake-up from deep-sleep mode. More...
 
void DisableDeepSleepIRQ (IRQn_Type interrupt)
 Disable specific interrupt for wake-up from deep-sleep mode. More...
 
uint32_t POWER_GetLibVersion (void)
 Power Library API to return the library version. More...
 

Driver version

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 power driver version 2.2.0. More...
 

Detailed Description


Data Structure Documentation

struct power_pad_vrange_t

Data Fields

uint32_t Vdde0Range: 2
 VDDE0 voltage range for VDDIO_0. More...
 
uint32_t Vdde1Range: 2
 VDDE1 voltage range for VDDIO_1. More...
 
uint32_t Vdde2Range: 2
 VDDE2 voltage range for VDDIO_2. More...
 
uint32_t __pad0__: 26
 Reserved. More...
 

Field Documentation

uint32_t power_pad_vrange_t::Vdde0Range
uint32_t power_pad_vrange_t::Vdde1Range
uint32_t power_pad_vrange_t::Vdde2Range
uint32_t power_pad_vrange_t::__pad0__

Macro Definition Documentation

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))

Enumeration Type Documentation

Note
These enums are meant to be OR'd together to form a bit mask.
Enumerator
kPMC_INT_LVDCORE 

Vddcore Low-Voltage Detector Interrupt Enable.

kPMC_INT_HVDCORE 

Vddcore High-Voltage Detector Interrupt Enable.

kPMC_INT_HVD1V8 

Vdd1v8 High-Voltage Detector Interrupt Enable.

kPMC_INT_AUTOWK 

PMC automatic wakeup enable and interrupt enable.

kPMC_INT_INTRPAD 

Interrupt pad deep powerdown and deep sleep wake up & interrupt enable.

Note
These enums are meant to be OR'd together to form a bit mask.
Enumerator
kPMC_FLAGS_PORCORE 

POR triggered by the vddcore POR monitor (0 = no, 1 = yes).

kPMC_FLAGS_POR1V8 

vdd1v8 power on event detected since last cleared(0 = no, 1 = yes).

kPMC_FLAGS_PORAO18 

vdd_ao18 power on event detected since last cleared (0 = no, 1 = yes).

kPMC_FLAGS_LVDCORE 

LVD tripped since last time this bit was cleared (0 = no, 1 = yes).

kPMC_FLAGS_HVDCORE 

HVD tripped since last time this bit was cleared (0 = no, 1 = yes).

kPMC_FLAGS_HVD1V8 

vdd1v8 HVD tripped since last time this bit was cleared (0 = no, 1 = yes).

kPMC_FLAGS_RTC 

RTC wakeup detected since last time flag was cleared (0 = no, 1 = yes).

kPMC_FLAGS_AUTOWK 

PMC Auto wakeup caused a deep sleep wakeup and interrupt (0 = no, 1 = yes).

kPMC_FLAGS_INTNPADF 

Pad interrupt caused a wakeup or interrupt event since the last time this flag was cleared (0 = no, 1 = yes).

kPMC_FLAGS_RESETNPAD 

Reset pad wakeup caused a wakeup or reset event since the last time this bit was cleared.

(0 = no, 1 = yes).

kPMC_FLAGS_DEEPPD 

Deep powerdown was entered since the last time this flag was cleared (0 = no, 1 = yes).

Enumerator
kPadVol_171_360 

Voltage from 1.71V to 3.60V.

kPadVol_171_198 

Voltage from 1.71V to 1.98V.

kPadVol_300_360 

Voltage from 3.00V to 3.60V.

Enumerator
kLvdFallingTripVol_720 

Voltage 720mV.

kLvdFallingTripVol_735 

Voltage 735mV.

kLvdFallingTripVol_750 

Voltage 750mV.

kLvdFallingTripVol_765 

Voltage 765mV.

kLvdFallingTripVol_780 

Voltage 780mV.

kLvdFallingTripVol_795 

Voltage 795mV.

kLvdFallingTripVol_810 

Voltage 810mV.

kLvdFallingTripVol_825 

Voltage 825mV.

kLvdFallingTripVol_840 

Voltage 840mV.

kLvdFallingTripVol_855 

Voltage 855mV.

kLvdFallingTripVol_870 

Voltage 870mV.

kLvdFallingTripVol_885 

Voltage 885mV.

kLvdFallingTripVol_900 

Voltage 900mV.

kLvdFallingTripVol_915 

Voltage 915mV.

kLvdFallingTripVol_930 

Voltage 930mV.

kLvdFallingTripVol_945 

Voltage 945mV.

Enumerator
kPartTemp_0C_P70C 

Part temp range 0C - 70C.

kPartTemp_N20C_P70C 

Part temp range -20C - 70C.

Function Documentation

static void POWER_EnablePD ( pd_bit_t  en)
inlinestatic

Note that enabling the bit powers down the peripheral

Parameters
enperipheral for which to enable the PDRUNCFG bit
static void POWER_DisablePD ( pd_bit_t  en)
inlinestatic

Note that disabling the bit powers up the peripheral

Parameters
enperipheral for which to disable the PDRUNCFG bit
void POWER_UpdateOscSettlingTime ( uint32_t  osc_delay)
Parameters
osc_delay: OSC stabilization time in unit of microsecond
void POWER_UpdatePmicRecoveryTime ( uint32_t  pmic_delay)
Parameters
pmic_delay: PMIC stabilization time in unit of microsecond
void POWER_ClearEventFlags ( uint32_t  statusMask)
Parameters
statusMask: A bitmask of event flags that are to be cleared.
uint32_t POWER_GetEventFlags ( void  )
Returns
PMC FLAGS register value
void POWER_EnableInterrupts ( uint32_t  interruptMask)
Parameters
interruptMask: A bitmask of of interrupts to enable.
void POWER_DisableInterrupts ( uint32_t  interruptMask)
Parameters
interruptMask: A bitmask of of interrupts to disable.
void POWER_SetAnalogBuffer ( bool  enable)
Parameters
enable: Set to true to enable analog buffer for references or ATX2, false to disable.
static uint32_t POWER_GetPmicMode ( pmic_mode_reg_t  reg)
inlinestatic
Parameters
reg: PDSLEEPCFG0 or PDRUNCFG0 register offset
Returns
PMIC_MODE pins value in PDSLEEPCFG0
static body_bias_mode_t POWER_GetBodyBiasMode ( pmic_mode_reg_t  reg)
inlinestatic
Parameters
reg: PDSLEEPCFG0 or PDRUNCFG0 register offset
Returns
Current body bias mode
void POWER_SetPadVolRange ( const power_pad_vrange_t *  config)

Wide voltage range cost more power due to enabled voltage detector.

NOTE: BE CAUTIOUS TO CALL THIS API. IF THE PAD SUPPLY IS BEYOND THE SET RANGE, SILICON MIGHT BE DAMAGED.

Parameters
configpad voltage range configuration.
void POWER_SetLdoVoltageForFreq ( power_part_temp_range  temp_range,
uint32_t  main_clk_freq,
uint32_t  dsp_main_clk_freq 
)
Parameters
temp_range: part temperature range
main_clk_freq: main clock frequency value
dsp_main_clk_freq: dsp main clock frequency value
void POWER_SetLvdFallingTripVoltage ( power_lvd_falling_trip_vol_val_t  volt)
Parameters
volttarget LVD voltage to set.
power_lvd_falling_trip_vol_val_t POWER_GetLvdFallingTripVoltage ( void  )
Returns
Current LVD voltage.
void POWER_SetPmicMode ( uint32_t  mode,
pmic_mode_reg_t  reg 
)
Parameters
mode: PMIC MODE pin value
reg: PDSLEEPCFG0 or PDRUNCFG0 register offset
Returns
PMIC_MODE pins value in PDSLEEPCFG0
void POWER_EnterDeepSleep ( const uint32_t  exclude_from_pd[4])
Parameters
exclude_from_pdBit mask of the PDRUNCFG0 ~ PDRUNCFG3 that needs to be powered on during Deep Sleep mode selected.
void POWER_EnterDeepPowerDown ( const uint32_t  exclude_from_pd[4])
Parameters
exclude_from_pdBit mask of the PDRUNCFG0 ~ PDRUNCFG3 that needs to be powered on during Deep Power Down mode selected.
void POWER_EnterFullDeepPowerDown ( const uint32_t  exclude_from_pd[4])
Parameters
exclude_from_pdBit mask of the PDRUNCFG0 ~ PDRUNCFG3 that needs to be powered on during Full Deep Power Down mode selected.
void POWER_EnterPowerMode ( power_mode_cfg_t  mode,
const uint32_t  exclude_from_pd[4] 
)
Parameters
modePower mode to enter.
exclude_from_pdBit mask of the PDRUNCFG0 ~ PDRUNCFG3 that needs to be powered on during power mode selected.
void EnableDeepSleepIRQ ( IRQn_Type  interrupt)

Enable the interrupt for wake-up from deep sleep mode. Some interrupts are typically used in sleep mode only and will not occur during deep-sleep mode because relevant clocks are stopped. However, it is possible to enable those clocks (significantly increasing power consumption in the reduced power mode), making these wake-ups possible.

Note
This function also enables the interrupt in the NVIC (EnableIRQ() is called internally).
Parameters
interruptThe IRQ number.
void DisableDeepSleepIRQ ( IRQn_Type  interrupt)

Disable the interrupt for wake-up from deep sleep mode. Some interrupts are typically used in sleep mode only and will not occur during deep-sleep mode because relevant clocks are stopped. However, it is possible to enable those clocks (significantly increasing power consumption in the reduced power mode), making these wake-ups possible.

Note
This function also disables the interrupt in the NVIC (DisableIRQ() is called internally).
Parameters
interruptThe IRQ number.
uint32_t POWER_GetLibVersion ( void  )
Returns
version number of the power library