![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
| Configuration for channel | |
| Configuration for ACMP | |
| Configuration for DAC | |
| Configuration for discrete mode | |
| Configuration for filter | |
| Configuration for round robin mode | |
| PLL configuration for SYSPLL | |
| PLL configuration for FRG | |
| PLL configuration for SYSPLL | |
| CRC protocol configuration | |
| Timer configuration structure | |
| Match configuration | |
| DMA channel trigger | |
| DMA channel trigger | |
| DMA descriptor structure | |
| DMA transfer handle structure | |
| DMA transfer configuration | |
| DMA transfer configuration | |
| DMIC Channel configuration structure | |
| DMIC DMA handle | |
| DMIC transfer structure | |
| Structure for DSP copy image to destination address | |
| FLEXSPI configuration structure | |
| External device configuration items | |
| FLEXSPI DMA transfer handle, users should not touch the content of the handle | |
| FLEXSPI DMA transfer handle, users should not touch the content of the handle | |
| Transfer handle structure for FLEXSPI | |
| Transfer structure for FLEXSPI | |
| Configures the interrupt generation condition | |
| The GPIO pin configuration structure | |
| UART configuration structure | |
| UART transfer structure | |
| Specify HASHCRYPT's key resource | |
| Storage type used to save hash context | |
| Structure with settings to initialize the I2C master module | |
| I2C master dma transfer structure | |
| Driver handle for master non-blocking APIs | |
| Non-blocking transfer descriptor structure | |
| I2C FreeRTOS handle | |
| Data structure with 7-bit Slave address and Slave address disable | |
| Structure with settings to initialize the I2C slave module | |
| I2C slave handle structure | |
| I2C slave transfer structure | |
| I2S configuration structure | |
| I2s dma handle | |
| Members not to be accessed / modified outside of the driver | |
| Buffer to transfer from or receive audio data into | |
| Structure with I3C baudrate settings | |
| Structure with settings to initialize the I3C master module | |
| Driver handle for master non-blocking APIs | |
| Non-blocking transfer descriptor structure | |
| Structure with setting master IBI rules and slave registry | |
| Structure with settings to initialize the I3C slave module | |
| I3C slave handle structure | |
| I3C slave transfer structure | |
| Array of IOPCTL pin definitions passed to IOPCTL_SetPinMuxing() must be in this format | |
| The list element | |
| The list structure | |
| LPADC global configuration | |
| Define structure to keep the configuration for conversion command | |
| Define the structure to keep the conversion result | |
| Define structure to keep the configuration for conversion trigger | |
| MMC card boot configuration definition | |
| Mmc card state | |
| MMC card CID register | |
| MMC card CSD register | |
| MMC Extended CSD configuration | |
| MMC card Extended CSD register (unit: byte) | |
| MRT configuration structure | |
| Callback configuration structure | |
| Notifier handle structure | |
| Notification block passed to the registered callback function | |
| Pad voltage range configuration | |
| Instance structure for the direct form II Biquad cascade filter | |
| Struct to save biquad parameters | |
| Struct to save biquad state | |
| Powerquad data structure format | |
| Conversion between integer and float type | |
| Coprocessor prescale | |
| Structure is used to hold the date and time | |
| FLEX USART configuration structure | |
| SCTimer configuration structure | |
| Options to configure a SCTimer PWM signal | |
| SD card state | |
| SD card CID register | |
| SD card CSD register | |
| SD card SCR register | |
| SD card status | |
| SDIO card state | |
| Sdio card common CIS | |
| Sdio card FBR register | |
| Sdio card function CIS | |
| Card interrupt application callback | |
| Card switch voltage function collection | |
| Sd card detect | |
| Card power control | |
| Card user parameter, user can define the parameter according the board, card capability | |
| SD Card Structure | |
| SDSPI host state | |
| Callback message structure | |
| Serial manager config structure | |
| Serial port swo config struct | |
| Serial port uart config struct | |
| Serial port usb config struct | |
| Serial port usb config struct | |
| User command data configuration structure | |
| Internal configuration structure used in 'spi' and 'spi_dma' driver | |
| SPI delay time configure structure | |
| SPI DMA transfer handle, users should not touch the content of the handle | |
| SPI half-duplex(master only) transfer structure | |
| SPI master user configure structure | |
| SPI transfer handle structure | |
| SPI FreeRTOS handle | |
| SPI slave user configure structure | |
| SPI transfer structure | |
| Data structure for the TRNG initialization | |
| Data structure for definition of statistical check limits | |
| USART configuration structure | |
| UART DMA handle | |
| USART handle structure | |
| FLEX USART FreeRTOS handle | |
| USART transfer structure | |
| Defines the ADMA2 descriptor structure | |
| ADMA configuration | |
| Data structure to configure the MMC boot feature | |
| USDHC capability information | |
| Card command descriptor | |
| Data structure to initialize the USDHC | |
| Card data descriptor | |
| USDHC handle | |
| USDHC host descriptor | |
| USDHC callback functions | |
| Transfer state | |
| Describes WWDT configuration structure |