![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | semaphore_t |
Type for an semaphore. More... | |
struct | mutex_t |
Type for a mutex. More... | |
struct | task_control_block_t |
Task control block for bare metal. More... | |
struct | event_t |
Type for an event object. More... | |
struct | msg_queue_t |
Type for a message queue. More... | |
Macros | |
#define | FSL_OSA_BM_TASK_ENABLE 1U |
Definition to determine whether enable TASK module. More... | |
#define | FSL_OSA_BM_TIMER_NONE 0U |
Bare Metal does not use timer. More... | |
#define | FSL_OSA_BM_TIMER_SYSTICK 1U |
Bare Metal uses SYSTICK as timer. More... | |
#define | FSL_OSA_BM_TIMER_CONFIG FSL_OSA_BM_TIMER_SYSTICK |
Configure what timer is used in Bare Metal. More... | |
#define | OSA_WAIT_FOREVER 0xFFFFFFFFU |
Constant to pass as timeout value in order to wait indefinitely. More... | |
#define | TASK_MAX_NUM 7 |
How many tasks can the bare metal support. More... | |
#define | FSL_OSA_TIME_RANGE 0xFFFFFFFFU |
OSA's time range in millisecond, OSA time wraps if exceeds this value. More... | |
#define | OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) |
The default interrupt handler installed in vector table. More... | |
Typedefs | |
typedef void * | task_param_t |
Type for task parameter. | |
typedef void(* | task_t )(task_param_t param) |
Type for a task handler, returned by the OSA_TaskCreate function. | |
typedef task_control_block_t * | task_handler_t |
Type for a task pointer. | |
typedef uint32_t | task_stack_t |
Type for a task stack. | |
typedef uint32_t | event_flags_t |
Type for an event flags group, bit 32 is reserved. | |
typedef msg_queue_t * | msg_queue_handler_t |
Type for a message queue handler. | |
Functions | |
void | DefaultISR (void) |
The default interrupt handler installed in vector table. More... | |
Thread management | |
#define | PRIORITY_OSA_TO_RTOS(osa_prio) (osa_prio) |
Defines a task. More... | |
#define | PRIORITY_RTOS_TO_OSA(rtos_prio) (rtos_prio) |
struct semaphore_t |
Data Fields | |
uint32_t | time_start |
The time to start timeout. | |
uint32_t | timeout |
Timeout to wait in milliseconds. | |
volatile bool | isWaiting |
Is any task waiting for a timeout on this object. | |
volatile uint8_t | semCount |
The count value of the object. | |
struct mutex_t |
Data Fields | |
uint32_t | time_start |
The time to start timeout. | |
uint32_t | timeout |
Timeout to wait in milliseconds. | |
volatile bool | isWaiting |
Is any task waiting for a timeout on this mutex. | |
volatile bool | isLocked |
Is the object locked or not. | |
struct task_control_block_t |
Data Fields | |
osa_task_ptr_t | p_func |
Task's entry. | |
osa_task_priority_t | priority |
Task's priority. | |
osa_task_param_t | param |
Task's parameter. | |
bool | haveToRun |
Task was signaled. | |
struct event_t |
Data Fields | |
uint32_t | time_start |
The time to start timeout. | |
uint32_t | timeout |
Timeout to wait in milliseconds. | |
volatile event_flags_t | flags |
The flags status. | |
task_handler_t | waitingTask |
Handler to the waiting task. | |
bool | autoClear |
Auto clear or manual clear. | |
volatile bool | isWaiting |
Is any task waiting for a timeout on this event. | |
struct msg_queue_t |
Data Fields | |
volatile bool | isWaiting |
Is any task waiting for a timeout. | |
uint32_t | time_start |
The time to start timeout. | |
uint32_t | timeout |
Timeout to wait in milliseconds. | |
uint32_t | size |
The size(byte) of a single message. | |
task_handler_t | waitingTask |
Handler to the waiting task. | |
uint8_t * | queueMem |
Points to the queue memory. | |
uint16_t | number |
The number of messages in the queue. | |
uint16_t | max |
The max number of queue messages. | |
uint16_t | head |
Index of the next message to be read. | |
uint16_t | tail |
Index of the next place to write to. | |
#define FSL_OSA_BM_TASK_ENABLE 1U |
#define FSL_OSA_BM_TIMER_NONE 0U |
#define FSL_OSA_BM_TIMER_SYSTICK 1U |
#define FSL_OSA_BM_TIMER_CONFIG FSL_OSA_BM_TIMER_SYSTICK |
#define OSA_WAIT_FOREVER 0xFFFFFFFFU |
#define TASK_MAX_NUM 7 |
#define FSL_OSA_TIME_RANGE 0xFFFFFFFFU |
#define OSA_DEFAULT_INT_HANDLER ((osa_int_handler_t)(&DefaultISR)) |
#define PRIORITY_OSA_TO_RTOS | ( | osa_prio | ) | (osa_prio) |
This macro defines resources for a task statically. Then, the OSA_TaskCreate creates the task based-on these resources.
task | The task function. |
stackSize | The stack size this task needs in bytes. |
void DefaultISR | ( | void | ) |