MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
X.509 module

Overview

The X.509 module provides X.509 support for reading, writing and verification of certificates. In summary:

This module can be used to build a certificate authority (CA) chain and verify its signature. It is also used to generate Certificate Signing Requests and X.509 certificates just as a CA would do.

Data Structures

struct  mbedtls_x509_time
 
struct  mbedtls_x509_crl_entry
 
struct  mbedtls_x509_crl
 
struct  mbedtls_x509_crt
 
struct  mbedtls_x509_crt_profile
 
struct  mbedtls_x509write_cert
 
struct  mbedtls_x509_crt_verify_chain_item
 
struct  mbedtls_x509_crt_verify_chain
 
struct  mbedtls_x509_csr
 
struct  mbedtls_x509write_csr
 

Macros

#define MBEDTLS_X509_MAX_INTERMEDIATE_CA   8
 

Functions

int mbedtls_dhm_parse_dhm (mbedtls_dhm_context *dhm, const unsigned char *dhmin, size_t dhminlen)
 This function parses DHM parameters in PEM or DER format. More...
 
int mbedtls_dhm_parse_dhmfile (mbedtls_dhm_context *dhm, const char *path)
 This function loads and parses DHM parameters from a file. More...
 

X509 Error codes

#define MBEDTLS_ERR_X509_FEATURE_UNAVAILABLE   -0x2080
 
#define MBEDTLS_ERR_X509_UNKNOWN_OID   -0x2100
 
#define MBEDTLS_ERR_X509_INVALID_FORMAT   -0x2180
 
#define MBEDTLS_ERR_X509_INVALID_VERSION   -0x2200
 
#define MBEDTLS_ERR_X509_INVALID_SERIAL   -0x2280
 
#define MBEDTLS_ERR_X509_INVALID_ALG   -0x2300
 
#define MBEDTLS_ERR_X509_INVALID_NAME   -0x2380
 
#define MBEDTLS_ERR_X509_INVALID_DATE   -0x2400
 
#define MBEDTLS_ERR_X509_INVALID_SIGNATURE   -0x2480
 
#define MBEDTLS_ERR_X509_INVALID_EXTENSIONS   -0x2500
 
#define MBEDTLS_ERR_X509_UNKNOWN_VERSION   -0x2580
 
#define MBEDTLS_ERR_X509_UNKNOWN_SIG_ALG   -0x2600
 
#define MBEDTLS_ERR_X509_SIG_MISMATCH   -0x2680
 
#define MBEDTLS_ERR_X509_CERT_VERIFY_FAILED   -0x2700
 
#define MBEDTLS_ERR_X509_CERT_UNKNOWN_FORMAT   -0x2780
 
#define MBEDTLS_ERR_X509_BAD_INPUT_DATA   -0x2800
 
#define MBEDTLS_ERR_X509_ALLOC_FAILED   -0x2880
 
#define MBEDTLS_ERR_X509_FILE_IO_ERROR   -0x2900
 
#define MBEDTLS_ERR_X509_BUFFER_TOO_SMALL   -0x2980
 
#define MBEDTLS_ERR_X509_FATAL_ERROR   -0x3000
 

X509 Verify codes

#define MBEDTLS_X509_BADCERT_EXPIRED   0x01
 
#define MBEDTLS_X509_BADCERT_REVOKED   0x02
 
#define MBEDTLS_X509_BADCERT_CN_MISMATCH   0x04
 
#define MBEDTLS_X509_BADCERT_NOT_TRUSTED   0x08
 
#define MBEDTLS_X509_BADCRL_NOT_TRUSTED   0x10
 
#define MBEDTLS_X509_BADCRL_EXPIRED   0x20
 
#define MBEDTLS_X509_BADCERT_MISSING   0x40
 
#define MBEDTLS_X509_BADCERT_SKIP_VERIFY   0x80
 
#define MBEDTLS_X509_BADCERT_OTHER   0x0100
 
#define MBEDTLS_X509_BADCERT_FUTURE   0x0200
 
#define MBEDTLS_X509_BADCRL_FUTURE   0x0400
 
#define MBEDTLS_X509_BADCERT_KEY_USAGE   0x0800
 
#define MBEDTLS_X509_BADCERT_EXT_KEY_USAGE   0x1000
 
#define MBEDTLS_X509_BADCERT_NS_CERT_TYPE   0x2000
 
#define MBEDTLS_X509_BADCERT_BAD_MD   0x4000
 
#define MBEDTLS_X509_BADCERT_BAD_PK   0x8000
 
#define MBEDTLS_X509_BADCERT_BAD_KEY   0x010000
 
#define MBEDTLS_X509_BADCRL_BAD_MD   0x020000
 
#define MBEDTLS_X509_BADCRL_BAD_PK   0x040000
 
#define MBEDTLS_X509_BADCRL_BAD_KEY   0x080000
 

Structures for parsing X.509 certificates, CRLs and CSRs

typedef mbedtls_asn1_buf mbedtls_x509_buf
 
typedef mbedtls_asn1_bitstring mbedtls_x509_bitstring
 
typedef mbedtls_asn1_named_data mbedtls_x509_name
 
typedef mbedtls_asn1_sequence mbedtls_x509_sequence
 

Structures and functions for parsing CRLs

int mbedtls_x509_crl_parse_der (mbedtls_x509_crl *chain, const unsigned char *buf, size_t buflen)
 Parse a DER-encoded CRL and append it to the chained list. More...
 
int mbedtls_x509_crl_parse (mbedtls_x509_crl *chain, const unsigned char *buf, size_t buflen)
 Parse one or more CRLs and append them to the chained list. More...
 
int mbedtls_x509_crl_parse_file (mbedtls_x509_crl *chain, const char *path)
 Load one or more CRLs and append them to the chained list. More...
 
int mbedtls_x509_crl_info (char *buf, size_t size, const char *prefix, const mbedtls_x509_crl *crl)
 Returns an informational string about the CRL. More...
 
void mbedtls_x509_crl_init (mbedtls_x509_crl *crl)
 Initialize a CRL (chain) More...
 
void mbedtls_x509_crl_free (mbedtls_x509_crl *crl)
 Unallocate all CRL data. More...
 

Structures and functions for parsing and writing X.509 certificates

typedef void mbedtls_x509_crt_restart_ctx
 
const mbedtls_x509_crt_profile mbedtls_x509_crt_profile_default
 
const mbedtls_x509_crt_profile mbedtls_x509_crt_profile_next
 
const mbedtls_x509_crt_profile mbedtls_x509_crt_profile_suiteb
 
int mbedtls_x509_crt_parse_der (mbedtls_x509_crt *chain, const unsigned char *buf, size_t buflen)
 Parse a single DER formatted certificate and add it to the chained list. More...
 
int mbedtls_x509_crt_parse (mbedtls_x509_crt *chain, const unsigned char *buf, size_t buflen)
 Parse one DER-encoded or one or more concatenated PEM-encoded certificates and add them to the chained list. More...
 
int mbedtls_x509_crt_parse_file (mbedtls_x509_crt *chain, const char *path)
 Load one or more certificates and add them to the chained list. Parses permissively. If some certificates can be parsed, the result is the number of failed certificates it encountered. If none complete correctly, the first error is returned. More...
 
int mbedtls_x509_crt_parse_path (mbedtls_x509_crt *chain, const char *path)
 Load one or more certificate files from a path and add them to the chained list. Parses permissively. If some certificates can be parsed, the result is the number of failed certificates it encountered. If none complete correctly, the first error is returned. More...
 
int mbedtls_x509_crt_info (char *buf, size_t size, const char *prefix, const mbedtls_x509_crt *crt)
 Returns an informational string about the certificate. More...
 
int mbedtls_x509_crt_verify_info (char *buf, size_t size, const char *prefix, uint32_t flags)
 Returns an informational string about the verification status of a certificate. More...
 
int mbedtls_x509_crt_verify (mbedtls_x509_crt *crt, mbedtls_x509_crt *trust_ca, mbedtls_x509_crl *ca_crl, const char *cn, uint32_t *flags, int(*f_vrfy)(void *, mbedtls_x509_crt *, int, uint32_t *), void *p_vrfy)
 Verify the certificate signature. More...
 
int mbedtls_x509_crt_verify_with_profile (mbedtls_x509_crt *crt, mbedtls_x509_crt *trust_ca, mbedtls_x509_crl *ca_crl, const mbedtls_x509_crt_profile *profile, const char *cn, uint32_t *flags, int(*f_vrfy)(void *, mbedtls_x509_crt *, int, uint32_t *), void *p_vrfy)
 Verify the certificate signature according to profile. More...
 
int mbedtls_x509_crt_verify_restartable (mbedtls_x509_crt *crt, mbedtls_x509_crt *trust_ca, mbedtls_x509_crl *ca_crl, const mbedtls_x509_crt_profile *profile, const char *cn, uint32_t *flags, int(*f_vrfy)(void *, mbedtls_x509_crt *, int, uint32_t *), void *p_vrfy, mbedtls_x509_crt_restart_ctx *rs_ctx)
 Restartable version of mbedtls_crt_verify_with_profile() More...
 
int mbedtls_x509_crt_check_key_usage (const mbedtls_x509_crt *crt, unsigned int usage)
 Check usage of certificate against keyUsage extension. More...
 
int mbedtls_x509_crt_check_extended_key_usage (const mbedtls_x509_crt *crt, const char *usage_oid, size_t usage_len)
 Check usage of certificate against extendedKeyUsage. More...
 
int mbedtls_x509_crt_is_revoked (const mbedtls_x509_crt *crt, const mbedtls_x509_crl *crl)
 Verify the certificate revocation status. More...
 
void mbedtls_x509_crt_init (mbedtls_x509_crt *crt)
 Initialize a certificate (chain) More...
 
void mbedtls_x509_crt_free (mbedtls_x509_crt *crt)
 Unallocate all certificate data. More...
 
#define MBEDTLS_X509_ID_FLAG(id)   ( 1 << ( (id) - 1 ) )
 
#define MBEDTLS_X509_CRT_VERSION_1   0
 
#define MBEDTLS_X509_CRT_VERSION_2   1
 
#define MBEDTLS_X509_CRT_VERSION_3   2
 
#define MBEDTLS_X509_RFC5280_MAX_SERIAL_LEN   32
 
#define MBEDTLS_X509_RFC5280_UTC_TIME_LEN   15
 
#define MBEDTLS_X509_MAX_FILE_PATH_LEN   512
 
#define MBEDTLS_X509_MAX_VERIFY_CHAIN_SIZE   ( MBEDTLS_X509_MAX_INTERMEDIATE_CA + 2 )
 

Structures and functions for X.509 Certificate Signing Requests (CSR)

int mbedtls_x509_csr_parse_der (mbedtls_x509_csr *csr, const unsigned char *buf, size_t buflen)
 Load a Certificate Signing Request (CSR) in DER format. More...
 
int mbedtls_x509_csr_parse (mbedtls_x509_csr *csr, const unsigned char *buf, size_t buflen)
 Load a Certificate Signing Request (CSR), DER or PEM format. More...
 
int mbedtls_x509_csr_parse_file (mbedtls_x509_csr *csr, const char *path)
 Load a Certificate Signing Request (CSR) More...
 
int mbedtls_x509_csr_info (char *buf, size_t size, const char *prefix, const mbedtls_x509_csr *csr)
 Returns an informational string about the CSR. More...
 
void mbedtls_x509_csr_init (mbedtls_x509_csr *csr)
 Initialize a CSR. More...
 
void mbedtls_x509_csr_free (mbedtls_x509_csr *csr)
 Unallocate all CSR data. More...
 

Data Structure Documentation

struct mbedtls_x509_time

Container for date and time (precision in seconds).

Data Fields

int day
 
int sec
 

Field Documentation

int mbedtls_x509_time::day

Date.

int mbedtls_x509_time::sec

Time.

struct mbedtls_x509_crl_entry

Certificate revocation list entry. Contains the CA-specific serial numbers and revocation dates.

struct mbedtls_x509_crl

Certificate revocation list structure. Every CRL may have multiple entries.

Data Fields

mbedtls_x509_buf raw
 
mbedtls_x509_buf tbs
 
int version
 
mbedtls_x509_buf sig_oid
 
mbedtls_x509_buf issuer_raw
 
mbedtls_x509_name issuer
 
mbedtls_x509_crl_entry entry
 
mbedtls_md_type_t sig_md
 
mbedtls_pk_type_t sig_pk
 
void * sig_opts
 

Field Documentation

mbedtls_x509_buf mbedtls_x509_crl::raw

The raw certificate data (DER).

mbedtls_x509_buf mbedtls_x509_crl::tbs

The raw certificate body (DER). The part that is To Be Signed.

int mbedtls_x509_crl::version

CRL version (1=v1, 2=v2)

mbedtls_x509_buf mbedtls_x509_crl::sig_oid

CRL signature type identifier

mbedtls_x509_buf mbedtls_x509_crl::issuer_raw

The raw issuer data (DER).

mbedtls_x509_name mbedtls_x509_crl::issuer

The parsed issuer data (named information object).

mbedtls_x509_crl_entry mbedtls_x509_crl::entry

The CRL entries containing the certificate revocation times for this CA.

mbedtls_md_type_t mbedtls_x509_crl::sig_md

Internal representation of the MD algorithm of the signature algorithm, e.g. MBEDTLS_MD_SHA256

mbedtls_pk_type_t mbedtls_x509_crl::sig_pk

Internal representation of the Public Key algorithm of the signature algorithm, e.g. MBEDTLS_PK_RSA

void* mbedtls_x509_crl::sig_opts

Signature options to be passed to mbedtls_pk_verify_ext(), e.g. for RSASSA-PSS

struct mbedtls_x509_crt

Container for an X.509 certificate. The certificate may be chained.

Data Fields

mbedtls_x509_buf raw
 
mbedtls_x509_buf tbs
 
int version
 
mbedtls_x509_buf serial
 
mbedtls_x509_buf sig_oid
 
mbedtls_x509_buf issuer_raw
 
mbedtls_x509_buf subject_raw
 
mbedtls_x509_name issuer
 
mbedtls_x509_name subject
 
mbedtls_x509_time valid_from
 
mbedtls_x509_time valid_to
 
mbedtls_pk_context pk
 
mbedtls_x509_buf issuer_id
 
mbedtls_x509_buf subject_id
 
mbedtls_x509_buf v3_ext
 
mbedtls_x509_sequence subject_alt_names
 
int ext_types
 
int ca_istrue
 
int max_pathlen
 
unsigned int key_usage
 
mbedtls_x509_sequence ext_key_usage
 
unsigned char ns_cert_type
 
mbedtls_x509_buf sig
 
mbedtls_md_type_t sig_md
 
mbedtls_pk_type_t sig_pk
 
void * sig_opts
 
struct mbedtls_x509_crt * next
 

Field Documentation

mbedtls_x509_buf mbedtls_x509_crt::raw

The raw certificate data (DER).

mbedtls_x509_buf mbedtls_x509_crt::tbs

The raw certificate body (DER). The part that is To Be Signed.

int mbedtls_x509_crt::version

The X.509 version. (1=v1, 2=v2, 3=v3)

mbedtls_x509_buf mbedtls_x509_crt::serial

Unique id for certificate issued by a specific CA.

mbedtls_x509_buf mbedtls_x509_crt::sig_oid

Signature algorithm, e.g. sha1RSA

mbedtls_x509_buf mbedtls_x509_crt::issuer_raw

The raw issuer data (DER). Used for quick comparison.

mbedtls_x509_buf mbedtls_x509_crt::subject_raw

The raw subject data (DER). Used for quick comparison.

mbedtls_x509_name mbedtls_x509_crt::issuer

The parsed issuer data (named information object).

mbedtls_x509_name mbedtls_x509_crt::subject

The parsed subject data (named information object).

mbedtls_x509_time mbedtls_x509_crt::valid_from

Start time of certificate validity.

mbedtls_x509_time mbedtls_x509_crt::valid_to

End time of certificate validity.

mbedtls_pk_context mbedtls_x509_crt::pk

Container for the public key context.

mbedtls_x509_buf mbedtls_x509_crt::issuer_id

Optional X.509 v2/v3 issuer unique identifier.

mbedtls_x509_buf mbedtls_x509_crt::subject_id

Optional X.509 v2/v3 subject unique identifier.

mbedtls_x509_buf mbedtls_x509_crt::v3_ext

Optional X.509 v3 extensions.

mbedtls_x509_sequence mbedtls_x509_crt::subject_alt_names

Optional list of Subject Alternative Names (Only dNSName supported).

int mbedtls_x509_crt::ext_types

Bit string containing detected and parsed extensions

int mbedtls_x509_crt::ca_istrue

Optional Basic Constraint extension value: 1 if this certificate belongs to a CA, 0 otherwise.

int mbedtls_x509_crt::max_pathlen

Optional Basic Constraint extension value: The maximum path length to the root certificate. Path length is 1 higher than RFC 5280 'meaning', so 1+

unsigned int mbedtls_x509_crt::key_usage

Optional key usage extension value: See the values in x509.h

mbedtls_x509_sequence mbedtls_x509_crt::ext_key_usage

Optional list of extended key usage OIDs.

unsigned char mbedtls_x509_crt::ns_cert_type

Optional Netscape certificate type extension value: See the values in x509.h

mbedtls_x509_buf mbedtls_x509_crt::sig

Signature: hash of the tbs part signed with the private key.

mbedtls_md_type_t mbedtls_x509_crt::sig_md

Internal representation of the MD algorithm of the signature algorithm, e.g. MBEDTLS_MD_SHA256

mbedtls_pk_type_t mbedtls_x509_crt::sig_pk

Internal representation of the Public Key algorithm of the signature algorithm, e.g. MBEDTLS_PK_RSA

void* mbedtls_x509_crt::sig_opts

Signature options to be passed to mbedtls_pk_verify_ext(), e.g. for RSASSA-PSS

struct mbedtls_x509_crt* mbedtls_x509_crt::next

Next certificate in the CA-chain.

struct mbedtls_x509_crt_profile

Security profile for certificate verification.

All lists are bitfields, built by ORing flags from MBEDTLS_X509_ID_FLAG().

Data Fields

uint32_t allowed_mds
 
uint32_t allowed_pks
 
uint32_t allowed_curves
 
uint32_t rsa_min_bitlen
 

Field Documentation

uint32_t mbedtls_x509_crt_profile::allowed_mds

MDs for signatures

uint32_t mbedtls_x509_crt_profile::allowed_pks

PK algs for signatures

uint32_t mbedtls_x509_crt_profile::allowed_curves

Elliptic curves for ECDSA

uint32_t mbedtls_x509_crt_profile::rsa_min_bitlen

Minimum size for RSA keys

struct mbedtls_x509write_cert

Container for writing a certificate (CRT)

struct mbedtls_x509_crt_verify_chain_item

Item in a verification chain: cert and flags for it

struct mbedtls_x509_crt_verify_chain

Verification chain as built by mbedtls_crt_verify_chain()

struct mbedtls_x509_csr

Certificate Signing Request (CSR) structure.

Data Fields

mbedtls_x509_buf raw
 
mbedtls_x509_buf cri
 
int version
 
mbedtls_x509_buf subject_raw
 
mbedtls_x509_name subject
 
mbedtls_pk_context pk
 
mbedtls_md_type_t sig_md
 
mbedtls_pk_type_t sig_pk
 
void * sig_opts
 

Field Documentation

mbedtls_x509_buf mbedtls_x509_csr::raw

The raw CSR data (DER).

mbedtls_x509_buf mbedtls_x509_csr::cri

The raw CertificateRequestInfo body (DER).

int mbedtls_x509_csr::version

CSR version (1=v1).

mbedtls_x509_buf mbedtls_x509_csr::subject_raw

The raw subject data (DER).

mbedtls_x509_name mbedtls_x509_csr::subject

The parsed subject data (named information object).

mbedtls_pk_context mbedtls_x509_csr::pk

Container for the public key context.

mbedtls_md_type_t mbedtls_x509_csr::sig_md

Internal representation of the MD algorithm of the signature algorithm, e.g. MBEDTLS_MD_SHA256

mbedtls_pk_type_t mbedtls_x509_csr::sig_pk

Internal representation of the Public Key algorithm of the signature algorithm, e.g. MBEDTLS_PK_RSA

void* mbedtls_x509_csr::sig_opts

Signature options to be passed to mbedtls_pk_verify_ext(), e.g. for RSASSA-PSS

struct mbedtls_x509write_csr

Container for writing a CSR

Macro Definition Documentation

#define MBEDTLS_X509_MAX_INTERMEDIATE_CA   8

Maximum number of intermediate CAs in a verification chain. That is, maximum length of the chain, excluding the end-entity certificate and the trusted root certificate.

Set this to a low value to prevent an adversary from making you waste resources verifying an overlong certificate chain.

#define MBEDTLS_ERR_X509_FEATURE_UNAVAILABLE   -0x2080

Unavailable feature, e.g. RSA hashing/encryption combination.

#define MBEDTLS_ERR_X509_UNKNOWN_OID   -0x2100

Requested OID is unknown.

#define MBEDTLS_ERR_X509_INVALID_FORMAT   -0x2180

The CRT/CRL/CSR format is invalid, e.g. different type expected.

#define MBEDTLS_ERR_X509_INVALID_VERSION   -0x2200

The CRT/CRL/CSR version element is invalid.

#define MBEDTLS_ERR_X509_INVALID_SERIAL   -0x2280

The serial tag or value is invalid.

#define MBEDTLS_ERR_X509_INVALID_ALG   -0x2300

The algorithm tag or value is invalid.

#define MBEDTLS_ERR_X509_INVALID_NAME   -0x2380

The name tag or value is invalid.

#define MBEDTLS_ERR_X509_INVALID_DATE   -0x2400

The date tag or value is invalid.

#define MBEDTLS_ERR_X509_INVALID_SIGNATURE   -0x2480

The signature tag or value invalid.

#define MBEDTLS_ERR_X509_INVALID_EXTENSIONS   -0x2500

The extension tag or value is invalid.

#define MBEDTLS_ERR_X509_UNKNOWN_VERSION   -0x2580

CRT/CRL/CSR has an unsupported version number.

#define MBEDTLS_ERR_X509_UNKNOWN_SIG_ALG   -0x2600

Signature algorithm (oid) is unsupported.

#define MBEDTLS_ERR_X509_SIG_MISMATCH   -0x2680

Signature algorithms do not match. (see mbedtls_x509_crt sig_oid)

#define MBEDTLS_ERR_X509_CERT_VERIFY_FAILED   -0x2700

Certificate verification failed, e.g. CRL, CA or signature check failed.

#define MBEDTLS_ERR_X509_CERT_UNKNOWN_FORMAT   -0x2780

Format not recognized as DER or PEM.

#define MBEDTLS_ERR_X509_BAD_INPUT_DATA   -0x2800

Input invalid.

#define MBEDTLS_ERR_X509_ALLOC_FAILED   -0x2880

Allocation of memory failed.

#define MBEDTLS_ERR_X509_FILE_IO_ERROR   -0x2900

Read/write of file failed.

#define MBEDTLS_ERR_X509_BUFFER_TOO_SMALL   -0x2980

Destination buffer is too small.

#define MBEDTLS_ERR_X509_FATAL_ERROR   -0x3000

A fatal error occured, eg the chain is too long or the vrfy callback failed.

#define MBEDTLS_X509_BADCERT_EXPIRED   0x01

The certificate validity has expired.

#define MBEDTLS_X509_BADCERT_REVOKED   0x02

The certificate has been revoked (is on a CRL).

#define MBEDTLS_X509_BADCERT_CN_MISMATCH   0x04

The certificate Common Name (CN) does not match with the expected CN.

#define MBEDTLS_X509_BADCERT_NOT_TRUSTED   0x08

The certificate is not correctly signed by the trusted CA.

#define MBEDTLS_X509_BADCRL_NOT_TRUSTED   0x10

The CRL is not correctly signed by the trusted CA.

#define MBEDTLS_X509_BADCRL_EXPIRED   0x20

The CRL is expired.

#define MBEDTLS_X509_BADCERT_MISSING   0x40

Certificate was missing.

#define MBEDTLS_X509_BADCERT_SKIP_VERIFY   0x80

Certificate verification was skipped.

#define MBEDTLS_X509_BADCERT_OTHER   0x0100

Other reason (can be used by verify callback)

#define MBEDTLS_X509_BADCERT_FUTURE   0x0200

The certificate validity starts in the future.

#define MBEDTLS_X509_BADCRL_FUTURE   0x0400

The CRL is from the future

#define MBEDTLS_X509_BADCERT_KEY_USAGE   0x0800

Usage does not match the keyUsage extension.

#define MBEDTLS_X509_BADCERT_EXT_KEY_USAGE   0x1000

Usage does not match the extendedKeyUsage extension.

#define MBEDTLS_X509_BADCERT_NS_CERT_TYPE   0x2000

Usage does not match the nsCertType extension.

#define MBEDTLS_X509_BADCERT_BAD_MD   0x4000

The certificate is signed with an unacceptable hash.

#define MBEDTLS_X509_BADCERT_BAD_PK   0x8000

The certificate is signed with an unacceptable PK alg (eg RSA vs ECDSA).

#define MBEDTLS_X509_BADCERT_BAD_KEY   0x010000

The certificate is signed with an unacceptable key (eg bad curve, RSA too short).

#define MBEDTLS_X509_BADCRL_BAD_MD   0x020000

The CRL is signed with an unacceptable hash.

#define MBEDTLS_X509_BADCRL_BAD_PK   0x040000

The CRL is signed with an unacceptable PK alg (eg RSA vs ECDSA).

#define MBEDTLS_X509_BADCRL_BAD_KEY   0x080000

The CRL is signed with an unacceptable key (eg bad curve, RSA too short).

#define MBEDTLS_X509_ID_FLAG (   id)    ( 1 << ( (id) - 1 ) )

Build flag from an algorithm/curve identifier (pk, md, ecp) Since 0 is always XXX_NONE, ignore it.

#define MBEDTLS_X509_MAX_VERIFY_CHAIN_SIZE   ( MBEDTLS_X509_MAX_INTERMEDIATE_CA + 2 )

Max size of verification chain: end-entity + intermediates + trusted root

Typedef Documentation

Type-length-value structure that allows for ASN1 using DER.

Container for ASN1 bit strings.

Container for ASN1 named information objects. It allows for Relative Distinguished Names (e.g. cn=localhost,ou=code,etc.).

Container for a sequence of ASN.1 items

Function Documentation

int mbedtls_dhm_parse_dhm ( mbedtls_dhm_context *  dhm,
const unsigned char *  dhmin,
size_t  dhminlen 
)
Parameters
dhmThe DHM context to import the DHM parameters into. This must be initialized.
dhminThe input buffer. This must be a readable buffer of length dhminlen Bytes.
dhminlenThe size of the input buffer dhmin, including the terminating NULL Byte for PEM data.
Returns
0 on success.
An MBEDTLS_ERR_DHM_XXX or MBEDTLS_ERR_PEM_XXX error code on failure.
int mbedtls_dhm_parse_dhmfile ( mbedtls_dhm_context *  dhm,
const char *  path 
)
Parameters
dhmThe DHM context to load the parameters to. This must be initialized.
pathThe filename to read the DHM parameters from. This must not be NULL.
Returns
0 on success.
An MBEDTLS_ERR_DHM_XXX or MBEDTLS_ERR_PEM_XXX error code on failure.
int mbedtls_x509_crl_parse_der ( mbedtls_x509_crl *  chain,
const unsigned char *  buf,
size_t  buflen 
)
Parameters
chainpoints to the start of the chain
bufbuffer holding the CRL data in DER format
buflensize of the buffer (including the terminating null byte for PEM data)
Returns
0 if successful, or a specific X509 or PEM error code
int mbedtls_x509_crl_parse ( mbedtls_x509_crl *  chain,
const unsigned char *  buf,
size_t  buflen 
)
Note
Mutliple CRLs are accepted only if using PEM format
Parameters
chainpoints to the start of the chain
bufbuffer holding the CRL data in PEM or DER format
buflensize of the buffer (including the terminating null byte for PEM data)
Returns
0 if successful, or a specific X509 or PEM error code
int mbedtls_x509_crl_parse_file ( mbedtls_x509_crl *  chain,
const char *  path 
)
Note
Mutliple CRLs are accepted only if using PEM format
Parameters
chainpoints to the start of the chain
pathfilename to read the CRLs from (in PEM or DER encoding)
Returns
0 if successful, or a specific X509 or PEM error code
int mbedtls_x509_crl_info ( char *  buf,
size_t  size,
const char *  prefix,
const mbedtls_x509_crl *  crl 
)
Parameters
bufBuffer to write to
sizeMaximum size of buffer
prefixA line prefix
crlThe X509 CRL to represent
Returns
The length of the string written (not including the terminated nul byte), or a negative error code.
void mbedtls_x509_crl_init ( mbedtls_x509_crl *  crl)
Parameters
crlCRL chain to initialize
void mbedtls_x509_crl_free ( mbedtls_x509_crl *  crl)
Parameters
crlCRL chain to free
int mbedtls_x509_crt_parse_der ( mbedtls_x509_crt *  chain,
const unsigned char *  buf,
size_t  buflen 
)
Parameters
chainpoints to the start of the chain
bufbuffer holding the certificate DER data
buflensize of the buffer
Returns
0 if successful, or a specific X509 or PEM error code
int mbedtls_x509_crt_parse ( mbedtls_x509_crt *  chain,
const unsigned char *  buf,
size_t  buflen 
)
            For CRTs in PEM encoding, the function parses permissively:
            if at least one certificate can be parsed, the function
            returns the number of certificates for which parsing failed
            (hence \c 0 if all certificates were parsed successfully).
            If no certificate could be parsed, the function returns
            the first (negative) error encountered during parsing.

            PEM encoded certificates may be interleaved by other data
            such as human readable descriptions of their content, as
            long as the certificates are enclosed in the PEM specific
            '-----{BEGIN/END} CERTIFICATE-----' delimiters.
Parameters
chainThe chain to which to add the parsed certificates.
bufThe buffer holding the certificate data in PEM or DER format. For certificates in PEM encoding, this may be a concatenation of multiple certificates; for DER encoding, the buffer must comprise exactly one certificate.
buflenThe size of buf, including the terminating NULL byte in case of PEM encoded data.
Returns
0 if all certificates were parsed successfully.
The (positive) number of certificates that couldn't be parsed if parsing was partly successful (see above).
A negative X509 or PEM error code otherwise.
int mbedtls_x509_crt_parse_file ( mbedtls_x509_crt *  chain,
const char *  path 
)
Parameters
chainpoints to the start of the chain
pathfilename to read the certificates from
Returns
0 if all certificates parsed successfully, a positive number if partly successful or a specific X509 or PEM error code
int mbedtls_x509_crt_parse_path ( mbedtls_x509_crt *  chain,
const char *  path 
)
Parameters
chainpoints to the start of the chain
pathdirectory / folder to read the certificate files from
Returns
0 if all certificates parsed successfully, a positive number if partly successful or a specific X509 or PEM error code
int mbedtls_x509_crt_info ( char *  buf,
size_t  size,
const char *  prefix,
const mbedtls_x509_crt *  crt 
)
Parameters
bufBuffer to write to
sizeMaximum size of buffer
prefixA line prefix
crtThe X509 certificate to represent
Returns
The length of the string written (not including the terminated nul byte), or a negative error code.
int mbedtls_x509_crt_verify_info ( char *  buf,
size_t  size,
const char *  prefix,
uint32_t  flags 
)
Parameters
bufBuffer to write to
sizeMaximum size of buffer
prefixA line prefix
flagsVerification flags created by mbedtls_x509_crt_verify()
Returns
The length of the string written (not including the terminated nul byte), or a negative error code.
int mbedtls_x509_crt_verify ( mbedtls_x509_crt *  crt,
mbedtls_x509_crt *  trust_ca,
mbedtls_x509_crl *  ca_crl,
const char *  cn,
uint32_t *  flags,
int(*)(void *, mbedtls_x509_crt *, int, uint32_t *)  f_vrfy,
void *  p_vrfy 
)
            The verify callback is a user-supplied callback that
            can clear / modify / add flags for a certificate. If set,
            the verification callback is called for each
            certificate in the chain (from the trust-ca down to the
            presented crt). The parameters for the callback are:
            (void *parameter, mbedtls_x509_crt *crt, int certificate_depth,
            int *flags). With the flags representing current flags for
            that specific certificate and the certificate depth from
            the bottom (Peer cert depth = 0).

            All flags left after returning from the callback
            are also returned to the application. The function should
            return 0 for anything (including invalid certificates)
            other than fatal error, as a non-zero return code
            immediately aborts the verification process. For fatal
            errors, a specific error code should be used (different
            from MBEDTLS_ERR_X509_CERT_VERIFY_FAILED which should not
            be returned at this point), or MBEDTLS_ERR_X509_FATAL_ERROR
            can be used if no better code is available.
Note
In case verification failed, the results can be displayed using mbedtls_x509_crt_verify_info()
Same as mbedtls_x509_crt_verify_with_profile() with the default security profile.
It is your responsibility to provide up-to-date CRLs for all trusted CAs. If no CRL is provided for the CA that was used to sign the certificate, CRL verification is skipped silently, that is without setting any flag.
The trust_ca list can contain two types of certificates: (1) those of trusted root CAs, so that certificates chaining up to those CAs will be trusted, and (2) self-signed end-entity certificates to be trusted (for specific peers you know) - in that case, the self-signed certificate doesn't need to have the CA bit set.
Parameters
crta certificate (chain) to be verified
trust_cathe list of trusted CAs (see note above)
ca_crlthe list of CRLs for trusted CAs (see note above)
cnexpected Common Name (can be set to NULL if the CN must not be verified)
flagsresult of the verification
f_vrfyverification function
p_vrfyverification parameter
Returns
0 (and flags set to 0) if the chain was verified and valid, MBEDTLS_ERR_X509_CERT_VERIFY_FAILED if the chain was verified but found to be invalid, in which case *flags will have one or more MBEDTLS_X509_BADCERT_XXX or MBEDTLS_X509_BADCRL_XXX flags set, or another error (and flags set to 0xffffffff) in case of a fatal error encountered during the verification process.
int mbedtls_x509_crt_verify_with_profile ( mbedtls_x509_crt *  crt,
mbedtls_x509_crt *  trust_ca,
mbedtls_x509_crl *  ca_crl,
const mbedtls_x509_crt_profile *  profile,
const char *  cn,
uint32_t *  flags,
int(*)(void *, mbedtls_x509_crt *, int, uint32_t *)  f_vrfy,
void *  p_vrfy 
)
Note
Same as mbedtls_x509_crt_verify(), but with explicit security profile.
The restrictions on keys (RSA minimum size, allowed curves for ECDSA) apply to all certificates: trusted root, intermediate CAs if any, and end entity certificate.
Parameters
crta certificate (chain) to be verified
trust_cathe list of trusted CAs
ca_crlthe list of CRLs for trusted CAs
profilesecurity profile for verification
cnexpected Common Name (can be set to NULL if the CN must not be verified)
flagsresult of the verification
f_vrfyverification function
p_vrfyverification parameter
Returns
0 if successful or MBEDTLS_ERR_X509_CERT_VERIFY_FAILED in which case *flags will have one or more MBEDTLS_X509_BADCERT_XXX or MBEDTLS_X509_BADCRL_XXX flags set, or another error in case of a fatal error encountered during the verification process.
int mbedtls_x509_crt_verify_restartable ( mbedtls_x509_crt *  crt,
mbedtls_x509_crt *  trust_ca,
mbedtls_x509_crl *  ca_crl,
const mbedtls_x509_crt_profile *  profile,
const char *  cn,
uint32_t *  flags,
int(*)(void *, mbedtls_x509_crt *, int, uint32_t *)  f_vrfy,
void *  p_vrfy,
mbedtls_x509_crt_restart_ctx *  rs_ctx 
)
Note
Performs the same job as mbedtls_crt_verify_with_profile() but can return early and restart according to the limit set with mbedtls_ecp_set_max_ops() to reduce blocking.
Parameters
crta certificate (chain) to be verified
trust_cathe list of trusted CAs
ca_crlthe list of CRLs for trusted CAs
profilesecurity profile for verification
cnexpected Common Name (can be set to NULL if the CN must not be verified)
flagsresult of the verification
f_vrfyverification function
p_vrfyverification parameter
rs_ctxrestart context (NULL to disable restart)
Returns
See mbedtls_crt_verify_with_profile(), or
#MBEDTLS_ERR_ECP_IN_PROGRESS if maximum number of operations was reached: see mbedtls_ecp_set_max_ops().
int mbedtls_x509_crt_check_key_usage ( const mbedtls_x509_crt *  crt,
unsigned int  usage 
)
Parameters
crtLeaf certificate used.
usageIntended usage(s) (eg MBEDTLS_X509_KU_KEY_ENCIPHERMENT before using the certificate to perform an RSA key exchange).
Note
Except for decipherOnly and encipherOnly, a bit set in the usage argument means this bit MUST be set in the certificate. For decipherOnly and encipherOnly, it means that bit MAY be set.
Returns
0 is these uses of the certificate are allowed, MBEDTLS_ERR_X509_BAD_INPUT_DATA if the keyUsage extension is present but does not match the usage argument.
Note
You should only call this function on leaf certificates, on (intermediate) CAs the keyUsage extension is automatically checked by mbedtls_x509_crt_verify().
int mbedtls_x509_crt_check_extended_key_usage ( const mbedtls_x509_crt *  crt,
const char *  usage_oid,
size_t  usage_len 
)
Parameters
crtLeaf certificate used.
usage_oidIntended usage (eg MBEDTLS_OID_SERVER_AUTH or MBEDTLS_OID_CLIENT_AUTH).
usage_lenLength of usage_oid (eg given by MBEDTLS_OID_SIZE()).
Returns
0 if this use of the certificate is allowed, MBEDTLS_ERR_X509_BAD_INPUT_DATA if not.
Note
Usually only makes sense on leaf certificates.
int mbedtls_x509_crt_is_revoked ( const mbedtls_x509_crt *  crt,
const mbedtls_x509_crl *  crl 
)
Parameters
crta certificate to be verified
crlthe CRL to verify against
Returns
1 if the certificate is revoked, 0 otherwise
void mbedtls_x509_crt_init ( mbedtls_x509_crt *  crt)
Parameters
crtCertificate chain to initialize
void mbedtls_x509_crt_free ( mbedtls_x509_crt *  crt)
Parameters
crtCertificate chain to free
int mbedtls_x509_csr_parse_der ( mbedtls_x509_csr *  csr,
const unsigned char *  buf,
size_t  buflen 
)
Note
CSR attributes (if any) are currently silently ignored.
Parameters
csrCSR context to fill
bufbuffer holding the CRL data
buflensize of the buffer
Returns
0 if successful, or a specific X509 error code
int mbedtls_x509_csr_parse ( mbedtls_x509_csr *  csr,
const unsigned char *  buf,
size_t  buflen 
)
Note
See notes for mbedtls_x509_csr_parse_der()
Parameters
csrCSR context to fill
bufbuffer holding the CRL data
buflensize of the buffer (including the terminating null byte for PEM data)
Returns
0 if successful, or a specific X509 or PEM error code
int mbedtls_x509_csr_parse_file ( mbedtls_x509_csr *  csr,
const char *  path 
)
Note
See notes for mbedtls_x509_csr_parse()
Parameters
csrCSR context to fill
pathfilename to read the CSR from
Returns
0 if successful, or a specific X509 or PEM error code
int mbedtls_x509_csr_info ( char *  buf,
size_t  size,
const char *  prefix,
const mbedtls_x509_csr *  csr 
)
Parameters
bufBuffer to write to
sizeMaximum size of buffer
prefixA line prefix
csrThe X509 CSR to represent
Returns
The length of the string written (not including the terminated nul byte), or a negative error code.
void mbedtls_x509_csr_init ( mbedtls_x509_csr *  csr)
Parameters
csrCSR to initialize
void mbedtls_x509_csr_free ( mbedtls_x509_csr *  csr)
Parameters
csrCSR to free

Variable Documentation

const mbedtls_x509_crt_profile mbedtls_x509_crt_profile_default

Default security profile. Should provide a good balance between security and compatibility with current deployments.

const mbedtls_x509_crt_profile mbedtls_x509_crt_profile_next

Expected next default profile. Recommended for new deployments. Currently targets a 128-bit security level, except for RSA-2048.

const mbedtls_x509_crt_profile mbedtls_x509_crt_profile_suiteb

NSA Suite B profile.