|  | MCUXpresso SDK API Reference Manual
    Rev. 0
    NXP Semiconductors | 
| Data Structures | |
| struct | nand_onfi_parameter_config_t | 
| Parallel NAND ONFI parameter config.  More... | |
| struct | nand_onfi_feature_config_t | 
| Parallel NAND ONFI feature config.  More... | |
| struct | semc_mem_nand_config_t | 
| SEMC NAND Flash Config block structure.  More... | |
| struct | semc_mem_nand_handle_t | 
| NAND Flash handle info.  More... | |
| Typedefs | |
| typedef void(* | delay_us )(uint32_t us) | 
| us delay function pointer | |
| Enumerations | |
| enum | _nand_vendor_type_index | 
| NAND Flash vendor type. | |
| enum | _nand_ac_timing_table_index | 
| Parallel NAND Flash AC timing mode. | |
| enum | _nand_onfi_command_set | 
| Parallel NAND Flash commands. | |
| enum | nand_onfi_version_t | 
| Parallel NAND Flash ONFI Version. | |
| enum | nand_status_command_type_t | 
| Parallel NAND Flash Status Command Type. | |
| enum | nand_change_readcolumn_command_type_t | 
| Parallel NAND Flash change read column Command Type. | |
| enum | nand_ecc_check_type_t | 
| NAND Flash ecc check type. | |
| enum | nand_ready_check_option_t { kNandReadyCheckOption_SR = 0U, kNandReadyCheckOption_RB = 1U } | 
| Parallel NAND Flash Ready check option.  More... | |
| struct nand_onfi_parameter_config_t | 
| Data Fields | |
| uint32_t | signature | 
| [0x000-0x003] | |
| uint16_t | revisionNumber | 
| [0x004-0x005] | |
| struct { | |
| } | supportedFeatures | 
| [0x006-0x007] | |
| struct { | |
| } | optionalCommands | 
| [0x008-0x009] | |
| uint8_t | reserved0 [22] | 
| [0x00a-0x01f] | |
| uint8_t | deviceManufacturer [12] | 
| [0x020-0x02b] | |
| uint8_t | deviceModel [20] | 
| [0x02c-0x03f] | |
| uint8_t | JEDECid | 
| [0x040-0x040] | |
| uint8_t | dataCode [2] | 
| [0x041-0x042] | |
| uint8_t | reserved1 [13] | 
| [0x043-0x04f] | |
| uint32_t | dataBytesPerPage | 
| [0x050-0x053] | |
| uint16_t | spareBytesPerPage | 
| [0x054-0x055] | |
| uint8_t | reserved2 [6] | 
| [0x056-0x05b] | |
| uint32_t | pagesPerBlock | 
| [0x05c-0x05f] | |
| uint32_t | blocksPerLUN | 
| [0x060-0x063] | |
| uint8_t | LUNsPerDevice | 
| [0x064-0x064] | |
| union { | |
| }; | |
| [0x065-0x065] | |
| uint8_t | reserved3 [26] | 
| [0x066-0x07f] | |
| uint8_t | reserved4 | 
| [0x080-0x080] | |
| struct { | |
| } | timingMode | 
| [0x081-0x081] | |
| uint8_t | reserved5 [3] | 
| [0x082-0x084] | |
| uint8_t | maxPageProgramTimeInUs [2] | 
| [0x085-0x086] | |
| uint8_t | maxBlockEraseTimeInUs [2] | 
| [0x087-0x088] | |
| uint8_t | maxPageReadTimeInUs [2] | 
| [0x089-0x08a] | |
| uint8_t | minChangeColunmSetupTimeInNs [2] | 
| [0x08b-0x08c] | |
| uint8_t | reserved6 [23] | 
| [0x08d-0x0a3] | |
| uint16_t | vendorSpecificRevisionNumber | 
| [0x0a4-0x0a5] | |
| uint8_t | reserved7 [88] | 
| [0x0a6-0x0fd] | |
| uint16_t | integrityCRC | 
| [0x0fe-0x0ff] | |
| struct nand_onfi_feature_config_t | 
| struct semc_mem_nand_config_t | 
| Data Fields | |
| semc_nand_config_t * | semcNandConfig | 
| memory controller configuration, shoule bd configured with controller  configure structure.  More... | |
| uint32_t | clkSrc_Hz | 
| The async clock frequency. | |
| delay_us | delayUS | 
| delay function pointer, application should prepare a delay function for it | |
| nand_onfi_version_t | onfiVersion | 
| only onfi nand flash will be supported currently.  More... | |
| uint8_t | readyCheckOption | 
| Set with enum type defined in "nand_ready_check_option_t". | |
| nand_ecc_check_type_t | eccCheckType | 
| Soft/device ECC check.  More... | |
| semc_nand_config_t* semc_mem_nand_config_t::semcNandConfig | 
| nand_onfi_version_t semc_mem_nand_config_t::onfiVersion | 
| nand_ecc_check_type_t semc_mem_nand_config_t::eccCheckType | 
| struct semc_mem_nand_handle_t | 
| Data Fields | |
| delay_us | delayUS | 
| delay function pointer, application should prepare a delay function for it | |
| uint32_t | ctlAccessMemAddr1 | 
| Nand memory address for memory controller access.  More... | |
| uint32_t | ctlAccessMemAddr2 | 
| Nand memory address for memory controller access.  More... | |
| uint8_t | readyCheckOption | 
| Set with enum type defined in "nand_ready_check_option_t". | |
| nand_ecc_check_type_t | eccCheckType | 
| Soft/device ECC check.  More... | |
| uint8_t | statusCommandType | 
| the command enhanced mode or normal command mode | |
| uint8_t | changeReadColumnType | 
| the change read column type.  More... | |
| uint8_t | columnWidth | 
| the Colum width setting in the controller.  More... | |
| bool | isFeatureCommandSupport | 
| feature command support .  More... | |
| uint32_t | rowAddressToGetSR | 
| Row address for read status enhanced command. | |
| uint32_t | pageReadTimeInUs_tR | 
| Page read time delay. | |
| uint32_t | PageProgramTimeInUs_tPROG | 
| Page program time delay. | |
| uint32_t | blockEraseTimeInUs_tBERS | 
| block erase time delay | |
| uint32_t | changeColumnSetupTimeInNs_tCCS | 
| Change column setup time delay. | |
| uint32_t semc_mem_nand_handle_t::ctlAccessMemAddr1 | 
| uint32_t semc_mem_nand_handle_t::ctlAccessMemAddr2 | 
| nand_ecc_check_type_t semc_mem_nand_handle_t::eccCheckType | 
| uint8_t semc_mem_nand_handle_t::changeReadColumnType | 
| uint8_t semc_mem_nand_handle_t::columnWidth | 
| bool semc_mem_nand_handle_t::isFeatureCommandSupport |