![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Macros | |
| #define | SNTP_SET_SYSTEM_TIME(sec) LWIP_UNUSED_ARG(sec) |
| #define | SNTP_MAX_SERVERS LWIP_DHCP_MAX_NTP_SERVERS |
| #define | SNTP_GET_SERVERS_FROM_DHCP LWIP_DHCP_GET_NTP_SRV |
| #define | SNTP_GET_SERVERS_FROM_DHCPV6 LWIP_DHCP6_GET_NTP_SRV |
| #define | SNTP_SERVER_DNS 0 |
| #define | SNTP_DEBUG LWIP_DBG_OFF |
| #define | SNTP_PORT LWIP_IANA_PORT_SNTP |
| #define | SNTP_CHECK_RESPONSE 0 |
| #define | SNTP_COMP_ROUNDTRIP 0 |
| #define | SNTP_STARTUP_DELAY 0 |
| #define | SNTP_STARTUP_DELAY_FUNC (LWIP_RAND() % 5000) |
| #define | SNTP_RECV_TIMEOUT 15000 |
| #define | SNTP_UPDATE_DELAY 3600000 |
| #define | SNTP_GET_SYSTEM_TIME(sec, us) do { (sec) = 0; (us) = 0; } while(0) |
| #define | SNTP_RETRY_TIMEOUT SNTP_RECV_TIMEOUT |
| #define | SNTP_RETRY_TIMEOUT_MAX (SNTP_RETRY_TIMEOUT * 10) |
| #define | SNTP_RETRY_TIMEOUT_EXP 1 |
| #define | SNTP_MONITOR_SERVER_REACHABILITY 1 |
| #define SNTP_SET_SYSTEM_TIME | ( | sec | ) | LWIP_UNUSED_ARG(sec) |
SNTP macro to change system time in seconds Define SNTP_SET_SYSTEM_TIME_US(sec, us) to set the time in microseconds instead of this one if you need the additional precision. Alternatively, define SNTP_SET_SYSTEM_TIME_NTP(sec, frac) in order to work with native NTP timestamps instead.
| #define SNTP_MAX_SERVERS LWIP_DHCP_MAX_NTP_SERVERS |
The maximum number of SNTP servers that can be set
| #define SNTP_GET_SERVERS_FROM_DHCP LWIP_DHCP_GET_NTP_SRV |
Set this to 1 to implement the callback function called by dhcp when NTP servers are received.
| #define SNTP_GET_SERVERS_FROM_DHCPV6 LWIP_DHCP6_GET_NTP_SRV |
Set this to 1 to implement the callback function called by dhcpv6 when NTP servers are received.
| #define SNTP_SERVER_DNS 0 |
Set this to 1 to support DNS names (or IP address strings) to set sntp servers One server address/name can be defined as default if SNTP_SERVER_DNS == 1: #define SNTP_SERVER_ADDRESS "pool.ntp.org"
| #define SNTP_DEBUG LWIP_DBG_OFF |
SNTP_DEBUG: Enable debugging for SNTP.
| #define SNTP_PORT LWIP_IANA_PORT_SNTP |
SNTP server port
| #define SNTP_CHECK_RESPONSE 0 |
Sanity check: Define this to
| #define SNTP_COMP_ROUNDTRIP 0 |
Enable round-trip delay compensation. Compensate for the round-trip delay by calculating the clock offset from the originate, receive, transmit and destination timestamps, as per RFC.
The calculation requires compiler support for 64-bit integers. Also, either SNTP_SET_SYSTEM_TIME_US or SNTP_SET_SYSTEM_TIME_NTP has to be implemented for setting the system clock with sub-second precision. Likewise, either SNTP_GET_SYSTEM_TIME or SNTP_GET_SYSTEM_TIME_NTP needs to be implemented with sub-second precision.
Although not strictly required, it makes sense to combine this option with SNTP_CHECK_RESPONSE >= 2 for sanity-checking of the received timestamps. Also, in order for the round-trip calculation to work, the difference between the local clock and the NTP server clock must not be larger than about 34 years. If that limit is exceeded, the implementation will fall back to setting the clock without compensation. In order to ensure that the local clock is always within the permitted range for compensation, even at first try, it may be necessary to store at least the current year in non-volatile memory.
| #define SNTP_STARTUP_DELAY 0 |
According to the RFC, this shall be a random delay between 1 and 5 minutes (in milliseconds) to prevent load peaks. This can be defined to a random generation function, which must return the delay in milliseconds as u32_t. Turned off by default.
| #define SNTP_STARTUP_DELAY_FUNC (LWIP_RAND() % 5000) |
If you want the startup delay to be a function, define this to a function (including the brackets) and define SNTP_STARTUP_DELAY to 1.
| #define SNTP_RECV_TIMEOUT 15000 |
SNTP receive timeout - in milliseconds Also used as retry timeout - this shouldn't be too low. Default is 15 seconds. Must not be beolw 15 seconds by specification (i.e. 15000)
| #define SNTP_UPDATE_DELAY 3600000 |
SNTP update delay - in milliseconds Default is 1 hour. Must not be beolw 60 seconds by specification (i.e. 60000)
| #define SNTP_GET_SYSTEM_TIME | ( | sec, | |
| us | |||
| ) | do { (sec) = 0; (us) = 0; } while(0) |
SNTP macro to get system time, used with SNTP_CHECK_RESPONSE >= 2 to send in request and compare in response. Also used for round-trip delay compensation if SNTP_COMP_ROUNDTRIP != 0. Alternatively, define SNTP_GET_SYSTEM_TIME_NTP(sec, frac) in order to work with native NTP timestamps instead.
| #define SNTP_RETRY_TIMEOUT SNTP_RECV_TIMEOUT |
Default retry timeout (in milliseconds) if the response received is invalid. This is doubled with each retry until SNTP_RETRY_TIMEOUT_MAX is reached.
| #define SNTP_RETRY_TIMEOUT_MAX (SNTP_RETRY_TIMEOUT * 10) |
Maximum retry timeout (in milliseconds).
| #define SNTP_RETRY_TIMEOUT_EXP 1 |
Increase retry timeout with every retry sent Default is on to conform to RFC.
| #define SNTP_MONITOR_SERVER_REACHABILITY 1 |
Keep a reachability shift register per server Default is on to conform to RFC.