![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
ASN1 Error codes | |
These error codes are OR'ed to X509 error codes for higher error granularity. ASN1 is a standard to specify data structures. | |
| #define | MBEDTLS_ERR_ASN1_OUT_OF_DATA -0x0060 |
| #define | MBEDTLS_ERR_ASN1_UNEXPECTED_TAG -0x0062 |
| #define | MBEDTLS_ERR_ASN1_INVALID_LENGTH -0x0064 |
| #define | MBEDTLS_ERR_ASN1_LENGTH_MISMATCH -0x0066 |
| #define | MBEDTLS_ERR_ASN1_INVALID_DATA -0x0068 |
| #define | MBEDTLS_ERR_ASN1_ALLOC_FAILED -0x006A |
| #define | MBEDTLS_ERR_ASN1_BUF_TOO_SMALL -0x006C |
DER constants | |
These constants comply with the DER encoded ASN.1 type tags. DER encoding uses hexadecimal representation. An example DER sequence is:
| |
| #define | MBEDTLS_ASN1_BOOLEAN 0x01 |
| #define | MBEDTLS_ASN1_INTEGER 0x02 |
| #define | MBEDTLS_ASN1_BIT_STRING 0x03 |
| #define | MBEDTLS_ASN1_OCTET_STRING 0x04 |
| #define | MBEDTLS_ASN1_NULL 0x05 |
| #define | MBEDTLS_ASN1_OID 0x06 |
| #define | MBEDTLS_ASN1_UTF8_STRING 0x0C |
| #define | MBEDTLS_ASN1_SEQUENCE 0x10 |
| #define | MBEDTLS_ASN1_SET 0x11 |
| #define | MBEDTLS_ASN1_PRINTABLE_STRING 0x13 |
| #define | MBEDTLS_ASN1_T61_STRING 0x14 |
| #define | MBEDTLS_ASN1_IA5_STRING 0x16 |
| #define | MBEDTLS_ASN1_UTC_TIME 0x17 |
| #define | MBEDTLS_ASN1_GENERALIZED_TIME 0x18 |
| #define | MBEDTLS_ASN1_UNIVERSAL_STRING 0x1C |
| #define | MBEDTLS_ASN1_BMP_STRING 0x1E |
| #define | MBEDTLS_ASN1_PRIMITIVE 0x00 |
| #define | MBEDTLS_ASN1_CONSTRUCTED 0x20 |
| #define | MBEDTLS_ASN1_CONTEXT_SPECIFIC 0x80 |
| #define | MBEDTLS_ASN1_TAG_CLASS_MASK 0xC0 |
| #define | MBEDTLS_ASN1_TAG_PC_MASK 0x20 |
| #define | MBEDTLS_ASN1_TAG_VALUE_MASK 0x1F |
| #define MBEDTLS_ERR_ASN1_OUT_OF_DATA -0x0060 |
Out of data when parsing an ASN1 data structure.
| #define MBEDTLS_ERR_ASN1_UNEXPECTED_TAG -0x0062 |
ASN1 tag was of an unexpected value.
| #define MBEDTLS_ERR_ASN1_INVALID_LENGTH -0x0064 |
Error when trying to determine the length or invalid length.
| #define MBEDTLS_ERR_ASN1_LENGTH_MISMATCH -0x0066 |
Actual length differs from expected length.
| #define MBEDTLS_ERR_ASN1_INVALID_DATA -0x0068 |
Data is invalid. (not used)
| #define MBEDTLS_ERR_ASN1_ALLOC_FAILED -0x006A |
Memory allocation failed
| #define MBEDTLS_ERR_ASN1_BUF_TOO_SMALL -0x006C |
Buffer too small when writing ASN.1 data structure.