The MCUXpresso SDK provides a peripheral driver for the General Purpose I/O (GPIO) module of MCUXpresso SDK devices.
Function groups
Initialization and deinitialization
The function GPIO_PinInit() initializes the GPIO with specified configuration.
Pin manipulation
The function GPIO_WritePinOutput() set output state of the selected GPIO pin. The function GPIO_ReadPinInput() read input value of the selected GPIO pin.
Port manipulation
The function GPIO_SetPinsOutput() sets the output level of selected GPIO pins to the logic 1. The function GPIO_ClearPinsOutput() sets the output level of selected GPIO pins to the logic 1. The function GPIO_TogglePinsOutput() reverse the output level of selected GPIO pins.
Typical use case
Example use of GPIO API.
int main(void)
{
BOARD_InitHardware();
while (1)
{
delay(500000);
delay(500000);
delay(500000);
}
}
|
| static void | GPIO_WritePinOutput (GPIO_Type *base, uint32_t pin, uint8_t output) |
| | Sets the output level of a GPIO pin to the logic 1 or 0. More...
|
| |
| static void | GPIO_SetPinsOutput (GPIO_Type *base, uint32_t mask) |
| | Sets the output level of the multiple GPIO pins to the logic 1. More...
|
| |
| static void | GPIO_ClearPinsOutput (GPIO_Type *base, uint32_t mask) |
| | Sets the output level of the multiple GPIO pins to the logic 0. More...
|
| |
| static void | GPIO_TogglePinsOutput (GPIO_Type *base, uint32_t mask) |
| | Reverses current output logic of the multiple GPIO pins. More...
|
| |
|
| static uint32_t | GPIO_ReadPinInput (GPIO_Type *base, uint32_t pin) |
| | Reads the current input value of the whole GPIO port. More...
|
| |
Every pin can only be configured as either output pin or input pin at a time. If configured as a input pin, then leave the outputLogic unused
| Enumerator |
|---|
| kGPIO_DigitalInput |
Set current pin as digital input.
|
| kGPIO_DigitalOutput |
Set current pin as digital output.
|
| void GPIO_PinInit |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
pin, |
|
|
const gpio_pin_config_t * |
config |
|
) |
| |
To initialize the GPIO, define a pin configuration, either input or output, in the user file. Then, call the GPIO_PinInit() function.
This is an example to define an input pin or output pin configuration:
*
* {
* 0,
* }
*
* {
* 0,
* }
*
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| pin | GPIO port pin number |
| config | GPIO pin configuration pointer |
| static void GPIO_WritePinOutput |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
pin, |
|
|
uint8_t |
output |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| pin | GPIO pin number |
| output | GPIO pin output logic level.
- 0: corresponding pin output low-logic level.
- 1: corresponding pin output high-logic level.
|
| static void GPIO_SetPinsOutput |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_ClearPinsOutput |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_TogglePinsOutput |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static uint32_t GPIO_ReadPinInput |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
pin |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| pin | GPIO pin number |
- Return values
-
| GPIO | port input value
- 0: corresponding pin input low-logic level.
- 1: corresponding pin input high-logic level.
|
| static uint32_t GPIO_GetPinsInterruptFlags |
( |
GPIO_Type * |
base | ) |
|
|
inlinestatic |
The flag remains set until a logic one is written to that flag. If configured for a level sensitive interrupt that remains asserted, the flag is set again immediately.
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
- Return values
-
| Current | GPIO port interrupt status flag, for example, 0x00010001 means the pin 0 and 17 have the interrupt. |
| static void GPIO_ClearPinsInterruptFlags |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_SetHighLevelInterrupt |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_SetRisingEdgeInterrupt |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_SetLowLevelInterrupt |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_SetFallingEdgeInterrupt |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_EnableInterrupt |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |
| static void GPIO_DisableInterrupt |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(GPIOA, GPIOB.) |
| mask | GPIO pin number macro |