![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the System Configuration (SYSCON) module of MCUXpresso SDK devices.
Modules | |
| Clock driver | |
Files | |
| file | fsl_syscon.h |
Functions | |
| __STATIC_INLINE void | SYSCON_SetLoadCap (SYSCON_Type *base, uint8_t xtalType, uint8_t loadCap) |
| Sets load cap for on bard crystal. More... | |
Driver version | |
| #define | LPC_SYSCON_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| SYSCON driver version 2.0.0. More... | |
| #define LPC_SYSCON_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| __STATIC_INLINE void SYSCON_SetLoadCap | ( | SYSCON_Type * | base, |
| uint8_t | xtalType, | ||
| uint8_t | loadCap | ||
| ) |
| base | The base of SYSCON peripheral on the chip |
| xtalType | XTAL type (1 : 16/32MHz, 0: 32KHz) |
| loadCap | load cap value |