![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Input/Output Pad Controller.
The IOPCTL, working in conjunction with the PIMCTL, enables the chip to share one pad for multiple signals from different peripheral interfaces.
Files | |
| file | fsl_iopctl.h |
Data Structures | |
| struct | iopctl_group_t |
| Array of IOPCTL pin definitions passed to IOPCTL_SetPinMuxing() must be in this format. More... | |
Macros | |
| #define | IOPCTL_FUNC0 0x0 |
| IOPCTL function and mode selection definitions. More... | |
| #define | IOPCTL_FUNC1 0x1 |
| Selects pin function 1. | |
| #define | IOPCTL_FUNC2 0x2 |
| Selects pin function 2. | |
| #define | IOPCTL_FUNC3 0x3 |
| Selects pin function 3. | |
| #define | IOPCTL_FUNC4 0x4 |
| Selects pin function 4. | |
| #define | IOPCTL_FUNC5 0x5 |
| Selects pin function 5. | |
| #define | IOPCTL_FUNC6 0x6 |
| Selects pin function 6. | |
| #define | IOPCTL_FUNC7 0x7 |
| Selects pin function 7. | |
| #define | IOPCTL_FUNC8 0x8 |
| Selects pin function 8. | |
| #define | IOPCTL_FUNC9 0x9 |
| Selects pin function 9. | |
| #define | IOPCTL_FUNC10 0xA |
| Selects pin function 10. | |
| #define | IOPCTL_FUNC11 0xB |
| Selects pin function 11. | |
| #define | IOPCTL_FUNC12 0xC |
| Selects pin function 12. | |
| #define | IOPCTL_FUNC13 0xD |
| Selects pin function 13. | |
| #define | IOPCTL_FUNC14 0xE |
| Selects pin function 14. | |
| #define | IOPCTL_FUNC15 0xF |
| Selects pin function 15. | |
| #define | IOPCTL_PUPD_EN (0x1 << 4) |
| Enables Pullup / Pulldown. | |
| #define | IOPCTL_PULLDOWN_EN (0x0 << 5) |
| Selects pull-down function. | |
| #define | IOPCTL_PULLUP_EN (0x1 << 5) |
| Selects pull-up function. | |
| #define | IOPCTL_INBUF_EN (0x1 << 6) |
| Enables buffer function on input. | |
| #define | IOPCTL_SLEW_RATE (0x0 << 7) |
| Slew Rate Control. | |
| #define | IOPCTL_FULLDRIVE_EN (0x1 << 8) |
| Selects full drive. | |
| #define | IOPCTL_ANAMUX_EN (0x1 << 9) |
| Enables analog mux function by setting 0 to bit 7. | |
| #define | IOPCTL_PSEDRAIN_EN (0x1 << 10) |
| Enables pseudo output drain function. | |
| #define | IOPCTL_INV_EN (0x1 << 11) |
| Enables invert function on input. | |
Functions | |
| __STATIC_INLINE void | IOPCTL_PinMuxSet (IOPCTL_Type *base, uint8_t port, uint8_t pin, uint32_t modefunc) |
| Sets I/O Pad Control pin mux. More... | |
| __STATIC_INLINE void | IOPCTL_SetPinMuxing (IOPCTL_Type *base, const iopctl_group_t *pinArray, uint32_t arrayLength) |
| Set all I/O Control pin muxing. More... | |
Driver version | |
| #define | LPC_IOPCTL_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| IOPCTL driver version 2.0.0. More... | |
| struct iopctl_group_t |
| #define LPC_IOPCTL_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| #define IOPCTL_FUNC0 0x0 |
| __STATIC_INLINE void IOPCTL_PinMuxSet | ( | IOPCTL_Type * | base, |
| uint8_t | port, | ||
| uint8_t | pin, | ||
| uint32_t | modefunc | ||
| ) |
| base | : The base of IOPCTL peripheral on the chip |
| port | : Port to mux |
| pin | : Pin to mux |
| modefunc | : OR'ed values of type IOPCTL_* |
| __STATIC_INLINE void IOPCTL_SetPinMuxing | ( | IOPCTL_Type * | base, |
| const iopctl_group_t * | pinArray, | ||
| uint32_t | arrayLength | ||
| ) |
| base | : The base of IOPCTL peripheral on the chip |
| pinArray | : Pointer to array of pin mux selections |
| arrayLength | : Number of entries in pinArray |