![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the In Application Programming (IAP).
It provides a set of functions to call the on-chip in application programming interface. User code executing from on-chip RAM can call these function to read information like part id, read and write flash, read and write ffr.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/iap
Modules | |
| IAP Boot Driver | |
| IAP FlexSPI Driver | |
| IAP OTP Driver | |
Files | |
| file | fsl_iap.h |
Driver version | |
| #define | FSL_IAP_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |
| IAP driver version 2.1.0. More... | |
| #define FSL_IAP_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) |