![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Modules | |
Nand Flash Component | |
Nor Flash Component | |
Data Structures | |
struct | flash_config_t |
Flash config structure. More... | |
struct | flash_transfer_t |
Flash transfer structure. More... | |
struct | flash_handle_t |
Flash handle. More... | |
Enumerations | |
enum | flash_err_t { flash_ok, flash_too_big, flash_not_aligned, flash_busy, flash_error } |
Flash error code structure. More... | |
enum | flash_op_code_t { kNorFlash_WriteEnable = 0x0, kNorFlash_Write = 0x1, kNorFlash_Read = 0x2, kNorFlash_ReadStatus = 0x3, kNorFlash_EraseSector = 0x4, kNorFlash_EraseChip = 0x5 } |
Flash operation code structure. More... | |
struct flash_config_t |
Data Fields | |
uint32_t | totalSize |
Total flash size. More... | |
uint32_t | pageSize |
Page size. More... | |
uint32_t | sectorSize |
Sector size. More... | |
bool | needWriteEnable |
Need do write enable before write/erase operation. More... | |
uint8_t | statusValueSize |
Status value size in bytes. More... | |
uint32_t | statusBusyMask |
Status busy mask. More... | |
uint8_t | statusBusyValue |
Status busy value. More... | |
uint32_t flash_config_t::totalSize |
uint32_t flash_config_t::pageSize |
uint32_t flash_config_t::sectorSize |
bool flash_config_t::needWriteEnable |
uint8_t flash_config_t::statusValueSize |
uint32_t flash_config_t::statusBusyMask |
uint8_t flash_config_t::statusBusyValue |
struct flash_transfer_t |
Data Fields | |
flash_op_code_t | opCode |
Operation code. More... | |
uint8_t | address |
Program/write address. More... | |
uint8_t * | data |
Data buffer pointer for program buffer or store buffer. More... | |
uint32_t | dataSize |
Data buffer size. More... | |
flash_op_code_t flash_transfer_t::opCode |
uint8_t flash_transfer_t::address |
uint8_t* flash_transfer_t::data |
uint32_t flash_transfer_t::dataSize |
struct flash_handle_t |
Data Fields | |
flash_err_t(* | executeCommand )(void *resource, flash_transfer_t *xfer) |
Execute command function. More... | |
void * | resource |
Pointer for resource, resource mean the SPI adapter resource. More... | |
uint32_t | totalSize |
Flash total size. More... | |
uint32_t | pageSize |
Flash page size. More... | |
uint32_t | sectorSize |
Flash sector size. More... | |
bool | needWriteEnable |
Need do write enable before write/erase operation. More... | |
uint8_t | statusValueSize |
Status value size in bytes. More... | |
uint32_t | statusBusyMask |
Status busy mask. More... | |
uint8_t | statusBusyValue |
Status busy value. More... | |
flash_err_t(* flash_handle_t::executeCommand)(void *resource, flash_transfer_t *xfer) |
void* flash_handle_t::resource |
uint32_t flash_handle_t::totalSize |
uint32_t flash_handle_t::pageSize |
uint32_t flash_handle_t::sectorSize |
bool flash_handle_t::needWriteEnable |
uint8_t flash_handle_t::statusValueSize |
uint32_t flash_handle_t::statusBusyMask |
uint8_t flash_handle_t::statusBusyValue |
enum flash_err_t |
enum flash_op_code_t |