![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Modules | |
| Flexspi Nand Flash | |
| Semc Nand Flash | |
Data Structures | |
| struct | nand_config_t |
| NAND Flash Config block structure. More... | |
| struct | nand_handle_t |
| NAND Flash handle info. More... | |
NAND FLASH Driver | |
| status_t | Nand_Flash_Init (nand_config_t *config, nand_handle_t *handle) |
| Initialize NAND FLASH devices. More... | |
| status_t | Nand_Flash_Read_Page (nand_handle_t *handle, uint32_t pageIndex, uint8_t *buffer, uint32_t length) |
| Read page data from NAND Flash. More... | |
| status_t | Nand_Flash_Read_Page_Partial (nand_handle_t *handle, uint32_t pageIndex, uint32_t offset_bytes, uint8_t *buffer, uint32_t length) |
| Read page partial data from NAND Flash. More... | |
| status_t | Nand_Flash_Page_Program (nand_handle_t *handle, uint32_t pageIndex, uint8_t *src, uint32_t length) |
| Program page data to NAND Flash. More... | |
| status_t | Nand_Flash_Erase_Block (nand_handle_t *handle, uint32_t blockIndex) |
| Erase block NAND Flash. More... | |
| struct nand_config_t |
Data Fields | |
| void * | memControlConfig |
| memory controller configuration, should be assigned to specific controller configuration structure pointer. More... | |
| void* nand_config_t::memControlConfig |
| struct nand_handle_t |
Data Fields | |
| uint8_t | vendorType |
| Driver Base address. More... | |
| uint32_t | bytesInPageDataArea |
| Bytes in page data area . More... | |
| uint32_t | bytesInPageSpareArea |
| Bytes in page spare area . More... | |
| uint32_t | pagesInBlock |
| Pages in each block. More... | |
| uint32_t | blocksInPlane |
| blocks in each plane. More... | |
| uint32_t | planesInDevice |
| planes in each device . More... | |
| void * | deviceSpecific |
| Device specific control parameter. | |
| uint8_t nand_handle_t::vendorType |
vendor type
| uint32_t nand_handle_t::bytesInPageDataArea |
| uint32_t nand_handle_t::bytesInPageSpareArea |
| uint32_t nand_handle_t::pagesInBlock |
| uint32_t nand_handle_t::blocksInPlane |
| uint32_t nand_handle_t::planesInDevice |
| status_t Nand_Flash_Init | ( | nand_config_t * | config, |
| nand_handle_t * | handle | ||
| ) |
This function initialize NAND Flash controller and NAND Flash.
| config | Nand flash configuration. The "memControlConfig" and "driverBaseAddr" are controller specific structure. please set those two parameter with your Nand controller configuration structure type pointer. such as for SEMC: |
semc_mem_nand_config_t semcNandconfig = { ..... } nand_config_t config = { .memControlConfig = (void *)&semcNandconfig; .driverBaseAddr = (void *)SEMC; }
| handle | The NAND Flash handler. |
| execution | status |
| status_t Nand_Flash_Read_Page | ( | nand_handle_t * | handle, |
| uint32_t | pageIndex, | ||
| uint8_t * | buffer, | ||
| uint32_t | length | ||
| ) |
| handle | The NAND Flash handler. |
| pageIndex | Nand flash page index, range from 0 ~ xxx. |
| buffer | Nand flash buffer to read data to. |
| length | Nand flash read length. |
| execution | status |
| status_t Nand_Flash_Read_Page_Partial | ( | nand_handle_t * | handle, |
| uint32_t | pageIndex, | ||
| uint32_t | offset_bytes, | ||
| uint8_t * | buffer, | ||
| uint32_t | length | ||
| ) |
| handle | The NAND Flash handler. |
| pageIndex | Nand flash page index, range from 0 ~ xxx. |
| offset_bytes | Offset to start read the page data. |
| buffer | Nand flash buffer to read data to. |
| length | Nand flash read length. |
| execution | status |
| status_t Nand_Flash_Page_Program | ( | nand_handle_t * | handle, |
| uint32_t | pageIndex, | ||
| uint8_t * | src, | ||
| uint32_t | length | ||
| ) |
| handle | The NAND Flash handler. |
| pageIndex | Nand flash page index, range from 0 ~ xxx. |
| src | The data to be programed to the page. |
| length | Nand flash read length. |
| execution | status |
| status_t Nand_Flash_Erase_Block | ( | nand_handle_t * | handle, |
| uint32_t | blockIndex | ||
| ) |
| handle | The NAND Flash handler. |
| blockIndex | Nand flash block index to be erased, range from 0 ~ xxx. |
| execution | status |