MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Enet_qos_qos

Overview

Data Structures

struct  enet_qos_rx_bd_struct_t
 Defines the receive descriptor structure has the read-format and write-back format structure. More...
 
struct  enet_qos_tx_bd_struct_t
 Defines the transmit descriptor structure has the read-format and write-back format structure. More...
 
struct  enet_qos_ptp_time_t
 Defines the ENET PTP time stamp structure. More...
 
struct  enet_qos_frame_info_t
 Defines the frame info structure. More...
 
struct  enet_qos_tx_dirty_ring_t
 Defines the ENET transmit dirty addresses ring/queue structure. More...
 
struct  enet_qos_ptp_config_t
 Defines the ENET PTP configuration structure. More...
 
struct  enet_qos_est_gate_op_t
 Defines the EST gate operation structure. More...
 
struct  enet_qos_est_gcl_t
 Defines the EST gate control list structure. More...
 
struct  enet_qos_rxp_config_t
 Defines the ENET_QOS Rx parser configuration structure. More...
 
struct  enet_qos_buffer_config_t
 Defines the buffer descriptor configure structure. More...
 
struct  enet_qos_cbs_config_t
 Defines the CBS configuration for queue. More...
 
struct  enet_qos_queue_tx_config_t
 Defines the queue configuration structure. More...
 
struct  enet_qos_queue_rx_config_t
 Defines the queue configuration structure. More...
 
struct  enet_qos_multiqueue_config_t
 Defines the configuration when multi-queue is used. More...
 
struct  enet_qos_config_t
 Defines the basic configuration structure for the ENET device. More...
 
struct  enet_qos_tx_bd_ring_t
 Defines the ENET transmit buffer descriptor ring/queue structure. More...
 
struct  enet_qos_rx_bd_ring_t
 Defines the ENET receive buffer descriptor ring/queue structure. More...
 
struct  enet_qos_handle_t
 Defines the ENET handler structure. More...
 

Typedefs

typedef void(* enet_qos_callback_t )(ENET_QOS_Type *base, enet_qos_handle_t *handle, enet_qos_event_t event, uint8_t channel, void *userData)
 ENET callback function. More...
 

Enumerations

enum  {
  kStatus_ENET_QOS_RxFrameError,
  kStatus_ENET_QOS_RxFrameFail = MAKE_STATUS(kStatusGroup_ENET_QOS, 1U),
  kStatus_ENET_QOS_RxFrameEmpty = MAKE_STATUS(kStatusGroup_ENET_QOS, 2U),
  kStatus_ENET_QOS_TxFrameBusy,
  kStatus_ENET_QOS_TxFrameFail = MAKE_STATUS(kStatusGroup_ENET_QOS, 4U),
  kStatus_ENET_QOS_TxFrameOverLen = MAKE_STATUS(kStatusGroup_ENET_QOS, 5U),
  kStatus_ENET_QOS_Est_SwListBusy,
  kStatus_ENET_QOS_Est_SwListWriteAbort = MAKE_STATUS(kStatusGroup_ENET_QOS, 7U),
  kStatus_ENET_QOS_Est_InvalidParameter,
  kStatus_ENET_QOS_Est_BtrError = MAKE_STATUS(kStatusGroup_ENET_QOS, 9U),
  kStatus_ENET_QOS_TrgtBusy = MAKE_STATUS(kStatusGroup_ENET_QOS, 10U),
  kStatus_ENET_QOS_Timeout = MAKE_STATUS(kStatusGroup_ENET_QOS, 11U),
  kStatus_ENET_QOS_PpsBusy = MAKE_STATUS(kStatusGroup_ENET_QOS, 12U)
}
 Defines the status return codes for transaction. More...
 
enum  enet_qos_mii_mode_t {
  kENET_QOS_MiiMode = 0U,
  kENET_QOS_RgmiiMode = 1U,
  kENET_QOS_RmiiMode = 4U
}
 Defines the MII/RGMII mode for data interface between the MAC and the PHY. More...
 
enum  enet_qos_mii_speed_t {
  kENET_QOS_MiiSpeed10M,
  kENET_QOS_MiiSpeed100M,
  kENET_QOS_MiiSpeed1000M,
  kENET_QOS_MiiSpeed2500M
}
 Defines the 10/100/1000 Mbps speed for the MII data interface. More...
 
enum  enet_qos_mii_duplex_t {
  kENET_QOS_MiiHalfDuplex = 0U,
  kENET_QOS_MiiFullDuplex
}
 Defines the half or full duplex for the MII data interface. More...
 
enum  enet_qos_mii_normal_opcode {
  kENET_QOS_MiiWriteFrame,
  kENET_QOS_MiiReadFrame
}
 Define the MII opcode for normal MDIO_CLAUSES_22 Frame. More...
 
enum  enet_qos_dma_burstlen {
  kENET_QOS_BurstLen1 = 0x00001U,
  kENET_QOS_BurstLen2 = 0x00002U,
  kENET_QOS_BurstLen4 = 0x00004U,
  kENET_QOS_BurstLen8 = 0x00008U,
  kENET_QOS_BurstLen16 = 0x00010U,
  kENET_QOS_BurstLen32 = 0x00020U,
  kENET_QOS_BurstLen64 = 0x10008U,
  kENET_QOS_BurstLen128 = 0x10010U,
  kENET_QOS_BurstLen256 = 0x10020U
}
 Define the DMA maximum transmit burst length. More...
 
enum  enet_qos_desc_flag {
  kENET_QOS_MiddleFlag = 0,
  kENET_QOS_LastFlagOnly,
  kENET_QOS_FirstFlagOnly,
  kENET_QOS_FirstLastFlag
}
 Define the flag for the descriptor. More...
 
enum  enet_qos_systime_op {
  kENET_QOS_SystimeAdd = 0U,
  kENET_QOS_SystimeSubtract = 1U
}
 Define the system time adjust operation control. More...
 
enum  enet_qos_ts_rollover_type {
  kENET_QOS_BinaryRollover = 0,
  kENET_QOS_DigitalRollover = 1
}
 Define the system time rollover control. More...
 
enum  enet_qos_special_config_t {
  kENET_QOS_DescDoubleBuffer = 0x0001U,
  kENET_QOS_StoreAndForward = 0x0002U,
  kENET_QOS_PromiscuousEnable = 0x0004U,
  kENET_QOS_FlowControlEnable = 0x0008U,
  kENET_QOS_BroadCastRxDisable = 0x0010U,
  kENET_QOS_MulticastAllEnable = 0x0020U,
  kENET_QOS_8023AS2KPacket = 0x0040U,
  kENET_QOS_HashMulticastEnable = 0x0080U
}
 Defines some special configuration for ENET. More...
 
enum  enet_qos_dma_interrupt_enable_t {
  kENET_QOS_DmaTx = ENET_QOS_DMA_CHX_INT_EN_TIE_MASK,
  kENET_QOS_DmaTxStop = ENET_QOS_DMA_CHX_INT_EN_TXSE_MASK,
  kENET_QOS_DmaTxBuffUnavail = ENET_QOS_DMA_CHX_INT_EN_TBUE_MASK,
  kENET_QOS_DmaRx = ENET_QOS_DMA_CHX_INT_EN_RIE_MASK,
  kENET_QOS_DmaRxBuffUnavail = ENET_QOS_DMA_CHX_INT_EN_RBUE_MASK,
  kENET_QOS_DmaRxStop = ENET_QOS_DMA_CHX_INT_EN_RSE_MASK,
  kENET_QOS_DmaRxWatchdogTimeout = ENET_QOS_DMA_CHX_INT_EN_RWTE_MASK,
  kENET_QOS_DmaEarlyTx = ENET_QOS_DMA_CHX_INT_EN_ETIE_MASK,
  kENET_QOS_DmaEarlyRx = ENET_QOS_DMA_CHX_INT_EN_ERIE_MASK,
  kENET_QOS_DmaBusErr = ENET_QOS_DMA_CHX_INT_EN_FBEE_MASK
}
 List of DMA interrupts supported by the ENET interrupt. More...
 
enum  enet_qos_mac_interrupt_enable_t
 List of mac interrupts supported by the ENET interrupt. More...
 
enum  enet_qos_event_t {
  kENET_QOS_RxIntEvent,
  kENET_QOS_TxIntEvent,
  kENET_QOS_WakeUpIntEvent,
  kENET_QOS_TimeStampIntEvent
}
 Defines the common interrupt event for callback use. More...
 
enum  enet_qos_queue_mode_t {
  kENET_QOS_AVB_Mode = 1U,
  kENET_QOS_DCB_Mode = 2U
}
 Define the MTL mode for multiple queues/rings. More...
 
enum  enet_qos_mtl_multiqueue_txsche {
  kENET_QOS_txWeightRR = 0U,
  kENET_QOS_txWeightFQ = 1U,
  kENET_QOS_txDefictWeightRR = 2U,
  kENET_QOS_txStrPrio = 3U
}
 Define the MTL tx scheduling algorithm for multiple queues/rings. More...
 
enum  enet_qos_mtl_multiqueue_rxsche {
  kENET_QOS_rxStrPrio = 0U,
  kENET_QOS_rxWeightStrPrio
}
 Define the MTL rx scheduling algorithm for multiple queues/rings. More...
 
enum  enet_qos_mtl_rxqueuemap_t {
  kENET_QOS_StaticDirctMap = 0x100U,
  kENET_QOS_DynamicMap
}
 Define the MTL rx queue and DMA channel mapping. More...
 
enum  enet_qos_rx_queue_route_t
 Defines the package type for receive queue routing. More...
 
enum  enet_qos_ptp_event_type_t {
  kENET_QOS_PtpEventMsgType = 3U,
  kENET_QOS_PtpSrcPortIdLen = 10U,
  kENET_QOS_PtpEventPort = 319U,
  kENET_QOS_PtpGnrlPort = 320U
}
 Defines the ENET PTP message related constant. More...
 
enum  enet_qos_ptp_pps_instance_t {
  kENET_QOS_PtpPpsIstance0 = 0U,
  kENET_QOS_PtpPpsIstance1,
  kENET_QOS_PtpPpsIstance2,
  kENET_QOS_PtpPpsIstance3
}
 Defines the PPS instance numbers. More...
 
enum  enet_qos_ptp_pps_trgt_mode_t {
  kENET_QOS_PtpPpsTrgtModeOnlyInt = 0U,
  kENET_QOS_PtpPpsTrgtModeIntSt = 2,
  kENET_QOS_PtpPpsTrgtModeOnlySt = 3
}
 Defines the Target Time register mode. More...
 
enum  enet_qos_ptp_pps_cmd_t {
  kENET_QOS_PtpPpsCmdNC = 0U,
  kENET_QOS_PtpPpsCmdSSP = 1U,
  kENET_QOS_PtpPpsCmdSPT = 2U,
  kENET_QOS_PtpPpsCmdCS = 3U,
  kENET_QOS_PtpPpsCmdSPTAT = 4U,
  kENET_QOS_PtpPpsCmdSPTI = 5U,
  kENET_QOS_PtpPpsCmdCSPT = 6U
}
 Defines commands for ppscmd register. More...
 
enum  enet_qos_ets_list_length_t {
  kENET_QOS_Ets_List_64 = 7U,
  kENET_QOS_Ets_List_128 = 8U,
  kENET_QOS_Ets_List_256 = 9U,
  kENET_QOS_Ets_List_512 = 10U,
  kENET_QOS_Ets_List_1024 = 11U
}
 Defines the enmueration of ETS list length. More...
 
enum  enet_qos_ets_gccr_addr_t {
  kENET_QOS_Ets_btr_low = 0U,
  kENET_QOS_Ets_btr_high = 1U,
  kENET_QOS_Ets_ctr_low = 2U,
  kENET_QOS_Ets_ctr_high = 3U,
  kENET_QOS_Ets_ter = 4U,
  kENET_QOS_Ets_llr = 5U
}
 Defines the enmueration of ETS gate control address. More...
 
enum  enet_qos_rxp_dma_chn_t {
  kENET_QOS_Rxp_DMAChn0 = 1U,
  kENET_QOS_Rxp_DMAChn1 = 2U,
  kENET_QOS_Rxp_DMAChn2 = 4U,
  kENET_QOS_Rxp_DMAChn3 = 8U,
  kENET_QOS_Rxp_DMAChn4 = 16U
}
 Defines the enmueration of DMA channel used for rx parser entry. More...
 

Driver version

#define FSL_ENET_QOS_DRIVER_VERSION   (MAKE_VERSION(2, 2, 2))
 Defines the driver version. More...
 

Control and status region bit masks of the receive buffer descriptor.

#define ENET_QOS_RXDESCRIP_RD_BUFF1VALID_MASK   (1UL << 24U)
 Defines for read format. More...
 
#define ENET_QOS_RXDESCRIP_RD_BUFF2VALID_MASK   (1UL << 25U)
 Buffer2 address valid. More...
 
#define ENET_QOS_RXDESCRIP_RD_IOC_MASK   (1UL << 30U)
 Interrupt enable on complete. More...
 
#define ENET_QOS_RXDESCRIP_RD_OWN_MASK   (1UL << 31U)
 Own bit. More...
 
#define ENET_QOS_RXDESCRIP_WR_ERR_MASK   ((1UL << 3U) | (1UL << 7U))
 Defines for write back format. More...
 
#define ENET_QOS_RXDESCRIP_WR_PYLOAD_MASK   (0x7UL)
 
#define ENET_QOS_RXDESCRIP_WR_PTPMSGTYPE_MASK   (0xF00UL)
 
#define ENET_QOS_RXDESCRIP_WR_PTPTYPE_MASK   (1UL << 12U)
 
#define ENET_QOS_RXDESCRIP_WR_PTPVERSION_MASK   (1UL << 13U)
 
#define ENET_QOS_RXDESCRIP_WR_PTPTSA_MASK   (1UL << 14U)
 
#define ENET_QOS_RXDESCRIP_WR_PACKETLEN_MASK   (0x7FFFUL)
 
#define ENET_QOS_RXDESCRIP_WR_ERRSUM_MASK   (1UL << 15U)
 
#define ENET_QOS_RXDESCRIP_WR_TYPE_MASK   (0x30000UL)
 
#define ENET_QOS_RXDESCRIP_WR_DE_MASK   (1UL << 19U)
 
#define ENET_QOS_RXDESCRIP_WR_RE_MASK   (1UL << 20U)
 
#define ENET_QOS_RXDESCRIP_WR_OE_MASK   (1UL << 21U)
 
#define ENET_QOS_RXDESCRIP_WR_RS0V_MASK   (1UL << 25U)
 
#define ENET_QOS_RXDESCRIP_WR_RS1V_MASK   (1UL << 26U)
 
#define ENET_QOS_RXDESCRIP_WR_RS2V_MASK   (1UL << 27U)
 
#define ENET_QOS_RXDESCRIP_WR_LD_MASK   (1UL << 28U)
 
#define ENET_QOS_RXDESCRIP_WR_FD_MASK   (1UL << 29U)
 
#define ENET_QOS_RXDESCRIP_WR_CTXT_MASK   (1UL << 30U)
 
#define ENET_QOS_RXDESCRIP_WR_OWN_MASK   (1UL << 31U)
 

Control and status bit masks of the transmit buffer descriptor.

#define ENET_QOS_TXDESCRIP_RD_BL1_MASK   (0x3fffUL)
 Defines for read format. More...
 
#define ENET_QOS_TXDESCRIP_RD_BL2_MASK   (ENET_QOS_TXDESCRIP_RD_BL1_MASK << 16U)
 
#define ENET_QOS_TXDESCRIP_RD_BL1(n)   ((uint32_t)(n)&ENET_QOS_TXDESCRIP_RD_BL1_MASK)
 
#define ENET_QOS_TXDESCRIP_RD_BL2(n)   (((uint32_t)(n)&ENET_QOS_TXDESCRIP_RD_BL1_MASK) << 16)
 
#define ENET_QOS_TXDESCRIP_RD_TTSE_MASK   (1UL << 30UL)
 
#define ENET_QOS_TXDESCRIP_RD_IOC_MASK   (1UL << 31UL)
 
#define ENET_QOS_TXDESCRIP_RD_FL_MASK   (0x7FFFUL)
 
#define ENET_QOS_TXDESCRIP_RD_FL(n)   ((uint32_t)(n)&ENET_QOS_TXDESCRIP_RD_FL_MASK)
 
#define ENET_QOS_TXDESCRIP_RD_CIC(n)   (((uint32_t)(n)&0x3U) << 16U)
 
#define ENET_QOS_TXDESCRIP_RD_TSE_MASK   (1UL << 18U)
 
#define ENET_QOS_TXDESCRIP_RD_SLOT(n)   (((uint32_t)(n)&0x0fU) << 19U)
 
#define ENET_QOS_TXDESCRIP_RD_SAIC(n)   (((uint32_t)(n)&0x07U) << 23U)
 
#define ENET_QOS_TXDESCRIP_RD_CPC(n)   (((uint32_t)(n)&0x03U) << 26U)
 
#define ENET_QOS_TXDESCRIP_RD_LDFD(n)   (((uint32_t)(n)&0x03U) << 28U)
 
#define ENET_QOS_TXDESCRIP_RD_LD_MASK   (1UL << 28U)
 
#define ENET_QOS_TXDESCRIP_RD_FD_MASK   (1UL << 29U)
 
#define ENET_QOS_TXDESCRIP_RD_CTXT_MASK   (1UL << 30U)
 
#define ENET_QOS_TXDESCRIP_RD_OWN_MASK   (1UL << 31U)
 
#define ENET_QOS_TXDESCRIP_WB_TTSS_MASK   (1UL << 17U)
 Defines for write back format. More...
 

Bit mask for interrupt enable type.

#define ENET_QOS_ABNORM_INT_MASK
 
#define ENET_QOS_NORM_INT_MASK
 

Defines some Ethernet parameters.

#define ENET_QOS_RING_NUM_MAX   (5U)
 The Maximum number of tx/rx descriptor rings. More...
 
#define ENET_QOS_FRAME_MAX_FRAMELEN   (1518U)
 Default maximum Ethernet frame size. More...
 
#define ENET_QOS_FCS_LEN   (4U)
 Ethernet FCS length. More...
 
#define ENET_QOS_ADDR_ALIGNMENT   (0x3U)
 Recommended Ethernet buffer alignment. More...
 
#define ENET_QOS_BUFF_ALIGNMENT   (8U)
 Receive buffer alignment shall be 4bytes-aligned. More...
 
#define ENET_QOS_MTL_RXFIFOSIZE   (8192U)
 The rx fifo size. More...
 
#define ENET_QOS_MTL_TXFIFOSIZE   (8192U)
 The tx fifo size. More...
 
#define ENET_QOS_MACINT_ENUM_OFFSET   (16U)
 The offest for mac interrupt in enum type. More...
 
#define ENET_QOS_RXP_ENTRY_COUNT   (256U)
 RXP table entry count, implied by FRPES in MAC_HW_FEATURE3.
 
#define ENET_QOS_RXP_BUFFER_SIZE   (256U)
 RXP Buffer size, implied by FRPBS in MAC_HW_FEATURE3.
 
#define ENET_QOS_EST_WID   (24U)
 Width of the time interval in Gate Control List.
 
#define ENET_QOS_EST_DEP   (512U)
 Maxmimum depth of Gate Control List.
 

Initialization and De-initialization

void ENET_QOS_GetDefaultConfig (enet_qos_config_t *config)
 Gets the ENET default configuration structure. More...
 
status_t ENET_QOS_Up (ENET_QOS_Type *base, const enet_qos_config_t *config, uint8_t *macAddr, uint8_t macCount, uint32_t refclkSrc_Hz)
 Initializes the ENET module. More...
 
status_t ENET_QOS_Init (ENET_QOS_Type *base, const enet_qos_config_t *config, uint8_t *macAddr, uint8_t macCount, uint32_t refclkSrc_Hz)
 Initializes the ENET module. More...
 
void ENET_QOS_Down (ENET_QOS_Type *base)
 brief Stops the ENET module. More...
 
void ENET_QOS_Deinit (ENET_QOS_Type *base)
 Deinitializes the ENET module. More...
 
uint32_t ENET_QOS_GetInstance (ENET_QOS_Type *base)
 Get the ENET instance from peripheral base address. More...
 
status_t ENET_QOS_DescriptorInit (ENET_QOS_Type *base, enet_qos_config_t *config, enet_qos_buffer_config_t *bufferConfig)
 Initialize for all ENET descriptors. More...
 
void ENET_QOS_StartRxTx (ENET_QOS_Type *base, uint8_t txRingNum, uint8_t rxRingNum)
 Starts the ENET rx/tx. More...
 

MII interface operation

static void ENET_QOS_SetMII (ENET_QOS_Type *base, enet_qos_mii_speed_t speed, enet_qos_mii_duplex_t duplex)
 Sets the ENET MII speed and duplex. More...
 
void ENET_QOS_SetSMI (ENET_QOS_Type *base, uint32_t csrClock_Hz)
 Sets the ENET SMI(serial management interface)- MII management interface. More...
 
static bool ENET_QOS_IsSMIBusy (ENET_QOS_Type *base)
 Checks if the SMI is busy. More...
 
static uint16_t ENET_QOS_ReadSMIData (ENET_QOS_Type *base)
 Reads data from the PHY register through SMI interface. More...
 
void ENET_QOS_StartSMIRead (ENET_QOS_Type *base, uint32_t phyAddr, uint32_t phyReg)
 Starts an SMI read command. More...
 
void ENET_QOS_StartSMIWrite (ENET_QOS_Type *base, uint32_t phyAddr, uint32_t phyReg, uint32_t data)
 Starts a SMI write command. More...
 

Other basic operation

static void ENET_QOS_SetMacAddr (ENET_QOS_Type *base, uint8_t *macAddr, uint8_t index)
 Sets the ENET module Mac address. More...
 
void ENET_QOS_GetMacAddr (ENET_QOS_Type *base, uint8_t *macAddr, uint8_t index)
 Gets the ENET module Mac address. More...
 
void ENET_QOS_AddMulticastGroup (ENET_QOS_Type *base, uint8_t *address)
 Adds the ENET_QOS device to a multicast group. More...
 
void ENET_QOS_LeaveMulticastGroup (ENET_QOS_Type *base, uint8_t *address)
 brief Moves the ENET_QOS device from a multicast group. More...
 
static void ENET_QOS_AcceptAllMulticast (ENET_QOS_Type *base)
 Enable ENET device to accept all multicast frames. More...
 
static void ENET_QOS_RejectAllMulticast (ENET_QOS_Type *base)
 ENET device reject to accept all multicast frames. More...
 
void ENET_QOS_EnterPowerDown (ENET_QOS_Type *base, uint32_t *wakeFilter)
 Set the MAC to enter into power down mode. More...
 
static void ENET_QOS_ExitPowerDown (ENET_QOS_Type *base)
 Set the MAC to exit power down mode. More...
 
status_t ENET_QOS_EnableRxParser (ENET_QOS_Type *base, bool enable)
 Enable/Disable Rx parser,please notice that for enable/disable Rx Parser, should better disable Receive first. More...
 

Interrupts.

void ENET_QOS_EnableInterrupts (ENET_QOS_Type *base, uint32_t mask)
 Enables the ENET DMA and MAC interrupts. More...
 
void ENET_QOS_DisableInterrupts (ENET_QOS_Type *base, uint32_t mask)
 Disables the ENET DMA and MAC interrupts. More...
 
static uint32_t ENET_QOS_GetDmaInterruptStatus (ENET_QOS_Type *base, uint8_t channel)
 Gets the ENET DMA interrupt status flag. More...
 
static void ENET_QOS_ClearDmaInterruptStatus (ENET_QOS_Type *base, uint8_t channel, uint32_t mask)
 Clear the ENET DMA interrupt status flag. More...
 
static uint32_t ENET_QOS_GetMacInterruptStatus (ENET_QOS_Type *base)
 Gets the ENET MAC interrupt status flag. More...
 
void ENET_QOS_ClearMacInterruptStatus (ENET_QOS_Type *base, uint32_t mask)
 Clears the ENET mac interrupt events status flag. More...
 

Functional operation.

static bool ENET_QOS_IsTxDescriptorDmaOwn (enet_qos_tx_bd_struct_t *txDesc)
 Get the tx descriptor DMA Own flag. More...
 
void ENET_QOS_SetupTxDescriptor (enet_qos_tx_bd_struct_t *txDesc, void *buffer1, uint32_t bytes1, void *buffer2, uint32_t bytes2, uint32_t framelen, bool intEnable, bool tsEnable, enet_qos_desc_flag flag, uint8_t slotNum)
 Setup a given tx descriptor. More...
 
static void ENET_QOS_UpdateTxDescriptorTail (ENET_QOS_Type *base, uint8_t channel, uint32_t txDescTailAddrAlign)
 Update the tx descriptor tail pointer. More...
 
static void ENET_QOS_UpdateRxDescriptorTail (ENET_QOS_Type *base, uint8_t channel, uint32_t rxDescTailAddrAlign)
 Update the rx descriptor tail pointer. More...
 
static uint32_t ENET_QOS_GetRxDescriptor (enet_qos_rx_bd_struct_t *rxDesc)
 Gets the context in the ENET rx descriptor. More...
 
void ENET_QOS_UpdateRxDescriptor (enet_qos_rx_bd_struct_t *rxDesc, void *buffer1, void *buffer2, bool intEnable, bool doubleBuffEnable)
 Updates the buffers and the own status for a given rx descriptor. More...
 
status_t ENET_QOS_ConfigureRxParser (ENET_QOS_Type *base, enet_qos_rxp_config_t *rxpConfig, uint16_t entryCount)
 Configure flexible rx parser. More...
 
status_t ENET_QOS_ReadRxParser (ENET_QOS_Type *base, enet_qos_rxp_config_t *rxpConfig, uint16_t entryIndex)
 Read flexible rx parser configuration at specified index. More...
 
status_t ENET_QOS_EstProgramGcl (ENET_QOS_Type *base, enet_qos_est_gcl_t *gcl, uint32_t ptpClk_Hz)
 Program Gate Control List. More...
 
status_t ENET_QOS_EstReadGcl (ENET_QOS_Type *base, enet_qos_est_gcl_t *gcl, uint32_t listLen, bool hwList)
 Read Gate Control List. More...
 
static void ENET_QOS_FpeEnable (ENET_QOS_Type *base)
 Enable Frame Preemption. More...
 
static void ENET_QOS_FpeDisable (ENET_QOS_Type *base)
 Disable Frame Preemption. More...
 
static void ENET_QOS_FpeConfigPreemptable (ENET_QOS_Type *base, uint8_t queueMask)
 Configure preemptable transmit queues. More...
 
void ENET_QOS_AVBConfigure (ENET_QOS_Type *base, const enet_qos_cbs_config_t *config, uint8_t queueIndex)
 Sets the ENET AVB feature. More...
 

Transactional operation

void ENET_QOS_CreateHandler (ENET_QOS_Type *base, enet_qos_handle_t *handle, enet_qos_config_t *config, enet_qos_buffer_config_t *bufferConfig, enet_qos_callback_t callback, void *userData)
 Create ENET Handler. More...
 
status_t ENET_QOS_GetRxFrameSize (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint32_t *length, uint8_t channel)
 Gets the size of the read frame. More...
 
status_t ENET_QOS_ReadFrame (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint8_t *data, uint32_t length, uint8_t channel, enet_qos_ptp_time_t *ts)
 Reads a frame from the ENET device. More...
 
status_t ENET_QOS_SendFrame (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint8_t *data, uint32_t length, uint8_t channel, bool isNeedTs, void *context)
 Transmits an ENET frame. More...
 
void ENET_QOS_ReclaimTxDescriptor (ENET_QOS_Type *base, enet_qos_handle_t *handle, uint8_t channel)
 Reclaim tx descriptors. More...
 
void ENET_QOS_CommonIRQHandler (ENET_QOS_Type *base, enet_qos_handle_t *handle)
 The ENET IRQ handler. More...
 
void ENET_QOS_SetISRHandler (ENET_QOS_Type *base, enet_qos_isr_t ISRHandler)
 Set the second level IRQ handler, allow user to overwrite the default second level weak IRQ handler. More...
 

ENET Enhanced function operation

status_t ENET_QOS_Ptp1588CorrectTimerInCoarse (ENET_QOS_Type *base, enet_qos_systime_op operation, uint32_t second, uint32_t nanosecond)
 Correct the ENET PTP 1588 timer in coarse method. More...
 
status_t ENET_QOS_Ptp1588CorrectTimerInFine (ENET_QOS_Type *base, uint32_t addend)
 Correct the ENET PTP 1588 timer in fine method. More...
 
static uint32_t ENET_QOS_Ptp1588GetAddend (ENET_QOS_Type *base)
 Get the ENET Time stamp current addend value. More...
 
void ENET_QOS_Ptp1588GetTimerNoIRQDisable (ENET_QOS_Type *base, uint64_t *second, uint32_t *nanosecond)
 Gets the current ENET time from the PTP 1588 timer without IRQ disable. More...
 
static status_t ENET_Ptp1588PpsControl (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, enet_qos_ptp_pps_trgt_mode_t trgtMode, enet_qos_ptp_pps_cmd_t cmd)
 Sets the ENET PTP 1588 PPS control. More...
 
status_t ENET_QOS_Ptp1588PpsSetTrgtTime (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, uint32_t seconds, uint32_t nanoseconds)
 Sets the ENET OQS PTP 1588 PPS target time registers. More...
 
static void ENET_QOS_Ptp1588PpsSetWidth (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, uint32_t width)
 Sets the ENET OQS PTP 1588 PPS output signal interval. More...
 
static void ENET_QOS_Ptp1588PpsSetInterval (ENET_QOS_Type *base, enet_qos_ptp_pps_instance_t instance, uint32_t interval)
 Sets the ENET OQS PTP 1588 PPS output signal width. More...
 
void ENET_QOS_Ptp1588GetTimer (ENET_QOS_Type *base, uint64_t *second, uint32_t *nanosecond)
 Gets the current ENET time from the PTP 1588 timer. More...
 
void ENET_QOS_GetTxFrame (enet_qos_handle_t *handle, enet_qos_frame_info_t *txFrame, uint8_t channel)
 Gets the time stamp of the transmit frame. More...
 

Data Structure Documentation

struct enet_qos_rx_bd_struct_t

They both has the same size with different region definition. so we define the read-format region as the recive descriptor structure Use the read-format region mask bits in the descriptor initialization Use the write-back format region mask bits in the receive data process.

Data Fields

__IO uint32_t buff1Addr
 Buffer 1 address.
 
__IO uint32_t reserved
 Reserved.
 
__IO uint32_t buff2Addr
 Buffer 2 or next descriptor address.
 
__IO uint32_t control
 Buffer 1/2 byte counts and control.
 
struct enet_qos_tx_bd_struct_t

They both has the same size with different region definition. so we define the read-format region as the transmit descriptor structure Use the read-format region mask bits in the descriptor initialization Use the write-back format region mask bits in the transmit data process.

Data Fields

__IO uint32_t buff1Addr
 Buffer 1 address.
 
__IO uint32_t buff2Addr
 Buffer 2 address.
 
__IO uint32_t buffLen
 Buffer 1/2 byte counts.
 
__IO uint32_t controlStat
 TDES control and status word.
 
struct enet_qos_ptp_time_t

Data Fields

uint64_t second
 Second. More...
 
uint32_t nanosecond
 Nanosecond. More...
 

Field Documentation

uint64_t enet_qos_ptp_time_t::second
uint32_t enet_qos_ptp_time_t::nanosecond
struct enet_qos_frame_info_t

Data Fields

void * context
 User specified data, could be buffer address for free.
 
bool isTsAvail
 Flag indicates timestamp available status.
 
enet_qos_ptp_time_t timeStamp
 Timestamp of frame.
 
struct enet_qos_tx_dirty_ring_t

Data Fields

enet_qos_frame_info_t * txDirtyBase
 Dirty buffer descriptor base address pointer. More...
 
uint16_t txGenIdx
 tx generate index. More...
 
uint16_t txConsumIdx
 tx consume index. More...
 
uint16_t txRingLen
 tx ring length. More...
 
bool isFull
 tx ring is full flag, add this parameter to avoid waste one element. More...
 

Field Documentation

enet_qos_frame_info_t* enet_qos_tx_dirty_ring_t::txDirtyBase
uint16_t enet_qos_tx_dirty_ring_t::txGenIdx
uint16_t enet_qos_tx_dirty_ring_t::txConsumIdx
uint16_t enet_qos_tx_dirty_ring_t::txRingLen
bool enet_qos_tx_dirty_ring_t::isFull
struct enet_qos_ptp_config_t

Data Fields

bool fineUpdateEnable
 Use the fine update. More...
 
uint32_t defaultAddend
 Default addend value when fine update is enable, could be 2^32 / (refClk_Hz / ENET_QOS_MICRSECS_ONESECOND / ENET_QOS_SYSTIME_REQUIRED_CLK_MHZ). More...
 
bool ptp1588V2Enable
 The desired system time frequency. More...
 
enet_qos_ts_rollover_type tsRollover
 1588 time nanosecond rollover. More...
 

Field Documentation

bool enet_qos_ptp_config_t::fineUpdateEnable
uint32_t enet_qos_ptp_config_t::defaultAddend
bool enet_qos_ptp_config_t::ptp1588V2Enable

Must be lower than reference clock. (Only used with fine correction method). ptp 1588 version 2 is used.

enet_qos_ts_rollover_type enet_qos_ptp_config_t::tsRollover
struct enet_qos_est_gate_op_t
struct enet_qos_est_gcl_t

Data Fields

bool enable
 Enable or disable EST.
 
uint64_t cycleTime
 Base Time 32 bits seconds 32 bits nanoseconds.
 
uint32_t extTime
 Cycle Time 32 bits seconds 32 bits nanoseconds.
 
uint32_t numEntries
 Time Extension 32 bits seconds 32 bits nanoseconds.
 
enet_qos_est_gate_op_t * opList
 Number of entries.
 
struct enet_qos_rxp_config_t

Data Fields

uint32_t matchEnable
 4-byte match data used for comparing with incoming packet
 
uint8_t acceptFrame: 1
 When matchEnable is set to 1, the matchData is used for comparing.
 
uint8_t rejectFrame: 1
 When acceptFrame = 1 and data is matched, the frame will be sent to DMA channel.
 
uint8_t inverseMatch: 1
 When rejectFrame = 1 and data is matched, the frame will be dropped.
 
uint8_t nextControl: 1
 Inverse match.
 
uint8_t reserved: 4
 Next instruction indexing control.
 
uint8_t frameOffset
 Reserved control fields.
 
uint8_t okIndex
 Frame offset in the packet data to be compared for match, in terms of 4 bytes. More...
 
uint8_t dmaChannel
 Memory Index to be used next. More...
 
uint32_t reserved2
 The DMA channel enet_qos_rxp_dma_chn_t used for receiving the frame when frame match and acceptFrame = 1.
 

Field Documentation

uint8_t enet_qos_rxp_config_t::okIndex
uint8_t enet_qos_rxp_config_t::dmaChannel
struct enet_qos_buffer_config_t

Notes:

  1. The receive and transmit descriptor start address pointer and tail pointer must be word-aligned.
  2. The recommended minimum tx/rx ring length is 4.
  3. The tx/rx descriptor tail address shall be the address pointer to the address just after the end of the last last descriptor. because only the descriptors between the start address and the tail address will be used by DMA.
  4. The descriptor address is the start address of all used contiguous memory. for example, the rxDescStartAddrAlign is the start address of rxRingLen contiguous descriptor memories for rx descriptor ring 0.
  5. The "*rxBufferstartAddr" is the first element of rxRingLen (2*rxRingLen for double buffers) rx buffers. It means the *rxBufferStartAddr is the rx buffer for the first descriptor the *rxBufferStartAddr + 1 is the rx buffer for the second descriptor or the rx buffer for the second buffer in the first descriptor. so please make sure the rxBufferStartAddr is the address of a rxRingLen or 2*rxRingLen array.

Data Fields

uint8_t rxRingLen
 The length of receive buffer descriptor ring. More...
 
uint8_t txRingLen
 The length of transmit buffer descriptor ring. More...
 
enet_qos_tx_bd_struct_t * txDescStartAddrAlign
 Aligned transmit descriptor start address. More...
 
enet_qos_tx_bd_struct_t * txDescTailAddrAlign
 Aligned transmit descriptor tail address. More...
 
enet_qos_frame_info_t * txDirtyStartAddr
 Start address of the dirty tx frame information. More...
 
enet_qos_rx_bd_struct_t * rxDescStartAddrAlign
 Aligned receive descriptor start address. More...
 
enet_qos_rx_bd_struct_t * rxDescTailAddrAlign
 Aligned receive descriptor tail address. More...
 
uint32_t * rxBufferStartAddr
 Start address of the rx buffers. More...
 
uint32_t rxBuffSizeAlign
 Aligned receive data buffer size. More...
 
bool rxBuffNeedMaintain
 Whether receive data buffer need cache maintain. More...
 

Field Documentation

uint8_t enet_qos_buffer_config_t::rxRingLen
uint8_t enet_qos_buffer_config_t::txRingLen
enet_qos_tx_bd_struct_t* enet_qos_buffer_config_t::txDescStartAddrAlign
enet_qos_tx_bd_struct_t* enet_qos_buffer_config_t::txDescTailAddrAlign
enet_qos_frame_info_t* enet_qos_buffer_config_t::txDirtyStartAddr
enet_qos_rx_bd_struct_t* enet_qos_buffer_config_t::rxDescStartAddrAlign
enet_qos_rx_bd_struct_t* enet_qos_buffer_config_t::rxDescTailAddrAlign
uint32_t* enet_qos_buffer_config_t::rxBufferStartAddr
uint32_t enet_qos_buffer_config_t::rxBuffSizeAlign
bool enet_qos_buffer_config_t::rxBuffNeedMaintain
struct enet_qos_cbs_config_t

Data Fields

uint16_t sendSlope
 Send slope configuration. More...
 
uint16_t idleSlope
 Idle slope configuration. More...
 
uint32_t highCredit
 High credit. More...
 
uint32_t lowCredit
 Low credit. More...
 

Field Documentation

uint16_t enet_qos_cbs_config_t::sendSlope
uint16_t enet_qos_cbs_config_t::idleSlope
uint32_t enet_qos_cbs_config_t::highCredit
uint32_t enet_qos_cbs_config_t::lowCredit
struct enet_qos_queue_tx_config_t

Data Fields

enet_qos_queue_mode_t mode
 tx queue mode configuration. More...
 
uint32_t weight
 Refer to the MTL TxQ Quantum Weight register. More...
 
uint32_t priority
 Refer to Transmit Queue Priority Mapping register. More...
 
enet_qos_cbs_config_t * cbsConfig
 CBS configuration if queue use AVB mode. More...
 

Field Documentation

enet_qos_queue_mode_t enet_qos_queue_tx_config_t::mode
uint32_t enet_qos_queue_tx_config_t::weight
uint32_t enet_qos_queue_tx_config_t::priority
enet_qos_cbs_config_t* enet_qos_queue_tx_config_t::cbsConfig
struct enet_qos_queue_rx_config_t

Data Fields

enet_qos_queue_mode_t mode
 rx queue mode configuration. More...
 
uint8_t mapChannel
 tx queue map dma channel. More...
 
uint32_t priority
 Rx queue priority. More...
 
enet_qos_rx_queue_route_t packetRoute
 Receive packet routing. More...
 

Field Documentation

enet_qos_queue_mode_t enet_qos_queue_rx_config_t::mode
uint8_t enet_qos_queue_rx_config_t::mapChannel
uint32_t enet_qos_queue_rx_config_t::priority
enet_qos_rx_queue_route_t enet_qos_queue_rx_config_t::packetRoute
struct enet_qos_multiqueue_config_t

Data Fields

enet_qos_dma_burstlen burstLen
 Burst len for the multi-queue. More...
 
uint8_t txQueueUse
 Used Tx queue count. More...
 
enet_qos_mtl_multiqueue_txsche mtltxSche
 Transmit schedule for multi-queue. More...
 
enet_qos_queue_tx_config_t txQueueConfig [ENET_QOS_RING_NUM_MAX]
 Tx Queue configuration. More...
 
uint8_t rxQueueUse
 Used Rx queue count. More...
 
enet_qos_mtl_multiqueue_rxsche mtlrxSche
 Receive schedule for multi-queue. More...
 
enet_qos_queue_rx_config_t rxQueueConfig [ENET_QOS_RING_NUM_MAX]
 Rx Queue configuration. More...
 

Field Documentation

enet_qos_dma_burstlen enet_qos_multiqueue_config_t::burstLen
uint8_t enet_qos_multiqueue_config_t::txQueueUse
enet_qos_mtl_multiqueue_txsche enet_qos_multiqueue_config_t::mtltxSche
enet_qos_queue_tx_config_t enet_qos_multiqueue_config_t::txQueueConfig[ENET_QOS_RING_NUM_MAX]
uint8_t enet_qos_multiqueue_config_t::rxQueueUse
enet_qos_mtl_multiqueue_rxsche enet_qos_multiqueue_config_t::mtlrxSche
enet_qos_queue_rx_config_t enet_qos_multiqueue_config_t::rxQueueConfig[ENET_QOS_RING_NUM_MAX]
struct enet_qos_config_t

Note:

  1. Default the signal queue is used so the "*multiqueueCfg" is set default with NULL. Set the pointer with a valid configuration pointer if the multiple queues are required. If multiple queue is enabled, please make sure the buffer configuration for all are prepared also.

Data Fields

uint16_t specialControl
 The logic or of enet_qos_special_config_t.
 
enet_qos_multiqueue_config_t * multiqueueCfg
 Use multi-queue. More...
 
enet_qos_mii_mode_t miiMode
 MII mode. More...
 
enet_qos_mii_speed_t miiSpeed
 MII Speed. More...
 
enet_qos_mii_duplex_t miiDuplex
 MII duplex. More...
 
uint16_t pauseDuration
 Used in the tx flow control frame, only valid when kENET_QOS_FlowControlEnable is set. More...
 
enet_qos_ptp_config_t * ptpConfig
 PTP 1588 feature configuration.
 
uint32_t csrClock_Hz
 CSR clock frequency in HZ. More...
 

Field Documentation

enet_qos_multiqueue_config_t* enet_qos_config_t::multiqueueCfg
enet_qos_mii_mode_t enet_qos_config_t::miiMode
enet_qos_mii_speed_t enet_qos_config_t::miiSpeed
enet_qos_mii_duplex_t enet_qos_config_t::miiDuplex
uint16_t enet_qos_config_t::pauseDuration
uint32_t enet_qos_config_t::csrClock_Hz
struct enet_qos_tx_bd_ring_t

Data Fields

enet_qos_tx_bd_struct_t * txBdBase
 Buffer descriptor base address pointer. More...
 
uint16_t txGenIdx
 tx generate index. More...
 
uint16_t txConsumIdx
 tx consume index. More...
 
volatile uint16_t txDescUsed
 tx descriptor used number. More...
 
uint16_t txRingLen
 tx ring length. More...
 

Field Documentation

enet_qos_tx_bd_struct_t* enet_qos_tx_bd_ring_t::txBdBase
uint16_t enet_qos_tx_bd_ring_t::txGenIdx
uint16_t enet_qos_tx_bd_ring_t::txConsumIdx
volatile uint16_t enet_qos_tx_bd_ring_t::txDescUsed
uint16_t enet_qos_tx_bd_ring_t::txRingLen
struct enet_qos_rx_bd_ring_t

Data Fields

enet_qos_rx_bd_struct_t * rxBdBase
 Buffer descriptor base address pointer. More...
 
uint16_t rxGenIdx
 The current available receive buffer descriptor pointer. More...
 
uint16_t rxRingLen
 Receive ring length. More...
 
uint32_t rxBuffSizeAlign
 Receive buffer size. More...
 

Field Documentation

enet_qos_rx_bd_struct_t* enet_qos_rx_bd_ring_t::rxBdBase
uint16_t enet_qos_rx_bd_ring_t::rxGenIdx
uint16_t enet_qos_rx_bd_ring_t::rxRingLen
uint32_t enet_qos_rx_bd_ring_t::rxBuffSizeAlign
struct _enet_qos_handle

Data Fields

uint8_t txQueueUse
 Used tx queue count. More...
 
uint8_t rxQueueUse
 Used rx queue count. More...
 
bool doubleBuffEnable
 The double buffer is used in the descriptor. More...
 
bool rxintEnable
 Rx interrupt enabled. More...
 
bool rxMaintainEnable [ENET_QOS_RING_NUM_MAX]
 Rx buffer cache maintain enabled. More...
 
enet_qos_rx_bd_ring_t rxBdRing [ENET_QOS_RING_NUM_MAX]
 Receive buffer descriptor. More...
 
enet_qos_tx_bd_ring_t txBdRing [ENET_QOS_RING_NUM_MAX]
 Transmit buffer descriptor. More...
 
enet_qos_tx_dirty_ring_t txDirtyRing [ENET_QOS_RING_NUM_MAX]
 Transmit dirty buffers addresses. More...
 
uint32_t * rxBufferStartAddr [ENET_QOS_RING_NUM_MAX]
 Rx buffer start address for reInitialize. More...
 
enet_qos_callback_t callback
 Callback function. More...
 
void * userData
 Callback function parameter. More...
 

Field Documentation

uint8_t enet_qos_handle_t::txQueueUse
uint8_t enet_qos_handle_t::rxQueueUse
bool enet_qos_handle_t::doubleBuffEnable
bool enet_qos_handle_t::rxintEnable
bool enet_qos_handle_t::rxMaintainEnable[ENET_QOS_RING_NUM_MAX]
enet_qos_rx_bd_ring_t enet_qos_handle_t::rxBdRing[ENET_QOS_RING_NUM_MAX]
enet_qos_tx_bd_ring_t enet_qos_handle_t::txBdRing[ENET_QOS_RING_NUM_MAX]
enet_qos_tx_dirty_ring_t enet_qos_handle_t::txDirtyRing[ENET_QOS_RING_NUM_MAX]
uint32_t* enet_qos_handle_t::rxBufferStartAddr[ENET_QOS_RING_NUM_MAX]
enet_qos_callback_t enet_qos_handle_t::callback
void* enet_qos_handle_t::userData

Macro Definition Documentation

#define FSL_ENET_QOS_DRIVER_VERSION   (MAKE_VERSION(2, 2, 2))
#define ENET_QOS_RXDESCRIP_RD_BUFF1VALID_MASK   (1UL << 24U)

Buffer1 address valid.

#define ENET_QOS_RXDESCRIP_RD_BUFF2VALID_MASK   (1UL << 25U)
#define ENET_QOS_RXDESCRIP_RD_IOC_MASK   (1UL << 30U)
#define ENET_QOS_RXDESCRIP_RD_OWN_MASK   (1UL << 31U)
#define ENET_QOS_RXDESCRIP_WR_ERR_MASK   ((1UL << 3U) | (1UL << 7U))
#define ENET_QOS_TXDESCRIP_RD_BL1_MASK   (0x3fffUL)
#define ENET_QOS_TXDESCRIP_WB_TTSS_MASK   (1UL << 17U)
#define ENET_QOS_RING_NUM_MAX   (5U)
#define ENET_QOS_FRAME_MAX_FRAMELEN   (1518U)
#define ENET_QOS_FCS_LEN   (4U)
#define ENET_QOS_ADDR_ALIGNMENT   (0x3U)
#define ENET_QOS_BUFF_ALIGNMENT   (8U)
#define ENET_QOS_MTL_RXFIFOSIZE   (8192U)
#define ENET_QOS_MTL_TXFIFOSIZE   (8192U)
#define ENET_QOS_MACINT_ENUM_OFFSET   (16U)

Typedef Documentation

typedef void(* enet_qos_callback_t)(ENET_QOS_Type *base, enet_qos_handle_t *handle, enet_qos_event_t event, uint8_t channel, void *userData)

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_ENET_QOS_RxFrameError 

A frame received but data error happen.

kStatus_ENET_QOS_RxFrameFail 

Failed to receive a frame.

kStatus_ENET_QOS_RxFrameEmpty 

No frame arrive.

kStatus_ENET_QOS_TxFrameBusy 

Transmit descriptors are under process.

kStatus_ENET_QOS_TxFrameFail 

Transmit frame fail.

kStatus_ENET_QOS_TxFrameOverLen 

Transmit oversize.

kStatus_ENET_QOS_Est_SwListBusy 

SW Gcl List not yet processed by HW.

kStatus_ENET_QOS_Est_SwListWriteAbort 

SW Gcl List write aborted .

kStatus_ENET_QOS_Est_InvalidParameter 

Invalid parameter in Gcl List .

kStatus_ENET_QOS_Est_BtrError 

Base Time Error when loading list.

kStatus_ENET_QOS_TrgtBusy 

Target time register busy.

kStatus_ENET_QOS_Timeout 

Target time register busy.

kStatus_ENET_QOS_PpsBusy 

Pps command busy.

Enumerator
kENET_QOS_MiiMode 

MII mode for data interface.

kENET_QOS_RgmiiMode 

RGMII mode for data interface.

kENET_QOS_RmiiMode 

RMII mode for data interface.

Enumerator
kENET_QOS_MiiSpeed10M 

Speed 10 Mbps.

kENET_QOS_MiiSpeed100M 

Speed 100 Mbps.

kENET_QOS_MiiSpeed1000M 

Speed 1000 Mbps.

kENET_QOS_MiiSpeed2500M 

Speed 2500 Mbps.

Enumerator
kENET_QOS_MiiHalfDuplex 

Half duplex mode.

kENET_QOS_MiiFullDuplex 

Full duplex mode.

Enumerator
kENET_QOS_MiiWriteFrame 

Write frame operation for a valid MII management frame.

kENET_QOS_MiiReadFrame 

Read frame operation for a valid MII management frame.

Enumerator
kENET_QOS_BurstLen1 

DMA burst length 1.

kENET_QOS_BurstLen2 

DMA burst length 2.

kENET_QOS_BurstLen4 

DMA burst length 4.

kENET_QOS_BurstLen8 

DMA burst length 8.

kENET_QOS_BurstLen16 

DMA burst length 16.

kENET_QOS_BurstLen32 

DMA burst length 32.

kENET_QOS_BurstLen64 

DMA burst length 64.

eight times enabled.

kENET_QOS_BurstLen128 

DMA burst length 128.

eight times enabled.

kENET_QOS_BurstLen256 

DMA burst length 256.

eight times enabled.

Enumerator
kENET_QOS_MiddleFlag 

It's a middle descriptor of the frame.

kENET_QOS_LastFlagOnly 

It's the last descriptor of the frame.

kENET_QOS_FirstFlagOnly 

It's the first descriptor of the frame.

kENET_QOS_FirstLastFlag 

It's the first and last descriptor of the frame.

Enumerator
kENET_QOS_SystimeAdd 

System time add to.

kENET_QOS_SystimeSubtract 

System time subtract.

Enumerator
kENET_QOS_BinaryRollover 

System time binary rollover.

kENET_QOS_DigitalRollover 

System time digital rollover.

These control flags are provided for special user requirements. Normally, these is no need to set this control flags for ENET initialization. But if you have some special requirements, set the flags to specialControl in the enet_qos_config_t.

Note
"kENET_QOS_StoreAndForward" is recommended to be set.
Enumerator
kENET_QOS_DescDoubleBuffer 

The double buffer is used in the tx/rx descriptor.

kENET_QOS_StoreAndForward 

The rx/tx store and forward enable.

kENET_QOS_PromiscuousEnable 

The promiscuous enabled.

kENET_QOS_FlowControlEnable 

The flow control enabled.

kENET_QOS_BroadCastRxDisable 

The broadcast disabled.

kENET_QOS_MulticastAllEnable 

All multicast are passed.

kENET_QOS_8023AS2KPacket 

8023as support for 2K packets.

kENET_QOS_HashMulticastEnable 

The multicast packets are filtered through hash table.

This enumeration uses one-bot encoding to allow a logical OR of multiple members.

Enumerator
kENET_QOS_DmaTx 

Tx interrupt.

kENET_QOS_DmaTxStop 

Tx stop interrupt.

kENET_QOS_DmaTxBuffUnavail 

Tx buffer unavailable.

kENET_QOS_DmaRx 

Rx interrupt.

kENET_QOS_DmaRxBuffUnavail 

Rx buffer unavailable.

kENET_QOS_DmaRxStop 

Rx stop.

kENET_QOS_DmaRxWatchdogTimeout 

Rx watchdog timeout.

kENET_QOS_DmaEarlyTx 

Early transmit.

kENET_QOS_DmaEarlyRx 

Early receive.

kENET_QOS_DmaBusErr 

Fatal bus error.

This enumeration uses one-bot encoding to allow a logical OR of multiple members.

Enumerator
kENET_QOS_RxIntEvent 

Receive interrupt event.

kENET_QOS_TxIntEvent 

Transmit interrupt event.

kENET_QOS_WakeUpIntEvent 

Wake up interrupt event.

kENET_QOS_TimeStampIntEvent 

Time stamp interrupt event.

Enumerator
kENET_QOS_AVB_Mode 

Enable queue in AVB mode.

kENET_QOS_DCB_Mode 

Enable queue in DCB mode.

Enumerator
kENET_QOS_txWeightRR 

Tx weight round-robin.

kENET_QOS_txWeightFQ 

Tx weight fair queuing.

kENET_QOS_txDefictWeightRR 

Tx deficit weighted round-robin.

kENET_QOS_txStrPrio 

Tx strict priority.

Enumerator
kENET_QOS_rxStrPrio 

Rx strict priority, Queue 0 has the lowest priority.

kENET_QOS_rxWeightStrPrio 

Weighted Strict Priority.

Enumerator
kENET_QOS_StaticDirctMap 

The received fame in rx Qn(n = 0,1) directly map to dma channel n.

kENET_QOS_DynamicMap 

The received frame in rx Qn(n = 0,1) map to the dma channel m(m = 0,1) related with the same Mac.

Enumerator
kENET_QOS_PtpEventMsgType 

PTP event message type.

kENET_QOS_PtpSrcPortIdLen 

PTP message sequence id length.

kENET_QOS_PtpEventPort 

PTP event port number.

kENET_QOS_PtpGnrlPort 

PTP general port number.

Enumerator
kENET_QOS_PtpPpsIstance0 

PPS instance 0.

kENET_QOS_PtpPpsIstance1 

PPS instance 1.

kENET_QOS_PtpPpsIstance2 

PPS instance 2.

kENET_QOS_PtpPpsIstance3 

PPS instance 3.

Enumerator
kENET_QOS_PtpPpsTrgtModeOnlyInt 

Only interrupts.

kENET_QOS_PtpPpsTrgtModeIntSt 

Both interrupt and output signal.

kENET_QOS_PtpPpsTrgtModeOnlySt 

Only output signal.

Enumerator
kENET_QOS_PtpPpsCmdNC 

No Command.

kENET_QOS_PtpPpsCmdSSP 

Start Single Pulse.

kENET_QOS_PtpPpsCmdSPT 

Start Pulse Train.

kENET_QOS_PtpPpsCmdCS 

Cancel Start.

kENET_QOS_PtpPpsCmdSPTAT 

Stop Pulse Train At Time.

kENET_QOS_PtpPpsCmdSPTI 

Stop Pulse Train Immediately.

kENET_QOS_PtpPpsCmdCSPT 

Cancel Stop Pulse Train.

Enumerator
kENET_QOS_Ets_List_64 

List length of 64.

kENET_QOS_Ets_List_128 

List length of 128.

kENET_QOS_Ets_List_256 

List length of 256.

kENET_QOS_Ets_List_512 

List length of 512.

kENET_QOS_Ets_List_1024 

List length of 1024.

Enumerator
kENET_QOS_Ets_btr_low 

BTR Low.

kENET_QOS_Ets_btr_high 

BTR High.

kENET_QOS_Ets_ctr_low 

CTR Low.

kENET_QOS_Ets_ctr_high 

CTR High.

kENET_QOS_Ets_ter 

TER.

kENET_QOS_Ets_llr 

LLR.

Enumerator
kENET_QOS_Rxp_DMAChn0 

DMA Channel 0 used for RXP entry match.

kENET_QOS_Rxp_DMAChn1 

DMA Channel 1 used for RXP entry match.

kENET_QOS_Rxp_DMAChn2 

DMA Channel 2 used for RXP entry match.

kENET_QOS_Rxp_DMAChn3 

DMA Channel 3 used for RXP entry match.

kENET_QOS_Rxp_DMAChn4 

DMA Channel 4 used for RXP entry match.

Function Documentation

void ENET_QOS_GetDefaultConfig ( enet_qos_config_t *  config)

The purpose of this API is to get the default ENET configure structure for ENET_QOS_Init(). User may use the initialized structure unchanged in ENET_QOS_Init(), or modify some fields of the structure before calling ENET_QOS_Init(). Example:

Parameters
configThe ENET mac controller configuration structure pointer.
status_t ENET_QOS_Up ( ENET_QOS_Type *  base,
const enet_qos_config_t *  config,
uint8_t *  macAddr,
uint8_t  macCount,
uint32_t  refclkSrc_Hz 
)

This function initializes it with the ENET basic configuration.

Parameters
baseENET peripheral base address.
configENET mac configuration structure pointer. The "enet_qos_config_t" type mac configuration return from ENET_QOS_GetDefaultConfig can be used directly. It is also possible to verify the Mac configuration using other methods.
macAddrPointer to ENET mac address array of Ethernet device. This MAC address should be provided.
macCountCount of macAddr in the ENET mac address array
refclkSrc_HzENET input reference clock.
status_t ENET_QOS_Init ( ENET_QOS_Type *  base,
const enet_qos_config_t *  config,
uint8_t *  macAddr,
uint8_t  macCount,
uint32_t  refclkSrc_Hz 
)

This function ungates the module clock and initializes it with the ENET basic configuration.

Parameters
baseENET peripheral base address.
configENET mac configuration structure pointer. The "enet_qos_config_t" type mac configuration return from ENET_QOS_GetDefaultConfig can be used directly. It is also possible to verify the Mac configuration using other methods.
macAddrPointer to ENET mac address array of Ethernet device. This MAC address should be provided.
macCountCount of macAddr in the ENET mac address array
refclkSrc_HzENET input reference clock.
void ENET_QOS_Down ( ENET_QOS_Type *  base)

This function disables the ENET module.

param base ENET peripheral base address.

void ENET_QOS_Deinit ( ENET_QOS_Type *  base)

This function gates the module clock and disables the ENET module.

Parameters
baseENET peripheral base address.
uint32_t ENET_QOS_GetInstance ( ENET_QOS_Type *  base)
Parameters
baseENET peripheral base address.
Returns
ENET instance.
status_t ENET_QOS_DescriptorInit ( ENET_QOS_Type *  base,
enet_qos_config_t *  config,
enet_qos_buffer_config_t *  bufferConfig 
)
Note
This function is do all tx/rx descriptors initialization. Because this API read all interrupt registers first and then set the interrupt flag for all descriptors, if the interrupt register is set. so the descriptor initialization should be called after ENET_QOS_Init(), ENET_QOS_EnableInterrupts() and ENET_QOS_CreateHandle()(if transactional APIs are used).
Parameters
baseENET peripheral base address.
configThe configuration for ENET.
bufferConfigAll buffers configuration.
void ENET_QOS_StartRxTx ( ENET_QOS_Type *  base,
uint8_t  txRingNum,
uint8_t  rxRingNum 
)

This function enable the tx/rx and starts the rx/tx DMA. This shall be set after ENET initialization and before starting to receive the data.

Parameters
baseENET peripheral base address.
rxRingNumThe number of the used rx rings. It shall not be larger than the ENET_QOS_RING_NUM_MAX(2). If the ringNum is set with 1, the ring 0 will be used.
txRingNumThe number of the used tx rings. It shall not be larger than the ENET_QOS_RING_NUM_MAX(2). If the ringNum is set with 1, the ring 0 will be used.
Note
This must be called after all the ENET initialization. And should be called when the ENET receive/transmit is required.
static void ENET_QOS_SetMII ( ENET_QOS_Type *  base,
enet_qos_mii_speed_t  speed,
enet_qos_mii_duplex_t  duplex 
)
inlinestatic

This API is provided to dynamically change the speed and duplex for MAC.

Parameters
baseENET peripheral base address.
speedThe speed of the RMII mode.
duplexThe duplex of the RMII mode.
void ENET_QOS_SetSMI ( ENET_QOS_Type *  base,
uint32_t  csrClock_Hz 
)
Parameters
baseENET peripheral base address.
csrClock_HzCSR clock frequency in HZ
static bool ENET_QOS_IsSMIBusy ( ENET_QOS_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
Returns
The status of MII Busy status.
static uint16_t ENET_QOS_ReadSMIData ( ENET_QOS_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
Returns
The data read from PHY
void ENET_QOS_StartSMIRead ( ENET_QOS_Type *  base,
uint32_t  phyAddr,
uint32_t  phyReg 
)

support both MDIO IEEE802.3 Clause 22 and clause 45.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
phyRegThe PHY register.
void ENET_QOS_StartSMIWrite ( ENET_QOS_Type *  base,
uint32_t  phyAddr,
uint32_t  phyReg,
uint32_t  data 
)

support both MDIO IEEE802.3 Clause 22 and clause 45.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
phyRegThe PHY register.
dataThe data written to PHY.
static void ENET_QOS_SetMacAddr ( ENET_QOS_Type *  base,
uint8_t *  macAddr,
uint8_t  index 
)
inlinestatic
Parameters
baseENET peripheral base address.
macAddrThe six-byte Mac address pointer. The pointer is allocated by application and input into the API.
indexConfigure macAddr to MAC_ADDRESS[index] register.
void ENET_QOS_GetMacAddr ( ENET_QOS_Type *  base,
uint8_t *  macAddr,
uint8_t  index 
)
Parameters
baseENET peripheral base address.
macAddrThe six-byte Mac address pointer. The pointer is allocated by application and input into the API.
indexGet macAddr from MAC_ADDRESS[index] register.
void ENET_QOS_AddMulticastGroup ( ENET_QOS_Type *  base,
uint8_t *  address 
)
Parameters
baseENET_QOS peripheral base address.
addressThe six-byte multicast group address which is provided by application.
void ENET_QOS_LeaveMulticastGroup ( ENET_QOS_Type *  base,
uint8_t *  address 
)

param base ENET_QOS peripheral base address. param address The six-byte multicast group address which is provided by application.

static void ENET_QOS_AcceptAllMulticast ( ENET_QOS_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
static void ENET_QOS_RejectAllMulticast ( ENET_QOS_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
void ENET_QOS_EnterPowerDown ( ENET_QOS_Type *  base,
uint32_t *  wakeFilter 
)

the remote power wake up frame and magic frame can wake up the ENET from the power down mode.

Parameters
baseENET peripheral base address.
wakeFilterThe wakeFilter provided to configure the wake up frame filter. Set the wakeFilter to NULL is not required. But if you have the filter requirement, please make sure the wakeFilter pointer shall be eight continuous 32-bits configuration.
static void ENET_QOS_ExitPowerDown ( ENET_QOS_Type *  base)
inlinestatic

Exit from the power down mode and recover to normal work mode.

Parameters
baseENET peripheral base address.
status_t ENET_QOS_EnableRxParser ( ENET_QOS_Type *  base,
bool  enable 
)
Parameters
baseENET_QOS peripheral base address.
enableEnable/Disable Rx parser function
Return values
kStatus_SuccessConfigure rx parser success.
kStatus_ENET_QOS_TimeoutPoll status flag timeout.
void ENET_QOS_EnableInterrupts ( ENET_QOS_Type *  base,
uint32_t  mask 
)

This function enables the ENET interrupt according to the provided mask. The mask is a logical OR of enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t. For example, to enable the dma and mac interrupt, do the following.

Parameters
baseENET peripheral base address.
maskENET interrupts to enable. This is a logical OR of both enumeration :: enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t.
void ENET_QOS_DisableInterrupts ( ENET_QOS_Type *  base,
uint32_t  mask 
)

This function disables the ENET interrupt according to the provided mask. The mask is a logical OR of enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t. For example, to disable the dma and mac interrupt, do the following.

Parameters
baseENET peripheral base address.
maskENET interrupts to disables. This is a logical OR of both enumeration :: enet_qos_dma_interrupt_enable_t and enet_qos_mac_interrupt_enable_t.
static uint32_t ENET_QOS_GetDmaInterruptStatus ( ENET_QOS_Type *  base,
uint8_t  channel 
)
inlinestatic
Parameters
baseENET peripheral base address.
channelThe DMA Channel. Shall not be larger than ENET_QOS_RING_NUM_MAX.
Returns
The event status of the interrupt source. This is the logical OR of members of the enumeration :: enet_qos_dma_interrupt_enable_t.
static void ENET_QOS_ClearDmaInterruptStatus ( ENET_QOS_Type *  base,
uint8_t  channel,
uint32_t  mask 
)
inlinestatic
Parameters
baseENET peripheral base address.
channelThe DMA Channel. Shall not be larger than ENET_QOS_RING_NUM_MAX.
maskThe interrupt status to be cleared. This is the logical OR of members of the enumeration :: enet_qos_dma_interrupt_enable_t.
static uint32_t ENET_QOS_GetMacInterruptStatus ( ENET_QOS_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
Returns
The event status of the interrupt source. Use the enum in enet_qos_mac_interrupt_enable_t and right shift ENET_QOS_MACINT_ENUM_OFFSET to mask the returned value to get the exact interrupt status.
void ENET_QOS_ClearMacInterruptStatus ( ENET_QOS_Type *  base,
uint32_t  mask 
)

This function clears enabled ENET interrupts according to the provided mask. The mask is a logical OR of enumeration members. See the enet_qos_mac_interrupt_enable_t. For example, to clear the TX frame interrupt and RX frame interrupt, do the following.

* ENET_QOS_ClearMacInterruptStatus(ENET, kENET_QOS_MacPmt);
*
Parameters
baseENET peripheral base address.
maskENET interrupt source to be cleared. This is the logical OR of members of the enumeration :: enet_qos_mac_interrupt_enable_t.
static bool ENET_QOS_IsTxDescriptorDmaOwn ( enet_qos_tx_bd_struct_t *  txDesc)
inlinestatic
Parameters
txDescThe given tx descriptor.
Return values
Truethe dma own tx descriptor, false application own tx descriptor.
void ENET_QOS_SetupTxDescriptor ( enet_qos_tx_bd_struct_t *  txDesc,
void *  buffer1,
uint32_t  bytes1,
void *  buffer2,
uint32_t  bytes2,
uint32_t  framelen,
bool  intEnable,
bool  tsEnable,
enet_qos_desc_flag  flag,
uint8_t  slotNum 
)

This function is a low level functional API to setup or prepare a given tx descriptor.

Parameters
txDescThe given tx descriptor.
buffer1The first buffer address in the descriptor.
bytes1The bytes in the fist buffer.
buffer2The second buffer address in the descriptor.
bytes2The bytes in the second buffer.
framelenThe length of the frame to be transmitted.
intEnableInterrupt enable flag.
tsEnableThe timestamp enable.
flagThe flag of this tx descriptor, enet_qos_desc_flag .
slotNumThe slot num used for AV only.
Note
This must be called after all the ENET initialization. And should be called when the ENET receive/transmit is required. Transmit buffers are 'zero-copy' buffers, so the buffer must remain in memory until the packet has been fully transmitted. The buffers should be free or requeued in the transmit interrupt irq handler.
static void ENET_QOS_UpdateTxDescriptorTail ( ENET_QOS_Type *  base,
uint8_t  channel,
uint32_t  txDescTailAddrAlign 
)
inlinestatic

This function is a low level functional API to update the the tx descriptor tail. This is called after you setup a new tx descriptor to update the tail pointer to make the new descriptor accessible by DMA.

Parameters
baseENET peripheral base address.
channelThe tx DMA channel.
txDescTailAddrAlignThe new tx tail pointer address.
static void ENET_QOS_UpdateRxDescriptorTail ( ENET_QOS_Type *  base,
uint8_t  channel,
uint32_t  rxDescTailAddrAlign 
)
inlinestatic

This function is a low level functional API to update the the rx descriptor tail. This is called after you setup a new rx descriptor to update the tail pointer to make the new descriptor accessible by DMA and to anouse the rx poll command for DMA.

Parameters
baseENET peripheral base address.
channelThe rx DMA channel.
rxDescTailAddrAlignThe new rx tail pointer address.
static uint32_t ENET_QOS_GetRxDescriptor ( enet_qos_rx_bd_struct_t *  rxDesc)
inlinestatic

This function is a low level functional API to get the the status flag from a given rx descriptor.

Parameters
rxDescThe given rx descriptor.
Return values
TheRDES3 regions for write-back format rx buffer descriptor.
Note
This must be called after all the ENET initialization. And should be called when the ENET receive/transmit is required.
void ENET_QOS_UpdateRxDescriptor ( enet_qos_rx_bd_struct_t *  rxDesc,
void *  buffer1,
void *  buffer2,
bool  intEnable,
bool  doubleBuffEnable 
)

This function is a low level functional API to Updates the buffers and the own status for a given rx descriptor.

Parameters
rxDescThe given rx descriptor.
buffer1The first buffer address in the descriptor.
buffer2The second buffer address in the descriptor.
intEnableInterrupt enable flag.
doubleBuffEnableThe double buffer enable flag.
Note
This must be called after all the ENET initialization. And should be called when the ENET receive/transmit is required.
status_t ENET_QOS_ConfigureRxParser ( ENET_QOS_Type *  base,
enet_qos_rxp_config_t *  rxpConfig,
uint16_t  entryCount 
)

This function is used to configure the flexible rx parser table.

Parameters
baseENET peripheral base address..
rxpConfigThe rx parser configuration pointer.
entryCountThe rx parser entry count.
Return values
kStatus_SuccessConfigure rx parser success.
kStatus_ENET_QOS_TimeoutPoll status flag timeout.
status_t ENET_QOS_ReadRxParser ( ENET_QOS_Type *  base,
enet_qos_rxp_config_t *  rxpConfig,
uint16_t  entryIndex 
)

This function is used to read flexible rx parser configuration at specified index.

Parameters
baseENET peripheral base address..
rxpConfigThe rx parser configuration pointer.
entryIndexThe rx parser entry index to read, start from 0.
Return values
kStatus_SuccessConfigure rx parser success.
kStatus_ENET_QOS_TimeoutPoll status flag timeout.
status_t ENET_QOS_EstProgramGcl ( ENET_QOS_Type *  base,
enet_qos_est_gcl_t *  gcl,
uint32_t  ptpClk_Hz 
)

This function is used to program the Enhanced Scheduled Transmisson. (IEEE802.1Qbv)

Parameters
baseENET peripheral base address..
gclPointer to the Gate Control List structure.
ptpClk_Hzfrequency of the PTP clock.
status_t ENET_QOS_EstReadGcl ( ENET_QOS_Type *  base,
enet_qos_est_gcl_t *  gcl,
uint32_t  listLen,
bool  hwList 
)

This function is used to read the Enhanced Scheduled Transmisson list. (IEEE802.1Qbv)

Parameters
baseENET peripheral base address..
gclPointer to the Gate Control List structure.
listLenlength of the provided opList array in gcl structure.
hwListBoolean if True read HW list, false read SW list.
static void ENET_QOS_FpeEnable ( ENET_QOS_Type *  base)
inlinestatic

This function is used to enable frame preemption. (IEEE802.1Qbu)

Parameters
baseENET peripheral base address..
static void ENET_QOS_FpeDisable ( ENET_QOS_Type *  base)
inlinestatic

This function is used to disable frame preemption. (IEEE802.1Qbu)

Parameters
baseENET peripheral base address..
static void ENET_QOS_FpeConfigPreemptable ( ENET_QOS_Type *  base,
uint8_t  queueMask 
)
inlinestatic

This function is used to configure the preemptable queues. (IEEE802.1Qbu)

Parameters
baseENET peripheral base address..
queueMaskbitmask representing queues to set in preemptable mode. The N-th bit represents the queue N.
void ENET_QOS_AVBConfigure ( ENET_QOS_Type *  base,
const enet_qos_cbs_config_t *  config,
uint8_t  queueIndex 
)

ENET_QOS AVB feature configuration, set transmit bandwidth. This API is called when the AVB feature is required.

Parameters
baseENET_QOS peripheral base address.
configThe ENET_QOS AVB feature configuration structure.
queueIndexENET_QOS queue index.
void ENET_QOS_CreateHandler ( ENET_QOS_Type *  base,
enet_qos_handle_t *  handle,
enet_qos_config_t *  config,
enet_qos_buffer_config_t *  bufferConfig,
enet_qos_callback_t  callback,
void *  userData 
)

This is a transactional API and it's provided to store all data which are needed during the whole transactional process. This API should not be used when you use functional APIs to do data tx/rx. This is function will store many data/flag for transactional use, so all configure API such as ENET_QOS_Init(), ENET_QOS_DescriptorInit(), ENET_QOS_EnableInterrupts() etc.

Note
as our transactional transmit API use the zero-copy transmit buffer. so there are two thing we emphasize here:
  1. tx buffer free/requeue for application should be done in the tx interrupt handler. Please set callback: kENET_QOS_TxIntEvent with tx buffer free/requeue process APIs.
  2. the tx interrupt is forced to open.
Parameters
baseENET peripheral base address.
handleENET handler.
configENET configuration.
bufferConfigENET buffer configuration.
callbackThe callback function.
userDataThe application data.
status_t ENET_QOS_GetRxFrameSize ( ENET_QOS_Type *  base,
enet_qos_handle_t *  handle,
uint32_t *  length,
uint8_t  channel 
)

This function gets a received frame size from the ENET buffer descriptors.

Note
The FCS of the frame is automatically removed by MAC and the size is the length without the FCS. After calling ENET_QOS_GetRxFrameSize, ENET_QOS_ReadFrame() should be called to update the receive buffers If the result is not "kStatus_ENET_QOS_RxFrameEmpty".
Parameters
baseENET peripheral base address.
handleThe ENET handler structure. This is the same handler pointer used in the ENET_QOS_Init.
lengthThe length of the valid frame received.
channelThe DMAC channel for the rx.
Return values
kStatus_ENET_QOS_RxFrameEmptyNo frame received. Should not call ENET_QOS_ReadFrame to read frame.
kStatus_ENET_QOS_RxFrameErrorData error happens. ENET_QOS_ReadFrame should be called with NULL data and NULL length to update the receive buffers.
kStatus_SuccessReceive a frame Successfully then the ENET_QOS_ReadFrame should be called with the right data buffer and the captured data length input.
status_t ENET_QOS_ReadFrame ( ENET_QOS_Type *  base,
enet_qos_handle_t *  handle,
uint8_t *  data,
uint32_t  length,
uint8_t  channel,
enet_qos_ptp_time_t *  ts 
)

This function reads a frame from the ENET DMA descriptors. The ENET_QOS_GetRxFrameSize should be used to get the size of the prepared data buffer. For example use rx dma channel 0:

* uint32_t length;
* enet_qos_handle_t g_handle;
* status = ENET_QOS_GetRxFrameSize(&g_handle, &length, 0);
* if (length != 0)
* {
* uint8_t *data = memory allocate interface;
* if (!data)
* {
* ENET_QOS_ReadFrame(ENET, &g_handle, NULL, 0, 0);
* }
* else
* {
* status = ENET_QOS_ReadFrame(ENET, &g_handle, data, length, 0);
* }
* }
* else if (status == kStatus_ENET_QOS_RxFrameError)
* {
* ENET_QOS_ReadFrame(ENET, &g_handle, NULL, 0, 0);
* }
*
Parameters
baseENET peripheral base address.
handleThe ENET handler structure. This is the same handler pointer used in the ENET_QOS_Init.
dataThe data buffer provided by user to store the frame which memory size should be at least "length".
lengthThe size of the data buffer which is still the length of the received frame.
channelThe rx DMA channel. shall not be larger than 2.
tsPointer to the structure enet_qos_ptp_time_t to save frame timestamp.
Returns
The execute status, successful or failure.
status_t ENET_QOS_SendFrame ( ENET_QOS_Type *  base,
enet_qos_handle_t *  handle,
uint8_t *  data,
uint32_t  length,
uint8_t  channel,
bool  isNeedTs,
void *  context 
)
Note
The CRC is automatically appended to the data. Input the data to send without the CRC.
Parameters
baseENET peripheral base address.
handleThe ENET handler pointer. This is the same handler pointer used in the ENET_QOS_Init.
dataThe data buffer provided by user to be send.
lengthThe length of the data to be send.
channelChannel to send the frame, same with queue index.
isNeedTsTrue to enable timestamp save for the frame
contextpointer to user context to be kept in the tx dirty frame information.
Return values
kStatus_SuccessSend frame succeed.
kStatus_ENET_QOS_TxFrameBusyTransmit buffer descriptor is busy under transmission. The transmit busy happens when the data send rate is over the MAC capacity. The waiting mechanism is recommended to be added after each call return with kStatus_ENET_QOS_TxFrameBusy.
void ENET_QOS_ReclaimTxDescriptor ( ENET_QOS_Type *  base,
enet_qos_handle_t *  handle,
uint8_t  channel 
)

This function is used to update the tx descriptor status and store the tx timestamp when the 1588 feature is enabled. This is called by the transmit interrupt IRQ handler after the complete of a frame transmission.

Parameters
baseENET peripheral base address.
handleThe ENET handler pointer. This is the same handler pointer used in the ENET_QOS_Init.
channelThe tx DMA channel.
void ENET_QOS_CommonIRQHandler ( ENET_QOS_Type *  base,
enet_qos_handle_t *  handle 
)
Parameters
baseENET peripheral base address.
handleThe ENET handler pointer.
void ENET_QOS_SetISRHandler ( ENET_QOS_Type *  base,
enet_qos_isr_t  ISRHandler 
)
Parameters
baseENET peripheral base address.
ISRHandlerThe handler to install.
status_t ENET_QOS_Ptp1588CorrectTimerInCoarse ( ENET_QOS_Type *  base,
enet_qos_systime_op  operation,
uint32_t  second,
uint32_t  nanosecond 
)
Parameters
baseENET peripheral base address.
operationThe system time operation, refer to "enet_qos_systime_op"
secondThe correction second.
nanosecondThe correction nanosecond.
status_t ENET_QOS_Ptp1588CorrectTimerInFine ( ENET_QOS_Type *  base,
uint32_t  addend 
)
Parameters
baseENET peripheral base address.
addendThe addend value to be set in the fine method
Note
Should take refer to the chapter "System time correction" and see the description for the "fine correction method".
static uint32_t ENET_QOS_Ptp1588GetAddend ( ENET_QOS_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
Returns
The addend value.
void ENET_QOS_Ptp1588GetTimerNoIRQDisable ( ENET_QOS_Type *  base,
uint64_t *  second,
uint32_t *  nanosecond 
)
Parameters
baseENET peripheral base address.
secondThe PTP 1588 system timer second.
nanosecondThe PTP 1588 system timer nanosecond. For the unit of the nanosecond is 1ns. so the nanosecond is the real nanosecond.
static status_t ENET_Ptp1588PpsControl ( ENET_QOS_Type *  base,
enet_qos_ptp_pps_instance_t  instance,
enet_qos_ptp_pps_trgt_mode_t  trgtMode,
enet_qos_ptp_pps_cmd_t  cmd 
)
inlinestatic

All channels operate in flexible PPS output mode.

Parameters
baseENET peripheral base address.
instanceThe ENET QOS PTP PPS instance.
trgtModeThe target time register mode.
cmdThe target flexible PPS output control command.
status_t ENET_QOS_Ptp1588PpsSetTrgtTime ( ENET_QOS_Type *  base,
enet_qos_ptp_pps_instance_t  instance,
uint32_t  seconds,
uint32_t  nanoseconds 
)
Parameters
baseENET QOS peripheral base address.
instanceThe ENET QOS PTP PPS instance.
secondsThe target seconds.
nanosecondsThe target nanoseconds.
static void ENET_QOS_Ptp1588PpsSetWidth ( ENET_QOS_Type *  base,
enet_qos_ptp_pps_instance_t  instance,
uint32_t  width 
)
inlinestatic

param base ENET QOS peripheral base address. param instance The ENET QOS PTP PPS instance. param width Signal Width. It is stored in terms of number of units of sub-second increment value. The width value must be lesser than interval value.

static void ENET_QOS_Ptp1588PpsSetInterval ( ENET_QOS_Type *  base,
enet_qos_ptp_pps_instance_t  instance,
uint32_t  interval 
)
inlinestatic

param base ENET QOS peripheral base address. param instance The ENET QOS PTP PPS instance. param interval Signal Interval. It is stored in terms of number of units of sub-second increment value.

void ENET_QOS_Ptp1588GetTimer ( ENET_QOS_Type *  base,
uint64_t *  second,
uint32_t *  nanosecond 
)
Parameters
baseENET peripheral base address.
secondThe PTP 1588 system timer second.
nanosecondThe PTP 1588 system timer nanosecond. For the unit of the nanosecond is 1ns.so the nanosecond is the real nanosecond.
void ENET_QOS_GetTxFrame ( enet_qos_handle_t *  handle,
enet_qos_frame_info_t *  txFrame,
uint8_t  channel 
)

This function is used for PTP stack to get the timestamp captured by the ENET driver.

Parameters
handleThe ENET handler pointer.This is the same state pointer used in ENET_QOS_Init.
txFrameInput parameter, pointer to enet_qos_frame_info_t for saving read out frame information.
channelChannel for searching the tx frame.