![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.
The clock driver supports:
Files | |
| file | fsl_clock.h |
Macros | |
| #define | FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0 |
| Configure whether driver controls clock. More... | |
| #define | MU_CLOCKS |
| Clock ip name array for MU. More... | |
| #define | GPIO_CLOCKS |
| Clock ip name array for GPIO. More... | |
| #define | FLEXSPI_CLOCKS |
| Clock ip name array for FLEXSPI. More... | |
| #define | RGPIO_CLOCKS |
| Clock ip name array for RGPIO. More... | |
| #define | FTM_CLOCKS |
| Clock ip name array for FTM. More... | |
| #define | GPT_CLOCKS |
| Clock ip name array for GPT. More... | |
| #define | FLEXCAN_CLOCKS |
| Clock ip name array for FLEXCAN.CAN1/CAN2 share the clock from CAN0. | |
| #define | LPUART_CLOCKS |
| Clock ip name array for LPUART. More... | |
| #define | LPADC_CLOCKS |
| Clock ip name array for LPADC. More... | |
| #define | LCDIF_CLOCKS |
| Clock ip name array for LCDIF. More... | |
| #define | INTMUX_CLOCKS |
| Clock ip name array for INTMUX. More... | |
| #define | SAI_CLOCKS |
| Clock ip name array for SAI. More... | |
| #define | SEMA42_CLOCKS |
| Clock ip name array for SAI. More... | |
| #define | TPM_CLOCKS |
| Clock ip name array for TPM. More... | |
| #define | LPIT_CLOCKS |
| Clock ip name array for LPIT. More... | |
| #define | LPI2C_CLOCKS |
| Clock ip name array for LPI2C. More... | |
| #define | LPSPI_CLOCKS |
| Clock ip name array for LPSPI. More... | |
| #define | EDMA_CLOCKS |
| Clock ip name array for EDMA. More... | |
| #define | ESAI_CLOCKS |
| Clock ip name array for LPIT. More... | |
| #define | ISI_CLOCKS |
| Clock ip name array for ISI. More... | |
| #define | MIPI_CSI2RX_CLOCKS |
| Clock ip name array for MIPI CSI2 RX. More... | |
| #define | MIPI_DSI_HOST_CLOCKS |
| Clock ip name array for MIPI DSI host. More... | |
| #define | ENET_CLOCKS |
| Clock ip name array for ENET. More... | |
| #define | ENETQOS_CLOCKS |
| Clock ip name array for ENET_QOS. More... | |
| #define | DPU_CLOCKS |
| Clock ip name array for DPU. More... | |
| #define | CI_PI_CLOCKS |
| Clock ip name array for CI_PI. More... | |
| #define | CAAM_CLOCKS |
| Clock ip name array for CAAM. More... | |
| #define | LDB_CLOCKS |
| Clock ip name array for LVDS display bridge(LDB). More... | |
| #define | LPCG_TUPLE(rsrc, base) ((uint32_t)((((base) >> 12U) << 10U) | (rsrc))) |
| LPCG TUPLE macors to map corresponding ip clock name, SCFW API resource index and LPCG Register base address. More... | |
| #define | LPCG_TUPLE_REG_BASE(tuple) ((volatile uint32_t *)((((uint32_t)(tuple) >> 10U) & 0xFFFFFU) << 12U)) |
| Get the LPCG REG base address. More... | |
| #define | LPCG_TUPLE_RSRC(tuple) ((sc_rsrc_t)((uint32_t)(tuple)&0x3FFU)) |
| Get the resource index. More... | |
| #define | NV (0U) |
| LPCG Cell not available. More... | |
Enumerations | |
| enum | clock_ip_src_t { kCLOCK_IpSrcNone = 0U, kCLOCK_IpSrcDummy = 1U } |
| Clock source for peripherals that support various clock selections. More... | |
| enum | clock_name_t { kCLOCK_CoreSysClk, kCLOCK_CONECTIVITY_AhbClk } |
| Clock name used to get clock frequency. More... | |
| enum | clock_ip_name_t |
| Peripheral clock name difinition used for clock gate, clock source and clock divider setting. More... | |
Functions | |
| void | CLOCK_Init (sc_ipc_t ipc) |
| Initialize Clock module. More... | |
| void | CLOCK_Deinit (void) |
| Deinitialize Clock module. | |
| bool | CLOCK_EnableClockExt (clock_ip_name_t name, uint32_t gate) |
| Enable the clock for specific IP, with gate setting. More... | |
| static bool | CLOCK_EnableClock (clock_ip_name_t name) |
| Enable the clock for specific IP. More... | |
| bool | CLOCK_DisableClock (clock_ip_name_t name) |
| Disable the clock for specific IP. More... | |
| uint32_t | CLOCK_SetIpFreq (clock_ip_name_t name, uint32_t freq) |
| Set the clock frequency for specific IP module. More... | |
| uint32_t | CLOCK_GetIpFreq (clock_ip_name_t name) |
| Get the clock frequency for a specific IP module. More... | |
| uint32_t | CLOCK_GetFreq (clock_name_t name) |
| Gets the clock frequency for a specific clock name. More... | |
| uint32_t | CLOCK_GetCoreSysClkFreq (void) |
| Get the core clock or system clock frequency. More... | |
| void | CLOCK_ConfigLPCG (clock_ip_name_t name, bool swGate, bool hwGate) |
| Config the LPCG cell for specific IP. More... | |
| void | CLOCK_SetLpcgGate (volatile uint32_t *regBase, bool swGate, bool hwGate, uint32_t bitsMask) |
| Set LPCG gate for specific LPCG. More... | |
Driver version | |
| #define | FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
| CLOCK driver version 2.3.1. More... | |
| #define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0 |
When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.
| #define FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
| #define MU_CLOCKS |
| #define GPIO_CLOCKS |
| #define FLEXSPI_CLOCKS |
| #define RGPIO_CLOCKS |
| #define FTM_CLOCKS |
| #define GPT_CLOCKS |
| #define LPUART_CLOCKS |
| #define LPADC_CLOCKS |
| #define LCDIF_CLOCKS |
| #define INTMUX_CLOCKS |
| #define SAI_CLOCKS |
| #define SEMA42_CLOCKS |
| #define TPM_CLOCKS |
| #define LPIT_CLOCKS |
| #define LPI2C_CLOCKS |
| #define LPSPI_CLOCKS |
| #define EDMA_CLOCKS |
| #define ESAI_CLOCKS |
| #define ISI_CLOCKS |
| #define MIPI_CSI2RX_CLOCKS |
| #define MIPI_DSI_HOST_CLOCKS |
| #define ENET_CLOCKS |
| #define ENETQOS_CLOCKS |
| #define DPU_CLOCKS |
| #define CI_PI_CLOCKS |
| #define CAAM_CLOCKS |
| #define LDB_CLOCKS |
| #define LPCG_TUPLE | ( | rsrc, | |
| base | |||
| ) | ((uint32_t)((((base) >> 12U) << 10U) | (rsrc))) |
The LPCG base should be 4KB aligned, if not it will be truncated.
| #define LPCG_TUPLE_REG_BASE | ( | tuple | ) | ((volatile uint32_t *)((((uint32_t)(tuple) >> 10U) & 0xFFFFFU) << 12U)) |
| #define LPCG_TUPLE_RSRC | ( | tuple | ) | ((sc_rsrc_t)((uint32_t)(tuple)&0x3FFU)) |
| #define NV (0U) |
| enum clock_ip_src_t |
| enum clock_name_t |
| enum clock_ip_name_t |
It is defined as the corresponding register address.
| void CLOCK_Init | ( | sc_ipc_t | ipc | ) |
| ipc | IPC handle for communication with SCU. |
| bool CLOCK_EnableClockExt | ( | clock_ip_name_t | name, |
| uint32_t | gate | ||
| ) |
| name | Which clock to enable, see clock_ip_name_t. |
| gate | 0: clock always on, 1: HW auto clock gating. |
|
inlinestatic |
| name | Which clock to enable, see clock_ip_name_t. |
| bool CLOCK_DisableClock | ( | clock_ip_name_t | name | ) |
| name | Which clock to disable, see clock_ip_name_t. |
| uint32_t CLOCK_SetIpFreq | ( | clock_ip_name_t | name, |
| uint32_t | freq | ||
| ) |
This function sets the IP module clock frequency.
| name | Which peripheral to check, see clock_ip_name_t. |
| freq | Target clock frequency value in hertz. |
| uint32_t CLOCK_GetIpFreq | ( | clock_ip_name_t | name | ) |
This function gets the IP module clock frequency.
| name | Which peripheral to get, see clock_ip_name_t. |
| uint32_t CLOCK_GetFreq | ( | clock_name_t | name | ) |
This function checks the current clock configurations and then calculates the clock frequency for a specific clock name defined in clock_name_t.
| name | Clock names defined in clock_name_t |
| uint32_t CLOCK_GetCoreSysClkFreq | ( | void | ) |
| void CLOCK_ConfigLPCG | ( | clock_ip_name_t | name, |
| bool | swGate, | ||
| bool | hwGate | ||
| ) |
| name | Which clock to enable, see clock_ip_name_t. |
| swGate | Software clock gating. 0: clock is gated; 1: clock is enabled |
| hwGate | Hardware auto gating. 0: disable the HW clock gate control; 1: HW clock gating is enabled |
| void CLOCK_SetLpcgGate | ( | volatile uint32_t * | regBase, |
| bool | swGate, | ||
| bool | hwGate, | ||
| uint32_t | bitsMask | ||
| ) |
| regBase | LPCG register base address. |
| swGate | Software clock gating. 0: clock is gated; 1: clock is enabled |
| hwGate | Hardware auto gating. 0: disable the HW clock gate control; 1: HW clock gating is enabled |
| bitsMask | The available bits in LPCG register. Each bit indicate the corresponding bit is available or not. |