![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
The flash driver provides general APIs to handle specific operations on chip flash; The user can use those APIs directly in the application. The flash supports:
Driver Overview | |
| Driver Change Log | |
| The current FLASH driver version is 3.0.0.  | |
Data Structures | |
| struct | flash_swap_state_config_t | 
| Flash Swap information.  More... | |
| struct | flash_spec_mem_t | 
| ftfx special memory access information.  More... | |
| struct | flash_mem_desc_t | 
| Flash memory descriptor.  More... | |
| struct | flash_ops_config_t | 
| Active FTFx information for the current operation.  More... | |
| struct | flash_ifr_desc_t | 
| Flash IFR memory descriptor.  More... | |
| struct | ftfx_config_t | 
| Flash driver state information.  More... | |
Macros | |
| #define | MAKE_STATUS(group, code) ((((group)*100) + (code))) | 
| Construct a status code value from a group and code number.  More... | |
| #define | FTFx_FLASH_COUNT 1 | 
| Flash driver state information.  More... | |
Flash version | |
| enum | _flash_driver_version_constants {  kFLASH_DriverVersionName = 'F', kFLASH_DriverVersionMajor = 3, kFLASH_DriverVersionMinor = 0, kFLASH_DriverVersionBugfix = 0 }  | 
| Flash driver version for ROM.  More... | |
| #define | FSL_FLASH_DRIVER_VERSION (MAKE_VERSION(3U, 0U, 0U)) | 
| Flash driver version for SDK.  More... | |
| #define | FSL_FLASH_DRIVER_VERSION_ROM (MAKE_VERSION(3U, 0U, 0U)) | 
| Flash driver version for ROM.  More... | |
Initialization | |
| flash_status_t | FLASH_Init (flash_config_t *config) | 
| Initializes the global flash properties structure members.  More... | |
Properties | |
| flash_status_t | FLASH_GetProperty (flash_config_t *config, flash_property_tag_t whichProperty, uint32_t *value) | 
| Returns the desired flash property.  More... | |
Erasing | |
| flash_status_t | FLASH_Erase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, uint32_t key) | 
| Erases the flash sectors encompassed by parameters passed into function.  More... | |
| flash_status_t | FLASH_EraseAll (flash_config_t *config, uint32_t key) | 
| Erases entire flash, after done flash is on security status.  More... | |
| flash_status_t | FLASH_EraseAllUnsecure (flash_config_t *config, uint32_t key) | 
| Erases the entire flash, after done flash is on unsecurity status.  More... | |
Programming | |
| flash_status_t | FLASH_ProgramSection (flash_config_t *config, uint32_t start, uint8_t *src, uint32_t lengthInBytes) | 
| Programs flash with data at locations passed in through parameters via the Program Section command.  More... | |
| flash_status_t | FLASH_ProgramOnce (ftfx_config_t *config, uint32_t index, uint8_t *src, uint32_t lengthInBytes) | 
| Programs Program Once Field through parameters.  More... | |
Verification | |
| flash_status_t | FLASH_VerifyErase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, flash_margin_value_t margin) | 
| Verifies an erasure of the desired flash area at a specified margin level.  More... | |
| flash_status_t | FLASH_VerifyEraseAll (flash_config_t *config, flash_margin_value_t margin) | 
| Verifies erasure of the entire flash at a specified margin level.  More... | |
| flash_status_t | FLASH_VerifyProgram (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, const uint8_t *expectedData, flash_margin_value_t margin, uint32_t *failedAddress, uint32_t *failedData) | 
| Verifies programming of the desired flash area at a specified margin level.  More... | |
Security | |
| flash_status_t | FLASH_GetSecurityState (flash_config_t *config, flash_security_state_t *state) | 
| Returns the security state via the pointer passed into the function.  More... | |
| flash_status_t | FLASH_SecurityBypass (flash_config_t *config, const uint8_t *backdoorKey) | 
| Allows users to bypass security with a backdoor key.  More... | |
Reading | |
| flash_status_t | FLASH_ReadOnce (ftfx_config_t *config, uint32_t index, uint8_t *dst, uint32_t lengthInBytes) | 
| Reads the Program Once Field through parameters.  More... | |
| flash_status_t | FLASH_ReadResource (flash_config_t *config, uint32_t start, uint8_t *dst, uint32_t lengthInBytes, flash_read_resource_opt_t option) | 
| Reads the resource with data at locations passed in through parameters.  More... | |
Swap | |
| flash_status_t | FLASH_Swap (flash_config_t *config, uint32_t address, uint8_t isSetEnable) | 
| Swaps the lower half flash with the higher half flash.  More... | |
| struct flash_swap_state_config_t | 
Data Fields | |
| flash_swap_state_t | flashSwapState | 
| The current Swap system status.  More... | |
| flash_swap_block_status_t | currentSwapBlockStatus | 
| The current Swap block status.  More... | |
| flash_swap_block_status_t | nextSwapBlockStatus | 
| The next Swap block status.  More... | |
| flash_swap_state_t flash_swap_state_config_t::flashSwapState | 
| flash_swap_block_status_t flash_swap_state_config_t::currentSwapBlockStatus | 
| flash_swap_block_status_t flash_swap_state_config_t::nextSwapBlockStatus | 
| struct flash_spec_mem_t | 
| struct flash_mem_desc_t | 
Data Fields | |
| uint8_t | type | 
| Type of flash block.  More... | |
| uint8_t | index | 
| Index of flash block.  More... | |
| uint32_t | blockBase | 
| A base address of the flash block.  | |
| uint32_t | totalSize | 
| The size of the flash block.  More... | |
| uint32_t | sectorSize | 
| The size in bytes of a sector of flash.  More... | |
| uint32_t | blockCount | 
| A number of flash blocks.  More... | |
| uint8_t flash_mem_desc_t::type | 
| uint8_t flash_mem_desc_t::index | 
| uint32_t flash_mem_desc_t::totalSize | 
| uint32_t flash_mem_desc_t::sectorSize | 
| uint32_t flash_mem_desc_t::blockCount | 
| struct flash_ops_config_t | 
Data Fields | |
| uint32_t | convertedAddress | 
| A converted address for the current flash type.  More... | |
| uint32_t flash_ops_config_t::convertedAddress | 
| struct flash_ifr_desc_t | 
| struct ftfx_config_t | 
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
Data Fields | |
| uint32_t | flexramBlockBase | 
| The base address of the FlexRAM/acceleration RAM.  | |
| uint32_t | flexramTotalSize | 
| The size of the FlexRAM/acceleration RAM.  | |
| uint16_t | eepromTotalSize | 
| The size of EEPROM area which was partitioned from FlexRAM.  | |
| uint32_t * | runCmdFuncAddr | 
| An buffer point to the flash execute-in-RAM function.  More... | |
| uint32_t* ftfx_config_t::runCmdFuncAddr | 
| #define FSL_FLASH_DRIVER_VERSION (MAKE_VERSION(3U, 0U, 0U)) | 
Version 3.0.0.
| #define FSL_FLASH_DRIVER_VERSION_ROM (MAKE_VERSION(3U, 0U, 0U)) | 
Version 3.0.0.
| #define MAKE_STATUS | ( | group, | |
| code | |||
| ) | ((((group)*100) + (code))) | 
| #define FTFx_FLASH_COUNT 1 | 
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
| enum flash_margin_value_t | 
| enum flash_swap_state_t | 
| enum flash_property_tag_t | 
| enum _flash_status | 
| flash_status_t FLASH_Init | ( | flash_config_t * | config | ) | 
This function checks and initializes the Flash module for the other Flash APIs.
| config | Pointer to the storage for the driver runtime state. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| flash_status_t FLASH_GetProperty | ( | flash_config_t * | config, | 
| flash_property_tag_t | whichProperty, | ||
| uint32_t * | value | ||
| ) | 
| config | A pointer to the storage for the driver runtime state. | 
| whichProperty | The desired property from the list of properties in enum flash_property_tag_t | 
| value | A pointer to the value returned for the desired flash property. | 
| kStatus_FLASH_Success | API was executed successfully; the flash property was stored to value. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_UnknownProperty | An unknown property tag. | 
| config | A pointer to the storage for the driver runtime state. | 
| whichProperty | The desired property from the list of properties in enum flash_property_tag_t | 
| value | A pointer to the value returned for the desired flash property. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_UnknownProperty | An unknown property tag. | 
| flash_status_t FLASH_Erase | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| uint32_t | key | ||
| ) | 
This function erases the appropriate number of flash sectors based on the desired start address and length.
| config | The pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be erased. The start address does not need to be sector-aligned but must be phrase-aligned (64 bits). | 
| lengthInBytes | The length, given in bytes (not words or long-words) to be erased. Must be phrase-aligned (64 bits). | 
| key | The value used to validate all flash erase APIs. Use kFLASH_ApiEraseKey here. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AlignmentError | The parameter is not aligned with the specified baseline. | 
| kStatus_FLASH_AddressError | The address is out of range. | 
| kStatus_FLASH_EraseKeyError | The API erase key is invalid. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_EraseAll | ( | flash_config_t * | config, | 
| uint32_t | key | ||
| ) | 
| config | Pointer to the storage for the driver runtime state. | 
| key | A value used to validate all flash erase APIs. Use kFLASH_ApiEraseKey here. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_EraseKeyError | API erase key is invalid. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during command execution. | 
| flash_status_t FLASH_EraseAllUnsecure | ( | flash_config_t * | config, | 
| uint32_t | key | ||
| ) | 
| config | Pointer to the storage for the driver runtime state. | 
| key | A value used to validate all flash erase APIs. Use kFLASH_ApiEraseKey here. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_EraseKeyError | API erase key is invalid. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during command execution. | 
| flash_status_t FLASH_ProgramSection | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function programs the flash memory with the desired data for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be programmed. Must be phrase-aligned (64 bits). | 
| src | A pointer to the source buffer of data that is to be programmed into the flash. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be phrase-aligned (64 bits). | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FLASH_AddressError | Address is out of range. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during command execution. | 
| flash_status_t FLASH_ProgramOnce | ( | ftfx_config_t * | config, | 
| uint32_t | index, | ||
| uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function programs the Program Once Field with the desired data for a given flash area as determined by the index and length.
| config | A pointer to the storage for the driver runtime state. | 
| index | The index indicating which area of the Program Once Field to be programmed.Index is 0~7. | 
| src | A pointer to the source buffer of data that is to be programmed into the Program Once Field. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be phrase-aligned (64 bits). This value is ignored, it's always 8 bytes that are written into specified IFR area. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_VerifyErase | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| flash_margin_value_t | margin | ||
| ) | 
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be phrase-aligned (64 bits). | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be phrase-aligned (64 bits). | 
| margin | Read margin choice. Choose from the members in flash_margin_value_t. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FLASH_AddressError | Address is out of range. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_VerifyEraseAll | ( | flash_config_t * | config, | 
| flash_margin_value_t | margin | ||
| ) | 
This function checks whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. | 
| margin | Read margin choice. Choose from the members in flash_margin_value_t. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_VerifyProgram | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| const uint8_t * | expectedData, | ||
| flash_margin_value_t | margin, | ||
| uint32_t * | failedAddress, | ||
| uint32_t * | failedData | ||
| ) | 
This function verifies the data programed in the flash memory using the Flash Program Check Command and compares it to the expected data for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be verified. Must be longword-aligned (32 bits). | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be longword-aligned (32 bits). | 
| expectedData | A pointer to the expected data that is to be verified against. | 
| margin | Read margin choice. Choose from the members in flash_margin_value_t. "kFLASH_MarginValueNormal" is not for this command. | 
| failedAddress | A pointer to the returned failing address, which is used by PGMCHK command. So it's always longword-aligned. | 
| failedData | A pointer to the returned failing data. Some derivatives do not include failed data as part of the FCCOBx registers. In this case, zeros are returned upon failure. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FLASH_AddressError | Address is out of range. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_GetSecurityState | ( | flash_config_t * | config, | 
| flash_security_state_t * | state | ||
| ) | 
This function retrieves the current flash security status, including the security enabling state and the backdoor key enabling state.
| config | A pointer to storage for the driver runtime state. | 
| state | A pointer to the value returned for the current security status code: one of the members in flash_security_state_t. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| flash_status_t FLASH_SecurityBypass | ( | flash_config_t * | config, | 
| const uint8_t * | backdoorKey | ||
| ) | 
If the MCU is in secured state, this function unsecures the MCU by comparing the provided backdoor key with ones in the flash configuration field.
| config | A pointer to the storage for the driver runtime state. | 
| backdoorKey | A pointer to the user buffer containing the backdoor key. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_ReadOnce | ( | ftfx_config_t * | config, | 
| uint32_t | index, | ||
| uint8_t * | dst, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function reads the read once feild with given index and length.
| config | A pointer to the storage for the driver runtime state. | 
| index | The index indicating the area of program once field to be read. Index is 0~7. | 
| dst | A pointer to the destination buffer of data that is used to store data to be read. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. This value is ignored, it's always 8 bytes that are read out from the specified IFR area. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_ReadResource | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint8_t * | dst, | ||
| uint32_t | lengthInBytes, | ||
| flash_read_resource_opt_t | option | ||
| ) | 
This function reads the flash memory with the desired location for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory resource to be read. Must be phrase-aligned (64 bits). | 
| dst | A pointer to the destination buffer of data that is used to store data to be read. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be read. Must be phrase-aligned (64 bits). When option is "kFLASH_ResourceOptionFlashIfr", lengthInBytes can't be larger than 64. When option is "kFLASH_ResourceOptionVersionId", lengthInBytes should be set to 8. | 
| option | The resource option which indicates which area should be read back. Choose from "kFLASH_ResourceOptionFlashIfr" and "kFLASH_ResourceOptionVersionId". | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AlignmentError | Parameter is not aligned with the specified baseline. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during the command execution. | 
| flash_status_t FLASH_Swap | ( | flash_config_t * | config, | 
| uint32_t | address, | ||
| uint8_t | isSetEnable | ||
| ) | 
| config | A pointer to the storage for the driver runtime state. | 
| address | Address used to configure the flash swap function | 
| isSetEnable | The possible option used to configure the Flash Swap function or check the flash Swap status. | 
| kStatus_FLASH_Success | API was executed successfully. | 
| kStatus_FLASH_InvalidArgument | An invalid argument is provided. | 
| kStatus_FLASH_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FLASH_SwapIndicatorAddressError | Swap indicator address is invalid. | 
| kStatus_FLASH_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FLASH_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FLASH_CommandFailure | Run-time error during command execution. | 
| kStatus_FLASH_SwapSystemNotInUninitialized | Swap system is not in an uninitialzed state. |